This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ad9574-user-guide [04 Feb 2021 21:08] – [Quick Start Guide] Petre Minciunescu | resources:eval:ad9574-user-guide [05 Feb 2021 22:58] (current) – [Signal Connections] Petre Minciunescu | ||
---|---|---|---|
Line 54: | Line 54: | ||
- Place R212, R219, C221, C222, C226, and C227 with 0Ω resistors. | - Place R212, R219, C221, C222, C226, and C227 with 0Ω resistors. | ||
\\ | \\ | ||
+ | <note important> | ||
+ | |||
+ | |||
=== Monitor Clock Input (MCLK_x) === | === Monitor Clock Input (MCLK_x) === | ||
The AD9574/PCBZ provides a signal path to the MCLK_x inputs using SMA connector J216. The default BOM configuration allows for a 3.3V single ended CMOS signal to be applied to SMA connector J216 with the monitor clock input set to differential using the PPR6 biasing jumpers. | The AD9574/PCBZ provides a signal path to the MCLK_x inputs using SMA connector J216. The default BOM configuration allows for a 3.3V single ended CMOS signal to be applied to SMA connector J216 with the monitor clock input set to differential using the PPR6 biasing jumpers. |