This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ad9574-user-guide [27 Apr 2015 15:46] – [Quick Start Guide] Kyle Slightom | resources:eval:ad9574-user-guide [05 Feb 2021 22:58] (current) – [Signal Connections] Petre Minciunescu | ||
---|---|---|---|
Line 27: | Line 27: | ||
===== General Description ===== | ===== General Description ===== | ||
---- | ---- | ||
- | The [[adi> | + | The [[adi> |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 41: | Line 41: | ||
==== Power Connections ==== | ==== Power Connections ==== | ||
- | Connect the included 6V wall supply to P500 to power all of the necessary on board components. | + | Connect the included 6V wall supply to P500 to power all of the necessary on board components. |
==== Signal Connections ==== | ==== Signal Connections ==== | ||
=== Reference Inputs (REFx) === | === Reference Inputs (REFx) === | ||
- | The AD9574/PCBZ allows for the reference inputs to be clocked by one of two crystal oscillators (XO) at Y202 and Y204 or via single ended SMA connectors | + | The AD9574/PCBZ allows for the reference inputs to be clocked by one of two crystal oscillators (XO) at Y202 and Y204 or via single ended SMA connectors J217 and J215. The default signal path is to use 25MHz CMOS XOs for both REF0_P and REF1_P.\\ |
\\ | \\ | ||
The following board modifications from the default BOM are required to use the SMA reference input connectors to supply a differential reference instead of the 25MHz XOs: | The following board modifications from the default BOM are required to use the SMA reference input connectors to supply a differential reference instead of the 25MHz XOs: | ||
Line 52: | Line 52: | ||
The following board modifications from the default BOM are required to use the SMA reference input connectors to supply an external single ended CMOS reference input instead of the 25MHz XOs: | The following board modifications from the default BOM are required to use the SMA reference input connectors to supply an external single ended CMOS reference input instead of the 25MHz XOs: | ||
- Remove R214, R217, R218, R221, R224, R225, T201 and T202 | - Remove R214, R217, R218, R221, R224, R225, T201 and T202 | ||
- | - Place R212, R219, C221 and C222 with 0Ω resistors. | + | - Place R212, R219, C221, C222, C226, and C227 with 0Ω resistors. |
\\ | \\ | ||
+ | <note important> | ||
+ | |||
+ | |||
=== Monitor Clock Input (MCLK_x) === | === Monitor Clock Input (MCLK_x) === | ||
The AD9574/PCBZ provides a signal path to the MCLK_x inputs using SMA connector J216. The default BOM configuration allows for a 3.3V single ended CMOS signal to be applied to SMA connector J216 with the monitor clock input set to differential using the PPR6 biasing jumpers. | The AD9574/PCBZ provides a signal path to the MCLK_x inputs using SMA connector J216. The default BOM configuration allows for a 3.3V single ended CMOS signal to be applied to SMA connector J216 with the monitor clock input set to differential using the PPR6 biasing jumpers. | ||
Line 80: | Line 83: | ||
|PPR3 |P414-P416 | |PPR3 |P414-P416 | ||
|PPR4 |P418-P420 | |PPR4 |P418-P420 | ||
- | |PPR5 |P422-P424 | + | |PPR5 |P422-P424 |
|PPR6 |P426-P428 | |PPR6 |P426-P428 | ||
Line 120: | Line 123: | ||
|REFMON | |REFMON | ||
+ | ==== Status LEDs ==== | ||
+ | There are 5 status LEDs: | ||
+ | * DS102 reflects the state of REF_SW output pin: high when a reference switch is in progress | ||
+ | * DS103 reflects the state of REF_ACT output pin: low when REF0 is the active reference and high when REF1 is the active reference | ||
+ | * DS104 reflects the state of REF_FHI output pin: high when the reference frequency is above the upper threshold limit | ||
+ | * DS105 reflects the state of REF_FLO output pin: high when the reference frequency is below the lower threshold limit | ||
+ | * DS106 reflects the state of LD output pin: low when the PLL is unlocked and high when the PLL is locked | ||
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
---- | ---- | ||
- | The quick start section covers simple PLL operation to lock the AD9574 PLL and output | + | The quick start section covers simple PLL operation to lock the [[adi>AD9574|AD9574]] |
- | Table 2 describes a summary of one possible operating mode of the AD9528 | + | **Table 4** describes a summary of one possible operating mode of the [[adi> |
- | **Table | + | **Table |
^ Parameter | ^ Parameter | ||
| Input Frequency and Logic Type | 25MHz, 3.3V CMOS | | | Input Frequency and Logic Type | 25MHz, 3.3V CMOS | | ||
Line 133: | Line 142: | ||
| Reference Doubler Enable/ | | Reference Doubler Enable/ | ||
| Reference Monitor Threshold | | Reference Monitor Threshold | ||
- | | MCLK Input Frequency and Logic Type | 10MHz CMOS | | + | | MCLK Input Frequency and Logic Type | 10MHz 3.3V CMOS |
| Reference Doubler Enable/ | | Reference Doubler Enable/ | ||
- | | OUT0 Frequency and Logic Type | 25MHz CMOS | | + | | OUT0 Frequency and Logic Type | 25MHz 3.3V CMOS |
- | | OUT1 Frequency and Logic Type | 25MHz CMOS | | + | | OUT1 Frequency and Logic Type | 25MHz 3.3V CMOS |
| OUT2 Frequency and Logic Type | 156.25MHz HSTL | | | OUT2 Frequency and Logic Type | 156.25MHz HSTL | | ||
| OUT3 Frequency and Logic Type | 156.25MHz HSTL | | | OUT3 Frequency and Logic Type | 156.25MHz HSTL | | ||
| OUT4 Frequency and Logic Type | 100MHz HSTL | | | OUT4 Frequency and Logic Type | 100MHz HSTL | | ||
| OUT5 Frequency and Logic Type | 125MHz HSTL | | | OUT5 Frequency and Logic Type | 125MHz HSTL | | ||
- | | OUT6 Frequency and Logic Type | 33.33MHz CMOS | + | | OUT6 Frequency and Logic Type | 33.33MHz |
- | Use the following steps to lock the AD9574 PLL to the on board 25MHz XO and output the frequencies listed in **Table | + | Use the following steps to lock the AD9574 PLL to the on board 25MHz XO and output the frequencies listed in **Table |
- Connect the 6V wall supply to P500 with jumpers P501 and P502 set to short pins 1 and 2. | - Connect the 6V wall supply to P500 with jumpers P501 and P502 set to short pins 1 and 2. | ||
- Connect a 10MHz 3.3V CMOS signal to J216 | - Connect a 10MHz 3.3V CMOS signal to J216 | ||
- | - Set the following PPRx states: | + | - Set the following PPRx states |
- | | + | |
- | | + | |
- | | + | |
- | | + | |
- | | + | |
- | | + | |
- | | + | |
- | As long as all jumpers have remained in their default positions, the AD9574 should now be operational. A red LED on the left side of the board, just below the round electrolytic capacitors, | + | The <fc #FF0000>red</ |