This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:ad9546-user-guide [04 Dec 2020 16:08] Shane Lambeth [Front Panel] |
resources:eval:ad9546-user-guide [03 Feb 2021 23:10] Petre Minciunescu [EVALUATION BOARD HARDWARE] |
||
---|---|---|---|
Line 51: | Line 51: | ||
{{:resources:eval:ad9546_eval_board_top.jpg?400|}} | {{:resources:eval:ad9546_eval_board_top.jpg?400|}} | ||
===== General Description ===== | ===== General Description ===== | ||
- | The AD9546 Evaluation Board is a compact, easy-to-use platform for evaluating all features of the [[www.analog.com/AD9546|AD9546]] multiple input, 10-Output, Dual Channel, Numeric Clock Synchronizer. | + | The AD9546 Evaluation Board is a compact, easy-to-use platform for evaluating all features of the [[adi>AD9546]] multiple input, 10-Output, Dual Channel, Numeric Clock Synchronizer. |
The AD9546 supports existing and emerging International Telecommunications Union (ITU) standards for the delivery of frequency, phase, and time of day over service provider packet networks, including ITU-G.8262, ITU-T G.812, ITU-T G.813, ITU-T G.823, ITU-T G.824, ITU-T G.825, and ITU-T G.8273.2. | The AD9546 supports existing and emerging International Telecommunications Union (ITU) standards for the delivery of frequency, phase, and time of day over service provider packet networks, including ITU-G.8262, ITU-T G.812, ITU-T G.813, ITU-T G.823, ITU-T G.824, ITU-T G.825, and ITU-T G.8273.2. | ||
Line 59: | Line 59: | ||
===== EVALUATION BOARD HARDWARE ===== | ===== EVALUATION BOARD HARDWARE ===== | ||
- | The following instructions are for setting up the physical connections to the [[www.analog.com/EVAL-AD9546|AD9546/PCBZ]] Evaluation Board. The user must install the Evaluation Software prior to connecting the Evaluation Board for the first time. | + | The following instructions are for setting up the physical connections to the AD9546/PCBZ Evaluation Board. The user must install the Evaluation Software prior to connecting the Evaluation Board for the first time. |
The 6 V supply powers the following: | The 6 V supply powers the following: | ||
Line 380: | Line 380: | ||
==== Channel 1 Settings ==== | ==== Channel 1 Settings ==== | ||
In the Front Panel (Figure 2), clicking on Channel 1 section launches a window identical with the Channel 0 Settings window (Figure 21). Use Channel 0 Settings section for more information. | In the Front Panel (Figure 2), clicking on Channel 1 section launches a window identical with the Channel 0 Settings window (Figure 21). Use Channel 0 Settings section for more information. | ||
+ | ==== Channel x Settings ==== |