This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ad9545-user-guide [24 Jun 2021 14:32] – [EVALUATION BOARD SOFTWARE] Petre Minciunescu | resources:eval:ad9545-user-guide [10 Aug 2022 20:27] (current) – [Software Installation] Petre Minciunescu | ||
---|---|---|---|
Line 20: | Line 20: | ||
=====Online Resources===== | =====Online Resources===== | ||
Required Software | Required Software | ||
- | * [[http:// | + | * [[https:// |
* AD9545 ACE Plug-in Module: {{ : | * AD9545 ACE Plug-in Module: {{ : | ||
* Please only use ACE Software Version 1.10.2671.1118. Do not update it to newer versions of ACE as they are not tested with the AD9545 plug-in module | * Please only use ACE Software Version 1.10.2671.1118. Do not update it to newer versions of ACE as they are not tested with the AD9545 plug-in module | ||
Line 120: | Line 120: | ||
^ Serial Protocol ^ Slave Address ^ Jumper P605, Top/ | ^ Serial Protocol ^ Slave Address ^ Jumper P605, Top/ | ||
| SPI | N/A | Jumpers removed | SCLK | SDIO | | | SPI | N/A | Jumpers removed | SCLK | SDIO | | ||
- | | SPI | N/A | 7-8 / 4-5 / 1-2 | SCLK | SDIO | | + | | SPI | N/A | 2-3, others do not matter| SCLK | SDIO | |
- | | I²C | 0x48 | 7-8 / 4-5 / 2-3 | SCL | SDA | | + | | I²C | 0x48 | 8-9 / 5-6 / 1-2 | SCL | SDA | |
- | | I²C | 0x49 | 7-8 / 5-6 / 2-3 | SCL | SDA | | + | | I²C | 0x49 | 8-9 / 4-5 / 1-2 | SCL | SDA | |
- | | I²C | 0x4A | 8-9 / 4-5 / 2-3 | SCL | SDA | | + | | I²C | 0x4A | 7-8 / 5-6 / 1-2 | SCL | SDA | |
- | | I²C | 0x4B | 8-9 / 5-6 / 2-3 | SCL | SDA | | + | | I²C | 0x4B | 7-8 / 4-5 / 1-2 | SCL | SDA | |
\\ | \\ | ||
\\ | \\ | ||
Line 141: | Line 141: | ||
- Follow the section 2.1, installation guide, of the ACE User Guide to completion. | - Follow the section 2.1, installation guide, of the ACE User Guide to completion. | ||
- Launch the ACE application prior to installing ACE Plug-ins. This creates the directories used by the ACE Plug-in installers. | - Launch the ACE application prior to installing ACE Plug-ins. This creates the directories used by the ACE Plug-in installers. | ||
- | - Download and install the latest AD9545 ACE Plug-ins: | + | - Download and install the latest AD9545 ACE Plug-ins: |
+ | (Note that there are a total of four plug-ins that must be installed. | ||
==== General Operation ==== | ==== General Operation ==== |