This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:ad9545-user-guide [21 Feb 2018 17:37] – [Known Issues] Paul Kern | resources:eval:ad9545-user-guide [03 Jan 2021 22:12] – fix links Robin Getz | ||
---|---|---|---|
Line 20: | Line 20: | ||
=====Online Resources===== | =====Online Resources===== | ||
Required Software | Required Software | ||
- | * [[http://www.analog.com/ | + | * [[http://swdownloads.analog.com/ |
* [[ftp:// | * [[ftp:// | ||
+ | * Please only use ACE Software Version 1.10.2671.1118. Do not update it to newer versions of ACE as they are not tested with the AD9545 plug-in module | ||
Documents Needed | Documents Needed | ||
- | * [[http:// | + | * [[adi>media/ |
- | * [[http:// | + | * [[adi>media/ |
* [[http:// | * [[http:// | ||
\\ | \\ | ||
Line 136: | Line 137: | ||
Use the following instructions to set up the AD9545 evaluation board software.\\ | Use the following instructions to set up the AD9545 evaluation board software.\\ | ||
Do not connect the evaluation board until the software installation is complete. | Do not connect the evaluation board until the software installation is complete. | ||
- | - Download and install ACE [[http://www.analog.com/ | + | - Download and install ACE Version 1.10.2671.1118 |
- Follow the section 2.1, installation guide, of the ACE User Guide to completion. | - Follow the section 2.1, installation guide, of the ACE User Guide to completion. | ||
- Launch the ACE application prior to installing ACE Plug-ins. This creates the directories used by the ACE Plug-in installers. | - Launch the ACE application prior to installing ACE Plug-ins. This creates the directories used by the ACE Plug-in installers. | ||
Line 305: | Line 306: | ||
The left hand section of the Start View also exposes the ability to create and open sessions as well as maintaining a list of recent sessions that may be directly opened. | The left hand section of the Start View also exposes the ability to create and open sessions as well as maintaining a list of recent sessions that may be directly opened. | ||
==== Known Issues ==== | ==== Known Issues ==== | ||
- | - The AD9545 plug-in may not work correctly with latest version of ACE. If that happens, notify ADI immediately. While the issue is being resolved, an older version of ACE can be downloaded here: [[http:// | + | - Please only use ACE Software Version 1.10.2671.1118 that can be downloaded here: [[http:// |
===== EVALUATION BOARD QUICK START USING A SESSION FILE ===== | ===== EVALUATION BOARD QUICK START USING A SESSION FILE ===== | ||