Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:ad9544-user-guide [16 Jun 2021 21:21] – [Online Resources] Petre Minciunescu | resources:eval:ad9544-user-guide [24 Jun 2021 14:33] – [EVALUATION BOARD SOFTWARE] Petre Minciunescu |
---|
* AD9544 ACE Plug-in Module: {{ :resources:eval:board.ad9544.1.1.8.zip |}} | * AD9544 ACE Plug-in Module: {{ :resources:eval:board.ad9544.1.1.8.zip |}} |
* Please only use ACE Software version 1.10.2671.1118. Do not update it to newer versions as they are not tested with the AD9544 plug-in module | * Please only use ACE Software version 1.10.2671.1118. Do not update it to newer versions as they are not tested with the AD9544 plug-in module |
| * Install ACE first. Unzip the plug-in. Double click on it to have it installed |
Documents Needed | Documents Needed |
* [[adi>media/en/technical-documentation/data-sheets/AD9544.pdf|AD9544 Datasheet]] | * [[adi>media/en/technical-documentation/data-sheets/AD9544.pdf|AD9544 Datasheet]] |
===== EVALUATION BOARD SOFTWARE ===== | ===== EVALUATION BOARD SOFTWARE ===== |
---- | ---- |
The AD9544 evaluation software allows the user to control the full functionality of the AD9544 through SPI (or I²C) communication with the evaluation board. The AD9544 evaluation software is implemented as a component plug-in in ADI’s [[resources:tools-software:ace|Analysis | Control | Evaluation (ACE) Software]] desktop software. ACE allows the evaluation of control of multiple evaluation systems from across ADI’s product portfolio and is designed to educate the user in the functional operation of the component. The [[resources:tools-software:ace|ACE wiki page]] contains system requirement and prerequisite information as well as links to the most recent installer and user guide. The ACE user guide contains detailed information concerning all current aspects of the ACE environment. Much of that information will not be described in this document, but some main ACE operational points relevant to component level functionality will be described. It is highly recommended to review the ACE user guide to discover the myriad capabilities and offerings the ACE environment provides to the user. | The AD9544 evaluation software allows the user to control the full functionality of the AD9544 through 3-wire SPI communication with the evaluation board. The AD9544 evaluation software is implemented as a component plug-in in ADI’s [[resources:tools-software:ace|Analysis | Control | Evaluation (ACE) Software]] desktop software. ACE allows the evaluation of control of multiple evaluation systems from across ADI’s product portfolio and is designed to educate the user in the functional operation of the component. The [[resources:tools-software:ace|ACE wiki page]] contains system requirement and prerequisite information as well as links to the most recent installer and user guide. The ACE user guide contains detailed information concerning all current aspects of the ACE environment. Much of that information will not be described in this document, but some main ACE operational points relevant to component level functionality will be described. It is highly recommended to review the ACE user guide to discover the myriad capabilities and offerings the ACE environment provides to the user. |
==== Software Installation ==== | ==== Software Installation ==== |
Use the following instructions to set up the AD9544 evaluation board software.\\ | Use the following instructions to set up the AD9544 evaluation board software.\\ |