Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:ad9508-user-guide [14 Feb 2013 21:13] – added lines Kyle Slightom | resources:eval:ad9508-user-guide [05 Apr 2013 18:46] – [Software Installation] updated information on software files Yuet Ng |
---|
====== AD9508 Evaluation Board User Guide ====== | ====== AD9508 Evaluation Board User Guide ====== |
| <WRAP column 30%> |
| =====Features===== |
| * Simple power connection using 6 V wall adapter and on-board LDO voltage regulators |
| * 8 ac-coupled single-ended SMA output connectors \\ (4 differential paths) |
| * 2 ac-coupled single-ended SMA connectors for reference input |
| * Pin selectable options for the following: |
| * 2.5 V or 3.3 V operation |
| * SPI/I<sup>2</sup>C or Sx pin programmable |
| * OUT0 through OUT3 divide value |
| * OUT0 through OUT3 logic type |
| * Input logic type |
| * USB connection to PC |
| * Microsoft Windows®-based evaluation software with simple graphical user interface (supports 64-bit versions of Windows) |
| </WRAP> |
| <WRAP column 10%> |
| \\ |
| </WRAP> |
| <WRAP column 30%> |
| =====Equipment Needed===== |
| * Reference oscillator or signal generator |
| * Other evaluation board to be clocked or test equipment |
| * Converters, DDS, transceivers |
| * Oscilloscope, spectrum analyzer, phase noise analyzer |
| * SMA cables (50 Ω) |
| * 6 V wall supply (provided) |
| * USB cable (provided) |
| |
===== GENERAL DESCRIPTION ===== | =====Online Resources===== |
| Required Software |
| * [[adi>eval-ad9508|AD9508 evaluation board software]] |
| Documents Needed |
| * [[adi>static/imported-files/data_sheets/AD9508.pdf|AD9508 data sheet]] |
| </WRAP> |
| |
| |
| ===== General Description ===== |
---- | ---- |
The [[adi>AD9508|AD9508]] evaluation board is a compact, easy-to-use platform for evaluating all features of the [[adi>AD9508|AD9508]]. This user guide focuses on the [[adi>AD9508|AD9508]] evaluation board and software. The [[adi>AD9508|AD9508]] is a high performance 1:4 flexible clock buffer. Each output has a programmable divider that may be set via SPI/I2C or S-pin strapping. The [[adi>AD9508|AD9508]] features both 2.5 V and 3.3V operation. For convenience, detailed information from the AD9508 data sheet has been included here. Use this user guide in conjunction with the [[adi>AD9508|AD9508]] data sheet and software documentation available at www.analog.com. | The [[adi>AD9508|AD9508]] evaluation board is a compact, easy-to-use platform for evaluating all features of the [[adi>AD9508|AD9508]]. This user guide focuses on the [[adi>AD9508|AD9508]] evaluation board and software. The [[adi>AD9508|AD9508]] is a high performance 1:4 flexible clock buffer. Each output has a programmable divider that can be set via SPI/I<sup>2</sup>C programming or Sx pin strapping. The [[adi>AD9508|AD9508]] features both 2.5 V and 3.3 V operation. For convenience, detailed information from the [[adi>AD9508|AD9508]] data sheet has been included here. Use this guide in conjunction with the [[adi>AD9508|AD9508]] data sheet and software documentation available at www.analog.com. |
| |
<WRAP centeralign> | <WRAP centeralign> |
{{:resources:eval:user-guides:ad9508:9508_evb_cropped.png?direct&800|}} | {{ :resources:eval:user-guides:ad9508:9508_evb_cropped.png?710x353 }} |
\\ | \\ |
**Figure 1. AD9508/PCBZ** | <wrap centeralign>//Figure 1. AD9508/PCBZ //</wrap> |
</WRAP> | </WRAP> |
| |
<WRAP column 48%> | ===== Evaluation Board Hardware ===== |
<WRAP round box> | |
//**FEATURES**// | |
*Simple power connection using 6V wall adapter and on-board LDO voltage regulators | |
*8 ac-coupled single ended SMA output connectors (4 differential paths) | |
*2 ac- coupled single ended SMA connectors for reference input | |
*Pin selectable options for the following: | |
*2.5V or 3.3V operation | |
*SPI/I2C or S-pin programmable | |
*OUT0 through OUT3 divide value | |
*OUT0 through OUT3 logic type | |
*Input logic type | |
*USB connection to PC | |
*Microsoft Windows-based evaluation software with simple graphical user interface(supports 64-bit versions of Windows) | |
</WRAP></WRAP> | |
| |
<WRAP column 48%> | |
<WRAP round box> | |
//**APPLICATIONS**// | |
* Low jitter, low phase noise clock distribution | |
* Clocking high speed ADCs, DACs, DDSs, DDCs, DUCs, MxFEs | |
* High performance wireless transceivers | |
* High performance instrumentation | |
* Broadband infrastructure | |
\\ \\ \\ \\ \\ \\ \\ \\ \\ \\ | |
</WRAP></WRAP> | |
| |
===== EVALUATION BOARD HARDWARE ===== | |
---- | ---- |
The following instructions are for setting up the physical connections to the AD9508/PCBZ evaluation board. | The following instructions are for setting up the physical connections to the AD9508/PCBZ evaluation board. |
Before connecting the evaluation board to a PC for the first time, the user must install the evaluation software prior to connecting the evaluation board. | Before connecting the evaluation board to a PC for the first time, the user must install the evaluation software. |
| |
=== Power and PC Connections === | ==== Power and PC Connections ==== |
- Install the AD9508 evaluation software, uninstall prior versions of the software before installation updates. Administrative privileges are required for installation. The 64-bit versions of Windows® are supported. | - Before installing the [[adi>AD9508|AD9508]] evaluation software, uninstall prior versions of the software. Administrative privileges are required for installation. The 64-bit versions of Windows are supported. |
- Connect the 6V wall power supply to the main power connector labeled P500. | - Connect the 6 V wall power supply to the main power connector labeled P500. |
- Connect the USB cable to the evaluation board and the computer. The red LED labeled CR300 on the AD9508 evaluation board should illuminate. | - Connect the USB cable to the evaluation board and the computer. The red LED labeled CR300 on the AD9508 evaluation board should illuminate. |
- If the **Found New Hardware Wizard** window automatically appears when the evaluation board is connected, select **Install the software automatically** and click **Next**. The **Found New Hardware Wizard** window may appear twice, and a system restart may be required. | - If the **Found New Hardware Wizard** window appears when the evaluation board is connected, select **Install the software automatically** and click **Next**. The **Found New Hardware Wizard** window may appear twice, and a system restart may be required. |
- Once the driver software has installed, the red LED labeled CR301 will blink. | - After the driver software has installed, the red LED labeled CR301 blinks. |
| |
=== Signal Connections === | ==== Signal Connections ==== |
To connect signals, connect a signal generator to the J200(CLKIN) SMA connector. By default, the CLKIN input is connected to a balun for single ended to differential conversion. This path is differentially terminated to 100Ω and ac-coupled into the AD9508 reference inputs. An amplitude setting of 0 dBm to 6 dBm is fine. The CLKINB SMA input is grounded by default. To input a differential signal, the user must remove balun (T200) and resistor R221 and place resistors R209 and R210 with 0Ω. Connect an oscilloscope, spectrum analyzer, or other lab equipment to any of the J209 to J216 SMA clock OUT connectors on the edge of the board. OUT0 through OUT3 are ac-coupled outputs differentially terminated to 100Ω. | To connect signals, connect a signal generator to the J200 (CLKIN) SMA connector. By default, the CLKIN input is connected to a balun for single-ended to differential conversion. This path is differentially terminated to 100 Ω and ac-coupled into the [[adi>AD9508|AD9508]] reference inputs. An amplitude setting of 0 dBm to 6 dBm is fine. The CLKIN_B SMA input is grounded by default. To input a differential signal, the user must remove Balun T200 and Resistor R221, and place Resistors R209 and R210 with 0 Ω. Connect an oscilloscope, spectrum analyzer, or other lab equipment to any of the J209 to J216 SMA clock OUTx connectors on the edge of the board. OUT0 through OUT3 are ac-coupled outputs differentially terminated to 100 Ω. |
| |
=== Pin Programming and Jumper Settings === | ==== Pin Programming and Jumper Settings ==== |
**Jumper P507** allows the user to select between 2.5V and 3.3V operation. \\ \\ | |
**Jumper P100** allows the user to select between differential (LVDS/ PECL/ etc) and CMOS input logic types.\\ \\ | |
**Jumper P101** allows the user to select which programming method (SPI/I2C/S-pin programming) will be used by the AD9508. Placing no jumper defaults the part to use SPI. I2C is not currently supported with the evaluation board software. When pin programming is selected, S-pins S0 through S5 are used to determine various divider ratios and output modes for each of the AD9508s outputs. Using the S-pins to program the part gives the user limited control of each channel divider ratio and no control of phase offset. Please refer to the [[adi>AD9508|AD9508 datasheet]] for a complete overview regarding the use of the part with S-pin programming.\\ \\ | |
| |
**Jumpers P102, P106, P110, and P114** connect and disconnect S-pins S0 through S3 to a SPI/I2C line. These need to be set with respect to the setting of **P101**. Table 1 describes the proper placement of these jumpers. \\ \\ | ===Jumpers P507, P100, and P101=== |
| * Jumper P507 allows the user to select between 2.5 V and 3.3 V operation. \\ \\ |
| * Jumper P100 allows the user to select between differential and single-ended inputs.\\ \\ |
| * Jumper P101 allows the user to select the programming method (SPI/I<sup>2</sup>C/Sx pin programming) to be used by the [[adi>AD9508|AD9508]]. Placing no jumper defaults the part to use the SPI. I<sup>2</sup>C programming is not currently supported with the evaluation board software. When pin programming is selected, Pin S0 through Pin S5 are used to determine various divider ratios and output modes for each of the [[adi>AD9508|AD9508]] outputs. Using the Sx pins to program the part gives the user limited control of each channel divider ratio and no control of phase offset. Refer to the [[adi>AD9508|AD9508]] data sheet for a complete overview regarding the use of the part with Sx pin programming. |
| |
<WRAP column 22%> | ===Jumpers P102, P106, P110, and P114=== |
. | * Jumpers P102, P106, P110, and P114 connect and disconnect Pin S0 through Pin S3 to a SPI/I<sup>2</sup>C line. These need to be set with respect to the setting of P101. Table 1 describes the proper placement of these jumpers. \\ \\ |
</WRAP> | |
| |
<WRAP centeralign> | |
|< 50% 20% 40% 80% >| | |
| **Programming Pins** | **Jumper Placement vs. Programming Method** || | |
| ::: ^ SPI or I2C ^ Pin Strapping ^ | |
^ S0 | P102 = SCLK | P102 = S0P | | |
^ S1 | P106 = SDIO | P106 = S1P | | |
^ S2 | P110 = CSB | P110 = S2P | | |
^ S3 | P114 = SDO | P114 = S3P | | |
| |
**Table 1. P102, P106, P110, and P114 Jumper Settings with Respect to Jumper P101 Setting** | **Table 1. P102, P106, P110, and P114 Jumper Settings with Respect to Jumper P101 Setting**\\ |
</WRAP><WRAP clear></WRAP> | ^Programming Pins^ Jumper Placement vs. Programming Method ^ ^ |
| ^::: ^ SPI or I<sup>2</sup>C ^ Pin Strapping ^ |
| |S0 |P102 = SCLK |P102 = S0P | |
| |S1 |P106 = SDIO |P106 = S1P | |
| |S2 |P110 = <m>overline{CS}</m> |P110 = S2P | |
| |S3 |P114 = SDO |P114 = S3P | |
| |
| |
There are two more jumpers allocated for each S-pin that are used to obtain all 8 divider settings (for S-pins 0 through 3) and to select between logic types (S-pins 4 and 5). The first jumper is used to pull the S-pin up to VDD or down to GND. The second jumper is used to select one of the four resistor settings on the evaluation board. Table 2 describes the possible divider and output mode settings when in S-pin programming mode. Table 3 lists the jumper label associated with each divider ratio and driver mode setting.\\ | There are two more jumpers allocated for each Sx pin that are used to obtain all eight divider settings (for Pin S0 through Pin S3) and to select between logic types (Pin S4 and Pin S5). The first jumper is used to pull the Sx pin up to VDD or down to GND. The second jumper is used to select one of the four resistor settings on the evaluation board. Table 2 describes the possible divider and output mode settings when in Sx pin programming mode. Table 3 lists the jumper label associated with each divider ratio and driver mode setting.\\ |
| |
<WRAP centeralign> | **Table 2. Divider Ratio and Driver Mode Table for S0, S1, S2, S3, S4, and S5 Pins (Driver Modes Are Listed in the Order of CH1/CH2 or CH3/CH4)** |
|< 100% 8% 8% 8% 8% 8% 8% 8% 8% 8% 22% >| | ^ Programming Pins ^ Sx Pin Settings (0 Through 7) vs. Resistor Value vs. Divide Value and Logic Type ^^^^^^^^ Description ^ |
| **Programming Pins** | **S-Pin Settings (0 through 7) vs. Resistor Value vs. Divide Value and Logic Type** |||||||| **Description** | | ^ ::: ^0 = 820 Ω Pulled to GND ^1 = 1.8 kΩ Pulled to GND ^2 = 3.9 kΩ Pulled to GND ^3 = 8.2 kΩ Pulled to GND ^4 = 820 Ω Pulled to VDD ^5 = 1.8 kΩ Pulled to VDD ^6 = 3.9 kΩ Pulled to VDD ^7 = 8.2 kΩ Pulled to VDD ^ ::: ^ |
| ::: ^ 0 = 820Ω Pulled to GND ^ 1 = 1.8kΩ Pulled to GND ^ 2 = 3.9kΩ Pulled to GND ^ 3 = 8.2kΩ Pulled to GND ^ 4 = 820Ω Pulled to VDD ^ 5 = 1.8kΩ Pulled to VDD ^ 6 = 3.9kΩ Pulled to VDD ^ 7 = 8.2kΩ Pulled to VDD ^ ::: | | |S0 |÷1 |÷2 |÷3 |÷4 |÷5 |÷6 |÷8 |÷16 |S0 is assigned to the CH0 divider ratio only | |
^ S0 | ÷1 | ÷2 | ÷3 | ÷4 | ÷5 | ÷6 | ÷8 | ÷16 |S0 is assigned to the CH0 divider ratio only | | |S1 |÷1 |÷2 |÷3 |÷4 |÷5 |÷6 |÷8 |÷16 |S1 is assigned to the CH1 divider ratio only | |
^ S1 | ÷1 | ÷2 | ÷3 | ÷4 | ÷5 | ÷6 | ÷8 | ÷16 |S1 is assigned to the CH1 divider ratio only | | |S2 |÷1 |÷2 |÷3 |÷4 |÷5 |÷6 |÷8 |÷16 |S2 is assigned to the CH2 divider ratio only | |
^ S2 | ÷1 | ÷2 | ÷3 | ÷4 | ÷5 | ÷6 | ÷8 | ÷16 |S2 is assigned to the CH2 divider ratio only | | |S3 |÷1 |÷2 |÷3 |÷4 |÷5 |÷6 |÷8 |÷16 |S3 is assigned to the CH3 divider ratio only | |
^ S3 | ÷1 | ÷2 | ÷3 | ÷4 | ÷5 | ÷6 | ÷8 | ÷16 |S3 is assigned to the CH3 divider ratio only | | |S4 |HSTL/HSTL |HSTL/LVDS |HSTL/ Disable |LVDS/HSTL |LVDS/ LVDS |LVDS/ Disable |Disable/ HSTL |Disable/ Disable |S4 is assigned to CH0/CH1 to select their output logic types | |
^ S4 | HSTL/ HSTL | HSTL/ LVDS | HSTL/ DISABLE | LVDS/ HSTL | LVDS/ LVDS | LVDS/ DISABLE | DISABLE/ HSTL | DISABLE/ DISABLE |S4 is assigned to CH0/CH1 to select their output logic types | | |S5 |HSTL/HSTL |HSTL/LVDS |HSTL/ Disable |LVDS/HSTL |LVDS/ LVDS |LVDS/ Disable |Disable/ HSTL |Disable/ Disable |S5 is assigned to CH2/CH3 to select their output logic types | |
^ S5 | HSTL/ HSTL | HSTL/ LVDS | HSTL/ DISABLE | LVDS/ HSTL | LVDS/ LVDS | LVDS/ DISABLE | DISABLE/ HSTL | DISABLE/ DISABLE |S5 is assigned to CH2/CH3 to select their output logic types | | |
**Table 2. Divider Ratio and Driver Mode Table for S0/S1/S2/S3/S4/S5 Pins***\\ | |
//*Driver modes are listed in the order of CH1/CH2 or CH3/CH4// | |
</WRAP> | |
| |
<WRAP clear></WRAP> | **Table 3. Evaluation Board S-pin Jumper Labels** \\ |
| ^Programming Pins ^ Evaluation Board Sx Pin Jumper Labels ^^^ |
| ^::: ^ 820 Ω/1.8 kΩ ^ 3.9 kΩ/8.2 kΩ ^ Pull Up to VDD/Pull Down to GND ^ |
| |S0 |P103 |P104 |P105 | |
| |S1 |P107 |P108 |P109 | |
| |S2 |P111 |P112 |P113 | |
| |S3 |P115 |P116 |P117 | |
| |S4 |P118 |P119 |P120 | |
| |S5 |P121 |P122 |P123 | |
| |
<WRAP column 22%> | ===== Evaluation Board Software ===== |
. | |
</WRAP> | |
| |
<WRAP centeralign> | |
|< 50% 10% 30% 30% 30% >| | |
| **Programming Pins** | **Evaluation Board S-Pin Jumper Labels** ||| | |
| ::: ^ 820Ω / 1.8kΩ ^ 3.9kΩ / 8.2kΩ ^ Pull to VDD / Pull to GND ^ | |
^ S0 | P103 | P104 | P105 | | |
^ S1 | P107 | P108 | P109 | | |
^ S2 | P111 | P112 | P113 | | |
^ S3 | P115 | P116 | P117 | | |
^ S4 | P118 | P119 | P120 | | |
^ S5 | P121 | P122 | P123 | | |
**Table 3. Evaluation Board S-pin Jumper Labels** | |
</WRAP><WRAP clear></WRAP> | |
| |
===== EVALUATION BOARD SOFTWARE ===== | |
---- | ---- |
The AD9508 evaluation software allows the user to control the full functionality of the AD9508 through SPI/I2C communication on the evaluation board. Use the following instructions to set up the evaluation board software. | The [[adi>AD9508|AD9508]] evaluation software allows the user to control the full functionality of the [[adi>AD9508|AD9508]] through SPI/I<sup>2</sup>C communication on the evaluation board. Use the following instructions to set up the evaluation board software. |
| |
| |
=== Software Installation === | ==== Software Installation ==== |
Do not connect the evaluation board until the software installation is complete. | Do not connect the evaluation board until the software installation is complete. |
- The latest evaluation software and documentation can be downloaded from http://www.analog.com/en/clock-and-timing/clock-generation-and-distribution/ad9508/products/product.html. | - The latest evaluation software and documentation can be downloaded from [[adi>eval-ad9508|http://www.analog.com/eval-ad9508]]. |
- On the AD9508 Evaluation Board page, double-click AD9508Eval_Setup1.1.0.exe. (Note that the website may have a newer version.) Follow the installation instructions. | - On the [[adi>eval-ad9508|AD9508 evaluation board page]], under **Software and Tools,** click **Evaluation Board AD9508 - Web Install** or **Evaluation Board AD9508 - Full Install**. The full version of the installer is a much larger file that contains the entire standalone installation for the .NET framework, and it does not require an Internet connection. The web installer contains an executable that can download the .NET framework, but this does require an internet connection. However, if the .NET framework has already been installed, an Internet connection is not required to proceed. |
| - Follow the installation instructions. |
| |
| |
=== Running the Software === | ==== Running the Software ==== |
Power up and connect the evaluation board to the PC. See the Evaluation Board Hardware section for details on the various connectors on the evaluation board. | Power up and connect the evaluation board to the PC. See the Evaluation Board Hardware section for details on the various connectors on the evaluation board. |
- Windows® may automatically detect the evaluation board after the board is first plugged in. Allow Windows® to install the device drivers.\\ <WRAP centeralign> | - Windows may automatically detect the evaluation board after the board is first plugged in. Allow Windows to install the device drivers.<WRAP centeralign> {{:resources:eval:user-guides:ad9508:figure2_device_hardware_instal.png?direct&450}}\\ |
{{:resources:eval:user-guides:ad9508:figure2_device_hardware_instal.png?direct&450}} | //Figure 2. Device Hardware Installation//</WRAP> |
| - Double-click **AD9508 Evaluation Software** to run the AD9508 software. If the evaluation board was found by the software, the lower left corner of the Main Window (see Figure 4) displays **AD9508 Evaluation Board** in green. If the evaluation board was not found, the lower left corner of the screen displays **No Hardware Connected!** in red. |
| - If the evaluation board is found, proceed to the [[resources/eval/ad9508-user-guide#evaluation_software_components|Evaluation Software Components]] section for details about running the software. If the evaluation board is not found, click **File** > **Select Hardware**. Select the appropriate [[adi>ad9508|AD9508]] evaluation board connected and click **OK** (see Figure 3). \\ <WRAP centeralign> |
| {{:resources:eval:user-guides:ad9508:figure3_select_hardware_window.png?direct|}} |
\\ | \\ |
**Figure 2. Device Hardware Installation** | //Figure 3. Select Hardware Window// |
</WRAP> | </WRAP> |
- Double-click **AD9508 Evaluation Software** to run the AD9508 software. If the evaluation board was found by the software, the lower left hand corner of the Main Window (shown in Figure 4) will read **“AD9508 Evaluation Board”** in green. If the evaluation board was not found, the lower left hand corner of the screen will read **“No Hardware Connected!”** in red. | |
- If the evaluation board is found, proceed to the Evaluation Software Components section for details about running the software. If the evaluation board is not found, click File > Select Hardware. Select the appropriate AD9508 evaluation board connected and press OK. \\ <WRAP centeralign> | |
{{:resources:eval:user-guides:ad9508:figure3_select_hardware_window.png?direct|}} | |
\\ | \\ |
**Figure 3. Select Hardware Window** | The bottom left corner of the main window should now display **AD9508 Evaluation Board** in green. Alternatively, you can use the software in standalone mode. The standalone mode is useful for verifying register settings for a given setup. See the [[resources/eval/ad9508-user-guide#evaluation_software_components|Evaluation Software Components]] section for a description of the evaluation software features. |
</WRAP> | |
| |
The bottom left corner of the main window should now read AD9508 Evaluation Board in green. Alternatively, you can use the software in standalone mode. The standalone mode is useful for verifying register settings for a given setup. See the **Evaluation Software Components** section for a description of the evaluation software features. | |
| |
===== EVALUATION SOFTWARE COMPONENTS ===== | ===== Evaluation Software Components ===== |
---- | ---- |
=== Main Window === | ==== Main Window ==== |
<WRAP centeralign> | <WRAP centeralign> |
{{:resources:eval:user-guides:ad9508:figure4_eval_softwaremenu.png?direct}} | {{:resources:eval:user-guides:ad9508:figure4_eval_softwaremenu.png?direct}} |
\\ | \\ |
**Figure 4. Evaluation Software Main Window** | //Figure 4. Evaluation Software Main Window// |
</WRAP> | </WRAP> |
| |
The AD9508 evaluation software is composed of subsections that correspond to the major functional blocks of the AD9508. These subsections are listed in the following sections of the user guide. Some of the major subsections have a dedicated window that allows the user to edit the register settings associated with the functional block. A functional block window can be accessed by clicking the appropriate button under each block. Some of the functional blocks have editable text areas that can be accessed and altered without opening each functional block window. Altering these text areas changes the settings found in the various block windows and immediately loads the change into the evaluation board. Conversely, editing the settings within a block will be reflected in a text area. | The [[adi>ad9508|AD9508]] evaluation software is composed of subsections that correspond to the major functional blocks of the [[adi>ad9508|AD9508]]. These subsections are described in the following sections of the user guide. Some of the subsections have dedicated windows that allows the user to edit the register settings associated with a functional block. For example, the output distribution functional block window can be accessed by clicking the **DIST REGISTER** button. Some of the functional blocks have editable text areas that can be accessed and altered without opening each functional block window. Altering these text areas changes the settings found in the various block windows and immediately loads the change into the evaluation board. Conversely, edits to the settings within a block are reflected in the respective text area. |
\\ \\ | \\ \\ |
After clicking **LOAD**, the settings from that subwindow are loaded to the evaluation board. When editing a text box within the main window, **ENTER** must be pressed before a change is saved and loaded into the evaluation board. | After clicking **Load**, the settings from that subwindow are loaded to the evaluation board. When editing a text box within the main window, the **ENTER** key must be pressed before a change is saved and loaded into the evaluation board. |
| |
=== Input Receiver === | ==== Input Receiver ==== |
The Input Receiver section allows the user to select between single ended and differential operation. By clicking on the MUX symbol within the block, the software will highlight which path is active. | The input receiver (**INPUT RECV**) section allows the user to select between single-ended and differential operation. Click the mux symbol within the block to highlight the active path (see Figure 5). The left image in Figure 5 shows the default differential operation of the input receiver. The right image shows single-ended operation.<WRAP centeralign> |
<WRAP centeralign> | |
{{:resources:eval:user-guides:ad9508:figure5a_inputreceiver_high.png?direct&150|}} | {{:resources:eval:user-guides:ad9508:figure5a_inputreceiver_high.png?direct&150|}} |
{{:resources:eval:user-guides:ad9508:figure5b_inputreceiver_low.png?direct&155|}} | {{:resources:eval:user-guides:ad9508:figure5b_inputreceiver_low.png?direct&155|}} |
\\ | \\ |
**Figure 5. Input Receiver Section***\\ | //Figure 5. Input Receiver Section\\ |
//*The left image shows default differential operation of the input receiver. The right image shows single ended operation.// | Left Image: Default Differential Operation of Input Receiver; Right Image: Single-Ended Operation// |
</WRAP> | </WRAP> |
| |
=== Output Distribution === | ==== Output Distribution ==== |
The **Output Distribution** section allows the user to alter divide ratios and phase offsets for each output of the AD9508. Each divide and phase block can be edited by typing the preferred value within the block followed by **ENTER**. Once enter is pressed, the values are loaded into the evaluation board. The phase offset blocks accept the prefixes u (micro), p (pico), and n (nano). Phase offset is limited to one half of the period of the input clock rate. Each divider supports integer divide values from 1 to 1024. If the typed value is not realizable in the current configuration, the software will automatically round to the nearest possible solution. The output distribution section is shown in Figure 6. | The output distribution (**OUTPUT DIST**) section allows the user to alter divide ratios and phase offsets for each output of the [[adi>ad9508|AD9508]]. Each divide and phase block can be edited by typing the preferred value within the block, and then pressing the **ENTER** key. When **ENTER** is pressed, the values are loaded into the evaluation board. The phase offset blocks accept the u (micro), p (pico), and n (nano) prefixes. Phase offset is limited to one half of the period of the input clock rate. Each divider supports integer divide values from 1 to 1024. If the typed value is not realizable in the current configuration, the software automatically rounds to the nearest possible solution. The output distribution section is shown in Figure 6. |
| |
<WRAP centeralign> | <WRAP centeralign> |
{{:resources:eval:user-guides:ad9508:figure6_outputdist.png?direct|}} | {{:resources:eval:user-guides:ad9508:figure6_outputdist.png?direct|}} |
\\ | \\ |
**Figure 6. Output Distribution Section** | //Figure 6. Output Distribution Section//</WRAP> |
</WRAP> | |
\\ | \\ |
Pressing the DIST REGISTERS button at the bottom of the Output Distribution section allows the user to access all of the distribution register settings in the Distribution Settings Window. \\ | Clicking the **DIST REGISTERS** button at the bottom of the output distribution section allows the user to access all of the distribution register settings in the **Distribution Settings** window (see Figure 7). \\ |
| |
<WRAP centeralign> | <WRAP centeralign> |
{{:resources:eval:user-guides:ad9508:figure7_distsettings.png?direct|}} | {{:resources:eval:user-guides:ad9508:figure7_distsettings.png?direct|}} |
\\ | \\ |
**Figure 7. Distribution Settings Window** | //Figure 7. Distribution Settings Window// |
</WRAP> | </WRAP> |
| |
The Distribution Settings Window consists of four individual tabs for each output channel. Each tab contains controls for each channel divide ratio, phase offset, driver mode, polarity and power down settings. To load any of the settings to the evaluation board changed within the Distribution Settings Window, the user must press the **Load** button. \\ \\ | The **Distribution Settings** window consists of four individual tabs for each output channel. Each tab contains controls for each channel divide ratio, phase offset, driver mode, polarity and power-down settings. To load any of the settings to the evaluation board changed within the **Distribution Settings** window, the user must click the **Load** button. \\ \\ |
The Driver Mode and Polarity settings are altered by selecting one of the values in each drop down tab and pressing the Load button. To power down a channel driver, the appropriate Channel Power Down box must be checked. | The driver mode and polarity settings are altered by selecting one of the values from the respective drop-down box and clicking the **Load** button. To power down a channel driver, the appropriate channel power-down box must be selected. |
| |
=== Operational Controls Window === | ==== Operational Controls Window ==== |
The Operational Controls Window is opened by pressing the CONTROL button at the bottom of the Main Window. This window contains controls for SPI, LDO voltage control, channel power down, sleep mode, and two buttons for Soft Reset and Soft Sync. The Operational Controls Window is shown in Figure 8. | The **Operational Controls** window is opened by clicking the **CONTROL** button at the bottom of the main window. This window contains controls for SPI configuration, LDO voltage control, channel power-down, sleep mode, and two buttons for soft reset and soft sync. The **Operational Controls** window is shown in Figure 8. |
<WRAP centeralign> | <WRAP centeralign> |
{{:resources:eval:user-guides:ad9508:figure8_opcontrolswindow.png?direct|}} | {{:resources:eval:user-guides:ad9508:figure8_opcontrolswindow.png?direct|}} |
\\ | \\ |
**Figure 8. Operational Controls Window** | //Figure 8. Operational Controls Window// |
</WRAP> | </WRAP> |
| |
=== Register Map Window === | ==== Register Map Window ==== |
The **Register Map** window is accessed by pressing the **REG MAP** button at the bottom of the main window. Figure 9 below shows the Register Map Window. | The **Register Map** window is accessed by clicking the **REG MAP** button at the bottom of the main window. Figure 9 shows the **Register Map** window. |
<WRAP centeralign> | <WRAP centeralign> |
{{:resources:eval:user-guides:ad9508:figure9_regmapwindow.png?direct|}} | {{:resources:eval:user-guides:ad9508:figure9_regmapwindow.png?direct|}} |
\\ | \\ |
**Figure 9. Register Map Window** | //Figure 9. Register Map Window// |
</WRAP> | </WRAP> |
| |
The Register Map window contains two tabs. The **All** tab displays all of the registers that can be changed through the AD9508 evaluation software. Each register can be selected by clicking the various blue boxes shown in Figure 9. Register details for the selected register will appear at the bottom of the window. These details include the name of the register, the current register value, and the various bit fields for the register. The **Changed** tab contains all of the registers that have been modified from within the AD9508 evaluation software but not loaded into the evaluation board yet. These same registers are also highlighted in the All tab as they are modified. | The **Register Map** window contains two tabs. The **All** tab displays all of the registers that can be changed through the [[adi>ad9508|AD9508]] evaluation software. Each register can be selected by clicking the various blue boxes shown in Figure 9. Register details for the selected register appears at the bottom of the window. These details include the name of the register, the current register value, and the various bit fields for the register. The **Changed** tab contains all of the registers that have been modified from within the [[adi>ad9508|AD9508]] evaluation software but not loaded into the evaluation board yet. These same registers are also highlighted in the **All** tab as they are modified. |
| |
=== Read All and Write All Buttons === | ==== READ ALL and WRITE ALL Buttons ==== |
The Read All and Write All buttons are located at the bottom of the Main Window. The **Read All** button reads all of the register values currently stored in the chip and transfers them to the evaluation software. The **Write All** button transfers all of the register values currently loaded into the software and writes them to the chip. | The **READ ALL** and **WRITE ALL** buttons are located at the bottom of the main window. The **READ ALL** button reads all of the register values currently stored in the chip and transfers them to the evaluation software. The **WRITE ALL** button transfers all of the register values currently loaded into the software and writes them to the chip. |
| |
=== Reset Button === | ==== Reset Button ==== |
The **Reset Button** is located at the bottom of the Main Window. This button resets the part to its default register settings, which is also reflected in the Main Window. | The **Reset Button** is located at the bottom of the main window. This button resets the part to its default register settings, which is also reflected in the main window. |
| |
=== SYNC Button === | ==== SYNC Button ==== |
===== EVALUATION SOFTWARE MENU ITEMS ===== | The **SYNC** button issues a soft synchronization command, which synchronizes all outputs that are not omitted by the appropriate SYNCMASKx bit. Refer to the [[adi>ad9508|AD9508]] data sheet for more information about the sync command. |
| |
| ===== Evaluation Software Menu Items ===== |
---- | ---- |
<WRAP centeralign> | <WRAP centeralign> |
{{:resources:eval:user-guides:ad9508:figure10_menubar.png?direct&|}} | {{:resources:eval:user-guides:ad9508:figure10_menubar.png?direct&|}} |
\\ | \\ |
**Figure 10. Menu Bar** | //Figure 10. Menu Bar// |
</WRAP> | </WRAP> |
| |
=== File Menu === | ==== File Menu ==== |
The **File** menu includes the following options:\\ | The **File** menu includes the following options:\\ |
| * Load Setup |
| * Save Setup |
| * Select Hardware |
| * Options |
| * Enable Polling |
| * Polling Interval |
| * Exit |
| |
__**Load Setup**__\\ | ===Load Setup=== |
Selecting Load Setup loads a previously saved AD9508 setup file (.stp). A setup file is a text file that contains the AD9508 register setup file, plus any evaluation board settings.\\ | Selecting **Load Setup** loads a previously saved [[adi>ad9508|AD9508]] setup file (.stp). A setup file is a text file that contains the [[adi>ad9508|AD9508]] register setup file, plus any evaluation board settings.\\ |
| |
__**Save Setup**__\\ | ===Save Setup=== |
Selecting Save Setup saves an AD9508 setup file (.stp). A setup file is a text file that contains the AD9508 register settings, plus any evaluation board settings.\\ | Selecting **Save Setup** saves an [[adi>ad9508|AD9508]] setup file (.stp). A setup file is a text file that contains the [[adi>ad9508|AD9508]] register settings, plus any evaluation board settings.\\ |
| |
__**Select Hardware**__\\ | ===Select Hardware=== |
The AD9508 evaluation system allows one PC to control multiple evaluation boards. This window allows you to select which evaluation board the software is controlling. Click **Refresh List** to detect a recently connected evaluation board. \\ | The [[adi>ad9508|AD9508]] evaluation system allows one PC to control multiple evaluation boards. This window allows the user to select the evaluation board that the software is controlling. Click the **Refresh** button to detect a recently connected evaluation board. \\ |
<WRAP centeralign> | <WRAP centeralign> |
{{:resources:eval:user-guides:ad9508:figure11_select_usb_dev.png?direct&|}} | {{:resources:eval:user-guides:ad9508:figure11_select_usb_dev.png?direct&|}} |
\\ | \\ |
**Figure 11. Select USB Device Window** | //Figure 11. Select USB Device Window// |
</WRAP> | </WRAP> |
| |
__**Options (Enable Polling and Polling Interval**__\\ | ===Options (Enable Polling and Polling Interval=== |
Polling allows the user to define how often the software checks for changes made to the register values on the AD9508. Polling also checks for a hardware connection, which updates in the lower left hand portion of the main window. Polling Interval sets the length of time in-between each software check. The default interval is 1second. Figure 12 shows the Polling Interval selection window. | Polling allows the user to define how often the software checks for changes made to the register values on the [[adi>ad9508|AD9508]]. Polling also checks for a hardware connection, which updates in the lower left corner of the main window. The polling interval window sets the length of time between each software check. The default interval is 1 sec. Figure 12 shows the polling interval selection window. |
<WRAP centeralign> | <WRAP centeralign> |
{{:resources:eval:user-guides:ad9508:figure12_pollingintervalwindow.png?direct&|}} | {{:resources:eval:user-guides:ad9508:figure12_pollingintervalwindow.png?direct&|}} |
\\ | \\ |
**Figure 12. Polling Interval Window** | //Figure 12. Polling Interval Window// |
</WRAP> | </WRAP> |
| |
__**Exit**__\\ | ===Exit=== |
Exits the evaluation software. No checking is performed to ensure that the existing setup is saved. \\ | Exits the evaluation software. No checking is performed to ensure that the existing setup is saved. \\ |
| |
=== View Menu === | ==== View Menu ==== |
The **View** menu includes the following options: | The **View** menu includes the following options: |
| * Register Map |
| * Debug |
| |
__**Register Map**__\\ | ===Register Map=== |
Opens the **Register Map** Window. See the Register Map Window subsection in the Evaluation Software Components Section. | Opens the **Register Map** window. See the [[resources/eval/ad9508-user-guide#register_map_window|Register Map Window]] subsection in the [[resources/eval/ad9508-user-guide#evaluation_software_components|Evaluation Software Components]] section. |
| |
__**Debug**__\\ | ===Debug=== |
The **Debug** Window allows the user to read the values that are loaded into the various register addresses as well as manually load values into each register address of the AD9508 on the evaluation board. Figure 13 below shows the Debug window. Detailed information about the usable registers and their functions can be found in the AD9508 datasheet. | The **Debug** window allows the user to read the values that are loaded into the various register addresses as well as manually load values into each register address of the [[adi>ad9508|AD9508]] on the evaluation board. Figure 13 shows the **Debug Window**. Detailed information about the usable registers and their functions can be found in the [[adi>ad9508|AD9508]] data sheet. |
<WRAP centeralign> | <WRAP centeralign> |
{{:resources:eval:user-guides:ad9508:figure13_debugwindow.png?direct&|}} | {{:resources:eval:user-guides:ad9508:figure13_debugwindow.png?direct&|}} |
\\ | \\ |
**Figure 13. Debug Window** | //Figure 13. Debug Window// |
</WRAP> | </WRAP> |
| |
=== About Menu === | ==== About Menu ==== |
Selecting **About** opens the AD9508 window, which contains information about the version of the evaluation board software. | Selecting **About** opens the [[adi>ad9508|AD9508]] window, which contains information about the version of the evaluation board software. |
| \\ |
| ---- |
| |
| I<sup>2</sup>C refers to a communications protocol originally developed by Philips Semiconductors (now NXP Semiconductors). |