This version is outdated by a newer approved version.This version (16 Mar 2015 15:27) is a draft.
Approvals: 0/1
This is an old revision of the document!
EVALUATING THE AD9467-FMC-250EBZ ANALOG-TO-DIGITAL CONVERTER
Preface
This user guide describes the AD9467 evaluation board AD9467-FMC-250EBZ which provides all the support circuitry required to operate the ADC in its various modes and configurations. The application software to interface with the devices is also described.
The AD9467 data sheet provides additional information and should be consulted when using the board. All documents and software tools are available at www.analog.com/hsadcevalboard. For additional information or questions send an email to highspeed.converters@analog.com.
AD9467-FMC-250EBZ
Typical Measurement Setup
Features
Helpful Documents
-
EVAL-SDP-CH1Z data capture kit
SDP-H1
-
-
-
-
Software Needed
Design and Integration Files
Equipment Needed
Getting Started
Configuring the Board
Before using the software for testing, configure the evaluation board as follows:
-
Connect one 12V, 2.5A switching power supply (such as the one supplied) to the
SDP-H1 board. Connect the Mini-B
USB port of the
SDP-H1 board to the PC with the supplied
USB cable.
The
SDP-H1 will appear in the Device Manager as shown in Figure 3.
Figure 3. Device Manager Showing SDP-H1
If the Device Manager does not show the
SDP-H1 listed as shown in Figure 2, unplug all
USB devices from the PC, uninstall and re-install SPIController and VisualAnalog and restart the hardware setup from step 1.
On the ADC evaluation board, provide a clean, low jitter 250MHz clock source to connector J201 and set the amplitude to 16dBm. This is the ADC Sample Clock.
On the ADC evaluation board, provide a clean, low jitter clock source to connector J100. Use a shielded, RG-58, 50Ohm, coaxial cable to connect the signal generator output to the ADC Evaluation Board. For best results, use a narrow-band, pass filter with 50Ohm terminations and appropriate center frequency. (
ADI uses TTE, Allen Avionics, and
K & L band-pass filters)*.
*When connecting the ADC clock and analog source, use clean signal generators with low phase noise, such as Rohde & Schwarz SMA or HP8644B signal generators or equivalent*
Visual Analog Setup
Click Start
All Programs
Analog Devices
VisualAnalog
VisualAnalog.
On the VisualAnalog “New Canvas” window, click
ADC Single AD9467 FFT.
Figure 4. Selecting the AD9467 canvas
If VisualAnalog opens with a collapsed view, click on the “Expand Display” icon (see Figure 5).
Figure 5. Expanding the Display
Click the
Settings button in the
ADC Data Capture block as shown in Figure 6
Figure 6. Changing the ADC Capture Settings
On the
General tab make sure the clock frequency is set to
250MHz (or other clock frequency).
Figure 7. Setting the clock frequency and capture length
Click on the
Capture Board tab and browse to the
ad9467_sdp_h1.bin file. Click the
Program button. The
FPGA_DONE LED should illuminate on the EVAL-SDP-CH1Z board indicating that the FPGA has been correctly programmed. The bin file is available at the ftp site
ftp://ftp.analog.com/pub/HSC_ADC_Apps/SDP-H1/ad9467_sdp_h1.bin
Click OK
SPIController Setup
Click Start
All Programs
Analog Devices
SPIController
SPIController
Figure 8. Control Window for AD9647
Select the AD9467_16Bit_250MSsspiR03.cfg if prompted.
If necessary, click File
Cfg Open
AD9467_16Bit_250MSsspiR03.cfg
To enable
SPI communications, click File
Config
Controller Dialog and un-check the
SDO Active button
Figure 9. Un-Selecting SDO Active in SPIController
Obtaining an FFT
Click the Run button in VisualAnalog , you should see the captured data similar to the plot shown in Figure 9
Figure 10. AD9467-FMC-250 FFT at 5MHz Analog Input
Adjust the amplitude of the input signal so that the fundamental is at the desired level. (Examine the Fund Power reading in the left panel of the VisualAnalog FFT window.)
To save the FFT plot do the following
Click on the Float Form button in the FFT window
Figure 11. Floating the FFT window
Click on File
Save Form As button and save it to a location of choice
Troubleshooting Tips
FFT plot appears abnormal
If you see a normal noise floor when you disconnect the signal generator from the analog input, be sure you are not overdriving the ADC. Reduce input level if necessary.
In VisualAnalog, Click on the Settings button in the Input Formatter block. Check that Number Format is set to the correct encoding (Offset Binary by default).
The FFT plot appears normal, but performance is poor.
Make sure you are using the appropriate band-pass filter on the analog input.
Make sure the signal generators for the clock and the analog input are clean (low phase noise).
If you are using non-coherent sampling, change the analog input frequency slightly, or use coherent frequencies.
Make sure the
SPI config file matches the product being evaluated.
Make sure there isn't any extra stress/torque on the clock and analog input connectors.
The FFT window remains blank after the Run button is clicked
Make sure the evaluation board is securely connected to the
SDP-H1.
Make sure the FPGA has been programmed by verifying that the
FPGA_DONE LED is illuminated on the EVAL-SDP-CH1Z. If this LED is not illuminated reprogram the FPGA through VisualAnalog. If the LED still does not illuminate disconnect the
USB and power cord for 15 seconds. Connect again and repeat the
SDP-H1setup process.
Make sure the correct FPGA bin file was used to program the FPGA.
Be sure that the correct sample rate is programmed. Click on the Settings button in the ADC Data Capture block in VisualAnalog, and verify that the Clock Frequency is properly set.
VisualAnalog displays a blank FFT when the RUN button is clicked
Ensure that the ADC's
PLL is locked by checking the status of the
PLL lock detect register 0x22F. This can be done using SPIController.