Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:ad9467-fmc-250ebz [16 Jul 2015 11:14] – [Configuring the Board] Lucian Sin | resources:eval:ad9467-fmc-250ebz [03 Jan 2021 22:11] – fix links Robin Getz |
---|
====== EVALUATING THE AD9467-FMC-250EBZ ANALOG-TO-DIGITAL CONVERTER ====== | ====== EVALUATING THE AD9467-FMC-250EBZ ANALOG-TO-DIGITAL CONVERTER ====== |
===== Preface ===== | ===== Preface ===== |
This user guide describes the [[adi>AD9467|AD9467]] evaluation board [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] which provides all the support circuitry required to operate the ADC in its various modes and configurations. The application software to interface with the devices is also described. | This user guide describes the [[adi>AD9467|AD9467]] evaluation board [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] which provides all the support circuitry required to operate the ADC in its various modes and configurations. The application software to interface with the devices is also described. |
\\ | \\ |
\\ | \\ |
===== AD9467-FMC-250EBZ ===== | ===== AD9467-FMC-250EBZ ===== |
{{ :resources:eval:ad9467_board.png?700 |}}<WRAP centeralign> | {{ :resources:eval:ad9467_board.png?700 |}}<WRAP centeralign> |
//Figure 1. [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] Evaluation Board//</WRAP> | //Figure 1. [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] Evaluation Board//</WRAP> |
| |
===== Typical Measurement Setup ===== | ===== Typical Measurement Setup ===== |
{{ :resources:eval:ad9467_datacapture.png?900 |}}<WRAP centeralign> | {{ :resources:eval:ad9467_datacapture.png?900 |}}<WRAP centeralign> |
//Figure 2. Evaluation Board Connection—[[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] (on Left) and [[adi>SDP-H1|SDP-H1]] (on Right)// | //Figure 2. Evaluation Board Connection—[[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] (on Left) and [[adi>SDP-H1|SDP-H1]] (on Right)// |
</WRAP> | </WRAP> |
| |
===== Helpful Documents ===== | ===== Helpful Documents ===== |
* [[adi>AD9467|AD9467]] Data Sheet | * [[adi>AD9467|AD9467]] Data Sheet |
* EVAL-SDP-CH1Z data capture kit [[http://www.analog.com/en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] | * EVAL-SDP-CH1Z data capture kit [[adi>en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] |
* [[adi>an-905|AN-905 Application Note]], //VisualAnalog Converter Evaluation Tool Version 1.0 User Manual// | * [[adi>an-905|AN-905 Application Note]], //VisualAnalog Converter Evaluation Tool Version 1.0 User Manual// |
* [[adi>an-878|AN-878 Application Note]], //High Speed ADC SPI Control Software// | * [[adi>an-878|AN-878 Application Note]], //High Speed ADC SPI Control Software// |
* USB 2.0 port | * USB 2.0 port |
* [[adi>AD9467|AD9467-FMC-250EBZ]] board | * [[adi>AD9467|AD9467-FMC-250EBZ]] board |
*[[http://www.analog.com/en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] FPGA-based data capture kit | *[[adi>en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] FPGA-based data capture kit |
| |
===== Getting Started ===== | ===== Getting Started ===== |
This section provides quick start procedures for using the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] board. \\ | This section provides quick start procedures for using the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] board. \\ |
| |
==== Configuring the Board ==== | ==== Configuring the Board ==== |
Before using the software for testing, configure the evaluation board as follows: | Before using the software for testing, configure the evaluation board as follows: |
- Connect the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] evaluation board to the [[adi>SDP-H1|SDP-H1]] data capture board, as shown in Figure 2. | - Connect the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] evaluation board to the [[adi>SDP-H1|SDP-H1]] data capture board, as shown in Figure 2. |
- Connect one 12V, 2.5A switching power supply (such as the one supplied) to the [[adi>SDP-H1|SDP-H1]] board. Connect the Mini-B USB port of the [[adi>SDP-H1|SDP-H1]] board to the PC with the supplied USB cable. | - Connect one 12V, 2.5A switching power supply (such as the one supplied) to the [[adi>SDP-H1|SDP-H1]] board. Connect the Mini-B USB port of the [[adi>SDP-H1|SDP-H1]] board to the PC with the supplied USB cable. |
- The [[http://www.analog.com/en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] will appear in the Device Manager as shown in Figure 3. {{ :resources:eval:device_manger.png?200 |}}<WRAP centeralign> | - The [[adi>en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] will appear in the Device Manager as shown in Figure 3. {{ :resources:eval:device_manger.png?200 |}}<WRAP centeralign> |
//Figure 3. Device Manager Showing SDP-H1 //</WRAP> | //Figure 3. Device Manager Showing SDP-H1 //</WRAP> |
- If the Device Manager does not show the [[adi>SDP-H1|SDP-H1]] listed as shown in Figure 2, unplug all USB devices from the PC, uninstall and re-install SPIController and VisualAnalog and restart the hardware setup from step 1. | - If the Device Manager does not show the [[adi>SDP-H1|SDP-H1]] listed as shown in Figure 2, unplug all USB devices from the PC, uninstall and re-install SPIController and VisualAnalog and restart the hardware setup from step 1. |