Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:ad9249-65ebz [24 Sep 2016 02:39] – Additional items for FMC connector version Doug Ito | resources:eval:ad9249-65ebz [22 Mar 2017 02:29] – Doug Ito |
---|
\\ | \\ |
\\ | \\ |
There are two versions of the [[adi>AD9249|AD9249]] evaluation board [[adi>AD9249|AD9249-65EBZ]]. The earlier version uses two 60 pin Tyco connectors (TE Connectivity AMP Connector 6469169-1) and interfaces to the [[adi>hsadcevalboard|HSC-ADC-EVALDZ]] capture board. The later version (available late 2016 or early 2017) has an FMC connector (Samtec ASP-134488-01) and interfaces to the [[adi>hsadcevalboard|HSC-ADC-EVALEZ]] capture board. Both versions of the board perform the same function and this user guide applies to both. | There are two versions of the [[adi>AD9249|AD9249]] evaluation board [[adi>AD9249|AD9249-65EBZ]]. The earlier version uses two 60 pin Tyco connectors (TE Connectivity AMP Connector 6469169-1) and interfaces to the [[adi>hsadcevalboard|HSC-ADC-EVALDZ]] capture board. The new version has an FMC connector (Samtec ASP-134488-01) and interfaces to the [[adi>hsadcevalboard|HSC-ADC-EVALEZ]] capture board. Both versions of the board perform the same function and this user guide applies to both. All boards ordered from March 2017 and later will be the new version. |
\\ | \\ |
\\ | \\ |