This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ad9083 [09 Jan 2021 17:43] – [Evaluation] Alex Arrants | resources:eval:ad9083 [05 Jan 2022 16:45] (current) – change Gerber layout files to layout files Brigid Duggan | ||
---|---|---|---|
Line 14: | Line 14: | ||
===== Hardware Needed ===== | ===== Hardware Needed ===== | ||
* AD9083EBZ Evaluation Board | * AD9083EBZ Evaluation Board | ||
- | * [[ADS8-V3EBZ]] | + | * [[ADS8-V3EBZ]] |
===== Software Needed ===== | ===== Software Needed ===== | ||
- | * [[https:// | + | * [[/ |
===== Helpful Documents ===== | ===== Helpful Documents ===== | ||
Line 26: | Line 26: | ||
===== Board Design and Integration Files ===== | ===== Board Design and Integration Files ===== | ||
* {{: | * {{: | ||
- | * {{: | + | * {{: |
* {{: | * {{: | ||
Line 37: | Line 37: | ||
To ensure proper connection between the microSD card and the | To ensure proper connection between the microSD card and the | ||
MicroZed™ board, follow these steps: | MicroZed™ board, follow these steps: | ||
- | -Locate the microSD card labeled | + | -Locate the microSD card labeled |
-Connect the microSD card to the MicroZed™ board (the contacts of the microSD card are face up). | -Connect the microSD card to the MicroZed™ board (the contacts of the microSD card are face up). | ||
-As a precaution, ensure that the MicroZed™ board is seated properly on the ADS8-V3EBZ. Only a visual inspection is needed. | -As a precaution, ensure that the MicroZed™ board is seated properly on the ADS8-V3EBZ. Only a visual inspection is needed. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | //Figure 2. MicroSD Card Slot in MicroZed Board // | ||
**Configure the Network Interface to the MicroZed™ Board** | **Configure the Network Interface to the MicroZed™ Board** | ||
Line 81: | Line 85: | ||
{{: | {{: | ||
- | // | + | // |
**Plugin Installation from the Web** | **Plugin Installation from the Web** | ||
Line 106: | Line 110: | ||
{{: | {{: | ||
- | // | + | // |
**Board View** | **Board View** | ||
Line 117: | Line 121: | ||
{{: | {{: | ||
- | // | + | // |
**Chip View** | **Chip View** | ||
Line 125: | Line 129: | ||
{{: | {{: | ||
- | // | + | // |
===== Evaluation ===== | ===== Evaluation ===== | ||
Line 154: | Line 158: | ||
{{: | {{: | ||
- | // | + | // |
**Narrow Bandwidth Complex Output Mode** | **Narrow Bandwidth Complex Output Mode** | ||
Line 183: | Line 187: | ||
{{: | {{: | ||
- | // | + | // |
+ | |||
+ | **Precision Time Domain Mode** | ||
+ | |||
+ | Parameters: | ||
+ | * Sample rate = 1 GSPS. | ||
+ | * On-chip PLL reference = 125 MHz.(Provided by the on-board AD9528) | ||
+ | * VMAX = 1.8 V. | ||
+ | * RTERM = 100 Ω. | ||
+ | * fC = 800 MHz. | ||
+ | * High Performance Mode = False | ||
+ | * Fin Max = 50 MHz (sample rate/20). | ||
+ | * Backoff = 0 | ||
+ | * # ADC Channels = 16 | ||
+ | * Bypass CIC = False | ||
+ | * CIC decimator = 8. | ||
+ | * Use Mixer? = False | ||
+ | * Decimate by J = Bypass (Decimate by 1) | ||
+ | * jtx_subclasv_cfg = 0 | ||
+ | * Lanes (L) = 3 | ||
+ | * Virtual Converters (M) = 16 | ||
+ | * (Octets/ | ||
+ | * Bits Packed (NP) = 12 | ||
+ | * Resolution Bits (N) = 12 | ||
+ | * Frames in a multi-frame (K) = 32 | ||
+ | * 3 lanes at 10 Gbps each. | ||
+ | |||
+ | -Configure the AD9083 and AD9528 using the AD9083EBZSTARTUP WIZARD using the parameters listed above. | ||
+ | -Click " | ||
+ | -Navigate to Analysis | ||
+ | -Click "Run Once" | ||
+ | |||
+ | You should see an FFT after setting up the board as shown and running the macro. | ||
+ | {{: | ||
+ | |||
+ | //Figure 9. AD9083EBZ Precision Time Domain Mode Typical FFT // | ||
+ | ===== External Trigger ===== | ||
+ | SMA connector J2 on the ADS8v3 can be used as an optional trigger so that the data capture start time can be controlled. The trigger requires a 1.8V active high pulse width that is longer than the FPGA internal peripheral clock, which has a frequency of 50 MHz. | ||
+ | To enable the external trigger: | ||
+ | |||
+ | 1. Click on " | ||
+ | {{: | ||
+ | |||
+ | 2. Click on the " | ||
+ | {{: | ||
+ | |||
+ | 3. Click on the " | ||
+ | {{: | ||
+ | |||
+ | 4. Click "Apply Changes" | ||
+ | {{: | ||
+ | |||
+ | SMA connector J3 is normally used as a system ready indicator. It indicates that the FPGA is ready to accept an external trigger. | ||
+ | To capture data, click on "Run Once" as normal. Capture will begin once 1.8V is detected on connector J2 of the ADS8v3. | ||
===== Troubleshooting Notes ===== | ===== Troubleshooting Notes ===== |