This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:ad9083 [18 Jan 2021 14:52] – [Set Up MicroZed™ Connection] Alex Arrants | resources:eval:ad9083 [22 Feb 2021 22:16] – [Evaluation] Alex Arrants | ||
---|---|---|---|
Line 158: | Line 158: | ||
{{: | {{: | ||
- | //Figure 7. AD9083EBZ Typical FFT // | + | //Figure 7. AD9083EBZ |
**Narrow Bandwidth Complex Output Mode** | **Narrow Bandwidth Complex Output Mode** | ||
Line 187: | Line 187: | ||
{{: | {{: | ||
- | //Figure 8. AD9083EBZ Typical FFT // | + | //Figure 8. AD9083EBZ |
+ | **Precision Time Domain Mode** | ||
+ | Parameters: | ||
+ | * Sample rate = 1 GSPS. | ||
+ | * On-chip PLL reference = 125 MHz.(Provided by the on-board AD9528) | ||
+ | * VMAX = 1.8 V. | ||
+ | * RTERM = 100 Ω. | ||
+ | * fC = 800 MHz. | ||
+ | * High Performance Mode = False | ||
+ | * Fin Max = 50 MHz (sample rate/20). | ||
+ | * Backoff = 0 | ||
+ | * # ADC Channels = 16 | ||
+ | * Bypass CIC = False | ||
+ | * CIC decimator = 8. | ||
+ | * Use Mixer? = False | ||
+ | * Decimate by J = Bypass (Decimate by 1) | ||
+ | * jtx_subclasv_cfg = 0 | ||
+ | * Lanes (L) = 3 | ||
+ | * Virtual Converters (M) = 16 | ||
+ | * (Octets/ | ||
+ | * Bits Packed (NP) = 12 | ||
+ | * Resolution Bits (N) = 12 | ||
+ | * Frames in a multi-frame (K) = 32 | ||
+ | * 3 lanes at 10 Gbps each. | ||
+ | |||
+ | -Configure the AD9083 and AD9528 using the AD9083EBZSTARTUP WIZARD using the parameters listed above. | ||
+ | -Click " | ||
+ | -Navigate to Analysis | ||
+ | -Click "Run Once" | ||
+ | |||
+ | You should see an FFT after setting up the board as shown and running the macro. | ||
+ | {{: | ||
+ | |||
+ | //Figure 9. AD9083EBZ Precision Time Domain Mode Typical FFT // | ||
===== Troubleshooting Notes ===== | ===== Troubleshooting Notes ===== | ||
**Evaluation Board is not Functioning Properly** | **Evaluation Board is not Functioning Properly** |