This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:ad9083 [03 Jan 2021 22:12] – fix links Robin Getz | resources:eval:ad9083 [09 Jan 2021 17:43] – [Evaluation] Alex Arrants | ||
---|---|---|---|
Line 14: | Line 14: | ||
===== Hardware Needed ===== | ===== Hardware Needed ===== | ||
* AD9083EBZ Evaluation Board | * AD9083EBZ Evaluation Board | ||
- | * ADS8-V3EBZ | + | * [[ADS8-V3EBZ]] HIGH SPEED CARRIER CARD |
===== Software Needed ===== | ===== Software Needed ===== | ||
Line 113: | Line 113: | ||
section in ACE opens the AD9083EBZ board view. | section in ACE opens the AD9083EBZ board view. | ||
- | The board view tab enables the user to quickly set up the AD9083. Figure 4 shows the STARTUP WIZARD pane within the AD9083EBZ board view. | + | The board view tab enables the user to quickly set up the AD9083. Figure 4 shows the STARTUP WIZARD pane within the AD9083EBZ board view. It may take several moments for the board view to initialize. |
{{: | {{: | ||
Line 129: | Line 129: | ||
===== Evaluation ===== | ===== Evaluation ===== | ||
The AD9083 can be configured in many different ways. We will provide examples for several configurations here. | The AD9083 can be configured in many different ways. We will provide examples for several configurations here. | ||
+ | |||
+ | **Wide Bandwidth Real Output Mode** | ||
+ | |||
+ | Parameters: | ||
+ | * Sample rate = 2 GSPS. | ||
+ | * On-chip PLL reference = 250 MHz.(Provided by the on-board AD9528) | ||
+ | * fINMAX = 100 MHz (sample rate/20). | ||
+ | * fC = 800 MHz. | ||
+ | * VMAX = 2.0 V. | ||
+ | * RTERM = 100 Ω. | ||
+ | * EN_HP = 0 | ||
+ | * Backoff = 0 | ||
+ | * CIC decimator = bypass. | ||
+ | * Use mixer? = No. | ||
+ | * Decimate by J = 8. | ||
+ | * Transport parameters L, M, F, S, N’, K = 4, 16, 6, 1, 12, 32. | ||
+ | * 4 lanes at 15 Gbps each | ||
+ | -Configure the AD9083 and AD9528 using the AD9083EBZSTARTUP WIZARD using the parameters listed above. | ||
+ | -Click " | ||
+ | -Navigate to Analysis | ||
+ | -Click "Run Once" | ||
+ | |||
+ | You should see an FFT after setting up the board as shown and running the macro. | ||
+ | {{: | ||
+ | |||
+ | //Figure 6. AD9083EBZ Typical FFT // | ||
**Narrow Bandwidth Complex Output Mode** | **Narrow Bandwidth Complex Output Mode** | ||
Line 149: | Line 175: | ||
* 2 lanes at 10 Gbps each. | * 2 lanes at 10 Gbps each. | ||
- | -Configure the AD9083 and AD9528 using the AD9083EBZSTARTUP WIZARD | + | -Configure the AD9083 and AD9528 using the AD9083EBZSTARTUP WIZARD |
- | -Click " | + | -Click " |
-Navigate to Analysis | -Navigate to Analysis | ||
-Click "Run Once" | -Click "Run Once" | ||
You should see an FFT after setting up the board as shown and running the macro. | You should see an FFT after setting up the board as shown and running the macro. | ||
- | {{: | + | {{: |
- | // | + | // |
Line 170: | Line 196: | ||
**Evaluation Board is not Communicating with the ADS8-V3 / No SPI Communication** | **Evaluation Board is not Communicating with the ADS8-V3 / No SPI Communication** | ||
- | *Make sure the USB cable is making good connection on the ADS8-V3EBZ board and the PC. Try another USB port on the PC if needed. | + | *Make sure the USB cable is making good connection on the ADS8-V3EBZ board and the PC. Try another USB port on the PC if needed. Some PCs work best with a SuperSpeed USB 3.0 port. |
*The ADS8-V3EBZ should show up on the PC Device Manager | *The ADS8-V3EBZ should show up on the PC Device Manager | ||
*Make sure that the FPGA on the ADS8-V3 has been programmed - a lit FPGA_DONE LED DS15 on the top of the ADS8-V3 and a powered fan are good indicators of the FPGA being programmed. | *Make sure that the FPGA on the ADS8-V3 has been programmed - a lit FPGA_DONE LED DS15 on the top of the ADS8-V3 and a powered fan are good indicators of the FPGA being programmed. |