This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | Last revision Both sides next revision | ||
resources:eval:ad9083 [22 Mar 2021 21:18] Alex Arrants [External Trigger] |
resources:eval:ad9083 [23 Mar 2021 13:17] Umesh Jayamohan [External Trigger] minor grammatical changes |
||
---|---|---|---|
Line 224: | Line 224: | ||
//Figure 9. AD9083EBZ Precision Time Domain Mode Typical FFT // | //Figure 9. AD9083EBZ Precision Time Domain Mode Typical FFT // | ||
===== External Trigger ===== | ===== External Trigger ===== | ||
- | SMA connector J2 on the ADS8v3 can used as an optional trigger so that the data capture start time can be controlled. The trigger requires an 1.8V active high pulse width that is longer than the FPGA internal peripheral clock, which has a frequency of 50 MHz. | + | SMA connector J2 on the ADS8v3 can be used as an optional trigger so that the data capture start time can be controlled. The trigger requires a 1.8V active high pulse width that is longer than the FPGA internal peripheral clock, which has a frequency of 50 MHz. |
To enable the external trigger: | To enable the external trigger: | ||
Line 235: | Line 235: | ||
3. Click on the "0" that is on the same row as "ext_trig_en". The 0 will change to a 1. | 3. Click on the "0" that is on the same row as "ext_trig_en". The 0 will change to a 1. | ||
{{:resources:eval:ad9083:ext_trig_en.png?1652|}} | {{:resources:eval:ad9083:ext_trig_en.png?1652|}} | ||
+ | |||
4. Click "Apply Changes" | 4. Click "Apply Changes" | ||
{{:resources:eval:ad9083:apply_changes.png?94|}} | {{:resources:eval:ad9083:apply_changes.png?94|}} |