This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:ad9083 [22 Feb 2021 22:07] – [Evaluation] Alex Arrants | resources:eval:ad9083 [22 Feb 2021 22:16] – [Evaluation] Alex Arrants | ||
---|---|---|---|
Line 158: | Line 158: | ||
{{: | {{: | ||
- | //Figure 7. AD9083EBZ Typical FFT // | + | //Figure 7. AD9083EBZ |
**Narrow Bandwidth Complex Output Mode** | **Narrow Bandwidth Complex Output Mode** | ||
Line 187: | Line 187: | ||
{{: | {{: | ||
- | //Figure 8. AD9083EBZ Typical FFT // | + | //Figure 8. AD9083EBZ |
**Precision Time Domain Mode** | **Precision Time Domain Mode** | ||
Line 198: | Line 198: | ||
* fC = 800 MHz. | * fC = 800 MHz. | ||
* High Performance Mode = False | * High Performance Mode = False | ||
- | * fIN Max = 50 MHz (sample rate/20). | + | * Fin Max = 50 MHz (sample rate/20). |
* Backoff = 0 | * Backoff = 0 | ||
* # ADC Channels = 16 | * # ADC Channels = 16 | ||
Line 220: | Line 220: | ||
You should see an FFT after setting up the board as shown and running the macro. | You should see an FFT after setting up the board as shown and running the macro. | ||
- | {{: | + | {{: |
- | // | + | // |
===== Troubleshooting Notes ===== | ===== Troubleshooting Notes ===== | ||
**Evaluation Board is not Functioning Properly** | **Evaluation Board is not Functioning Properly** |