This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ad9082 [16 Jun 2021 02:48] – Add troubleshooting tip to try a different USB cable Doug Ito | resources:eval:ad9082 [06 Oct 2022 16:31] (current) – Added ACE Matlab Automation Sydney Wells | ||
---|---|---|---|
Line 166: | Line 166: | ||
This MATLAB support is provided through ADI’s High Speed Converter Toolbox. | This MATLAB support is provided through ADI’s High Speed Converter Toolbox. | ||
Click on this link below on GitHub | Click on this link below on GitHub | ||
- | https:// | + | https:// |
{{ : | {{ : | ||
Line 320: | Line 320: | ||
After powering up the ADS9-V2EBZ FPGA board and starting ACE, the hardware will be auto-detected and the plugin icon should appear in the GUI as shown at the top of the " | After powering up the ADS9-V2EBZ FPGA board and starting ACE, the hardware will be auto-detected and the plugin icon should appear in the GUI as shown at the top of the " | ||
+ | |||
+ | ======= Automating ACE with MATLAB ======= | ||
+ | User Guide: {{ : | ||
+ | |||
+ | Code: {{ : |