This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:ad6688-3000ebz [11 May 2017 21:46] – Ryan Chojnacki | resources:eval:ad6688-3000ebz [11 May 2017 22:16] – Ryan Chojnacki | ||
---|---|---|---|
Line 126: | Line 126: | ||
* Check the PLL Locked indicator (see Figure 16) or register 0x056F (PLL Status). If the light is green / if the register reads back 0x80, the PLL is locked. If it is not locked: | * Check the PLL Locked indicator (see Figure 16) or register 0x056F (PLL Status). If the light is green / if the register reads back 0x80, the PLL is locked. If it is not locked: | ||
* Check the clock being inputted to connector J201 (in this guide, 3 GHz). | * Check the clock being inputted to connector J201 (in this guide, 3 GHz). | ||
- | * Check the JESD settings under the Initial Configuration. Reference the AD9208 | + | * Check the JESD settings under the Initial Configuration. Reference the AD6688 |
* Check the reference clock and make sure it matches your JESD settings. | * Check the reference clock and make sure it matches your JESD settings. | ||
* Make sure P100 (Power Down / Standby Jumper, see Figure 6) is not jumped. | * Make sure P100 (Power Down / Standby Jumper, see Figure 6) is not jumped. | ||