Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:ad6684-500ebz [05 May 2017 17:08] – [Obtaining an FFT - NSR Mode] Judy Chui | resources:eval:ad6684-500ebz [25 Feb 2019 15:22] – [Design and Integration Files] Alan Yu |
---|
The [[adi>AD6684|AD6684]] data sheet provides additional information and should be consulted when using the evaluation board. All documents and software tools are available at [[adi>hsadcevalboard|www.analog.com/hsadcevalboard]]. For additional information or questions, send an email to highspeed.converters@analog.com. | The [[adi>AD6684|AD6684]] data sheet provides additional information and should be consulted when using the evaluation board. All documents and software tools are available at [[adi>hsadcevalboard|www.analog.com/hsadcevalboard]]. For additional information or questions, send an email to highspeed.converters@analog.com. |
===== AD6684 Evaluation Board ===== | ===== AD6684 Evaluation Board ===== |
| The images below show the location and position of the jumpers on the old (first image) and new (second image) versions of the [[adi>AD6684|AD6684-500EBZ]]. |
{{ :resources:eval:ad9694_jumpers.jpg?direct800 |}}<WRAP centeralign> | {{ :resources:eval:ad9694_jumpers.jpg?direct800 |}}<WRAP centeralign> |
//[[adi>AD6684|AD6684]] Evaluation Board//</WRAP> | //[[adi>AD6684|AD6684]] Evaluation Board//</WRAP> |
| {{ :resources:eval:ad9694_jumpers_new_board.jpg?direct800 |}}<WRAP centeralign> |
| //[[adi>AD6684|AD6684]] Evaluation Board (new version)//</WRAP> |
===== Typical Measurement Setup ===== | ===== Typical Measurement Setup ===== |
The [[adi>AD6684|AD6684-500EBZ]] can be evaluated using the [[ads7-v2|ADS7-V2EBZ]] FPGA data capture board. The figure below shows the [[adi>AD6684|AD6684-500EBZ]] connected to the [[ads7-v2|ADS7-V2EBZ]]. | The [[adi>AD6684|AD6684-500EBZ]] can be evaluated using the [[ads7-v2|ADS7-V2EBZ]] FPGA data capture board. The figure below shows the [[adi>AD6684|AD6684-500EBZ]] connected to the [[ads7-v2|ADS7-V2EBZ]]. If using the old version of the board, refer to the first image for connections, otherwise if using the new version of the board, refer to the second image. |
{{ :resources:eval:ad9694_connection.png?direct&800 |}}<WRAP centeralign> | {{ :resources:eval:ad9694_connection.png?direct&800 |}}<WRAP centeralign> |
//Evaluation Board Connection—[[adi>AD6684|AD6684-500EBZ]]// | //Evaluation Board Connection—[[adi>AD6684|AD6684-500EBZ]]// |
| </WRAP> |
| {{ :resources:eval:ad9694_connection_new_board.jpg?direct&800 |}}<WRAP centeralign> |
| //(New) Evaluation Board Connection—[[adi>AD6684|AD6684-500EBZ]]// |
</WRAP> | </WRAP> |
===== Features ===== | ===== Features ===== |
* ACE [[https://wiki.analog.com/resources/tools-software/ace]] | * ACE [[https://wiki.analog.com/resources/tools-software/ace]] |
===== Design and Integration Files ===== | ===== Design and Integration Files ===== |
*[[https://wiki.analog.com/_media/eval/9694_board_files_ce01.zip|AD9694CE01A schematic, BOM, layout files]] | *[[https://wiki.analog.com/_media/eval/9694_board_files_ce04.zip|AD9694CE04A schematic, BOM, layout files]] |
===== Equipment Needed ===== | ===== Equipment Needed ===== |
* Analog signal source and antialiasing filter | * Analog signal source and antialiasing filter |