This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:ad6674-1000ebz [03 Jun 2015 19:18] – [Visual Analog Setup] Jonathan Harris | resources:eval:ad6674-1000ebz [19 Aug 2015 17:38] – [Viewing the VDR Punish Bits and the VDR High/Low Resolution Bit - VDR Mode] Jonathan Harris | ||
---|---|---|---|
Line 124: | Line 124: | ||
- Click on File < | - Click on File < | ||
==== Setting up SPIController to Use Control Bits as VDR Punish Bits and the VDR High/Low Resolution Bit - VDR Mode ==== | ==== Setting up SPIController to Use Control Bits as VDR Punish Bits and the VDR High/Low Resolution Bit - VDR Mode ==== | ||
- | - The first step go to the ADCBase2 tab in SPIController to set up the control bits to select the VDR indicator bits. In this example Control Bit 2 is set to VDR Punish Bit 1, Control Bit 1 is set to VDR Punish Bit 0, and Control Bit 0 is set to the VDR High/Low resolution bit.{{ : | + | - The first step go to the ADCBase2 tab in SPIController to set up the control bits to select the VDR indicator bits. In this example Control Bit 2 is set to VDR Punish Bit 1, Control Bit 1 is set to VDR Punish Bit 0, and Control Bit 0 is set to the VDR High/Low resolution bit. (Similarly, the control bits may be set up to function as Overrange, Signal Monitor (SMON), |
- Next go to the ADCBase4 tab to set up the control bits to select the VDR indicator bits. In this example three control bits are sent per sample. In order to accommodate three control bits, the converter resolution (N) must be set to 13 bits (there are 16 available bits in the JESD204B data word and if three are used for control bits there are 13 bits available for the converter sample - in this example this means there will only be 13 bits available instead of the 14 bits of converter resolution.{{ : | - Next go to the ADCBase4 tab to set up the control bits to select the VDR indicator bits. In this example three control bits are sent per sample. In order to accommodate three control bits, the converter resolution (N) must be set to 13 bits (there are 16 available bits in the JESD204B data word and if three are used for control bits there are 13 bits available for the converter sample - in this example this means there will only be 13 bits available instead of the 14 bits of converter resolution.{{ : | ||
==== Viewing the VDR Punish Bits and the VDR High/Low Resolution Bit - VDR Mode ==== | ==== Viewing the VDR Punish Bits and the VDR High/Low Resolution Bit - VDR Mode ==== | ||
- The first step is to open a new Logic canvas in VisualAnalog. | - The first step is to open a new Logic canvas in VisualAnalog. | ||
- Next configure the Logic Analysis block for the data alignement. | - Next configure the Logic Analysis block for the data alignement. | ||
- | - These settings will create the space in the Logic Canvas display so that all three control bits available in the JESD204B data stream will be visible. {{ : | + | - These settings will create the space in the Logic Canvas display so that all three control bits available in the JESD204B data stream will be visible. |
- Once a signal is input that will trigger VDR to operate the VDR punish bits [1:0] and the VDR High/Low resolution bit can be seen in the Logic Canvas display. In this case control bit 2 is VDR punish bit 1, control bit 1 is VDR punish bit 0, and control bit 0 is the VDR High/Low resolution bit. {{ : | - Once a signal is input that will trigger VDR to operate the VDR punish bits [1:0] and the VDR High/Low resolution bit can be seen in the Logic Canvas display. In this case control bit 2 is VDR punish bit 1, control bit 1 is VDR punish bit 0, and control bit 0 is the VDR High/Low resolution bit. {{ : | ||
- Note that the data alignment from the FPGA to VisualAnalog will fill in the control bits starting from the LSB location in the Logic Canvas display. | - Note that the data alignment from the FPGA to VisualAnalog will fill in the control bits starting from the LSB location in the Logic Canvas display. |