This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:ad4630-16-eval-board [25 May 2022 01:14] – [Sampling Frequency] Jim Catt | resources:eval:ad4630-16-eval-board [20 Jul 2022 16:01] (current) – Updated text Padraic O Reilly | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD4630-24, AD4030-24 & AD4630-16 SAR ADC Evaluation Board User Guide ====== | + | {{section> |
- | ===== General Description ===== | + | |
- | + | ||
- | The EVAL-AD4630-24FMCZ, | + | |
- | The [[http:// | + | |
- | The evaluation boards are designed for use with the Digilent [[http:// | + | |
- | The evaluation board includes:\\ | + | |
- | * A high precision buffered band gap 5 volt reference ([[https:// | + | |
- | * An analog front end (AFE) that provides signal conditioning and drive for the AD4630-24, AD4030-24 & AD4630-16. The AFE can be configured to use either the [[http:// | + | |
- | * An optional 100 MHz clock source that provides a reference clock for the FPGA and ADC. | + | |
- | * Full power supply solution that provides all the necessary voltage rails from a 12 volt supply that is provided from the ZedBoard through the FMC connector. \\ | + | |
- | + | ||
- | Full descriptions of these products are available in their respective data sheets, which should be consulted when using the evaluation board.\\ | + | |
- | ===== Features ===== | + | |
- | * On-board voltage reference, clock source, and ADC drivers | + | |
- | * Versatile analog signal conditioning circuitry | + | |
- | * FMC-LPC system board connector | + | |
- | * ACE PC software for configuration and data analysis (time and frequency domain) | + | |
- | * Compatible with other off-the-shelf controller boards | + | |
- | ===== Evaluation Board Kit Contents ===== | + | |
- | * EVAL-AD4630-24FMCZ, | + | |
- | * Micro-SD memory card (with adapter) containing system board boot software and Linux OS | + | |
- | * Optional - ZedBoard (system controller board ) | + | |
- | + | ||
- | ===== Equipment Needed ===== | + | |
- | * PC with Windows 7 or Windows 10 operating system | + | |
- | * Digilent ZedBoard with 12 V wall adapter power supply | + | |
- | * Precision signal source | + | |
- | * SMA Cable(s) (input to evaluation board) | + | |
- | * Recommended - Band-pass filter centered on test signal frequency. | + | |
- | + | ||
- | ===== Quick Start Guide ===== | + | |
- | 1. Download and install ACE Software from [[adi> | + | |
- | < | + | |
- | 2. Connect the evaluation board and ZedBoard™ firmly together through the FMC Connector. \\ | + | |
- | 3. Insert the SD card provided with the evaluation board into the SD card slot of the ZedBoard™. \\ | + | |
- | 4. Connect the ZedBoard™’s USB OTG port (next to PMOD connector JE1) to the PC via a micro-USB cable. \\ | + | |
- | 5. Connect the 12 volt power adaptor to ZedBoard™ and slide the POWER switch (SW8) on the ZedBoard™ to the ON position.\\ | + | |
- | 6. Verify that the Green POWER LED (LD13) and the Blue Done LED (LD12) on the ZedBoard™ turn on.\\ | + | |
- | 7. Wait for the Red LED (LD7) on the ZedBoard™ to start blinking.\\ | + | |
- | 8. Launch the ACE software from the Windows Start menu.\\ | + | |
- | + | ||
- | ===== Evaluation Board Hardware ===== | + | |
- | + | ||
- | {{:resources: | + | |
- | + | ||
- | + | ||
- | + | ||
- | **//Figure 1. EVAL-AD4630-XXFMCZ Evaluation System//** \\ | + | |
- | {{: | + | |
- | \\ | + | |
- | **//Figure 2a. EVAL-AD4030-24FMCZ// | + | |
- | + | ||
- | {{: | + | |
- | \\ | + | |
- | **Figure 2b. EVAL-AD4630-24FMCZ** \\ | + | |
- | + | ||
- | {{: | + | |
- | **Figure 2c. EVAL-AD4630-16FMCZ** \\ | + | |
- | + | ||
- | + | ||
- | ==== Setting Up the Evaluation Board ==== | + | |
- | Figure 1 illustrates the evaluation system components. To use the system, connect the evaluation board to the ZedBoard, connect a micro-USB cable to the USB OTG port, apply power to the ZedBoard, open the ACE GUI, and supply an input stimulus to one or both ADC channels.\\ | + | |
- | + | ||
- | Each ADC channel has dedicated SMA connectors that support either a singled-ended or differential input. The signals on these inputs are injected to the configurable AFE (see the **Analog Front End** section below for more details). The digital interface to the system controller board uses level shifters to translate between the VIO supply of the AD4630-16 and the I/O voltage of the Zynq 7000 on the ZedBoard. By default, the evaluation board is powered from the system controller board 12V supply through the FMC connector. The **Power Supplies** section contains a list of optional on-board connections that can be used to connect external supplies and references to the board.\\ | + | |
- | ==== Power Supplies ==== | + | |
- | The primary 12 volt supply to the EVAL-AD4X30-XXFMCZ comes from the ZedBoard through the FMC connector. 12 volts is regulated down to an intermediate voltage with a switcher and then is post regulated down to the various voltage rails. 12 volts is also used to generate the negative rails for the buffers and final drive amplifiers. | + | |
- | + | ||
- | Each of the voltage rails are brought out to turrets so they can be easily measured (see **Figure 1**). A bench supply can be used to drive these turrets to supply the evaluation board manually. This is useful if a current measurement is required. Each supply is decoupled where it enters the board and at each device. A single ground plane is used on this board to minimize the effect of high frequency interference. The voltage ranges listed in the table below represent the expected ranges for the board. If the user desires to connect external supplies to the board, the amplifier data sheets and the [[http:// | + | |
- | + | ||
- | + | ||
- | ^ Power Supply | + | |
- | | +12V | 12 volt primary supply via FMC connector | + | |
- | | GND | Ground connection | + | |
- | | +3.3V | 3.3 volts for various digital logic | + | |
- | | +1.8V | 1.8 volts for the ADC | + | |
- | | VIO | 1.8 volt supply for the ADC digital I/O | + | |
- | | +5V | 5 volts for the ADC | + | |
- | | REFIN | 5 volt ADC reference input | 4.95 | 5.05 | | + | |
- | | VAMP+ | Positive supply for the amplifiers | + | |
- | | VAMP- | Negative supply for the amplifiers | + | |
- | | VP1 | 5.7 volts at the input of the switcher | + | |
- | | REF | 5 volts at the ADC reference output | + | |
- | | EN | 1.8 volts enable signal for the power supplies | + | |
- | + | ||
- | ** //Table 1. On-Board Power Supplies// ** \\ | + | |
- | ==== Reference Circuit ==== | + | |
- | By default, the on-board LT6655 provides a 5 V reference to the AD4630-24, AD4030-24 & AD4630-16. It drives the REFIN pin of the ADC through an R-C filter (R=100Ω, C=1μF) that reduces the wideband noise. The REFIN pin is connected to an internal buffer, eliminating the need for an external buffer. However, if the user desires to use an external reference that drives the internal buffer, it can be attached the EXT REF SMA connector (see figure below). R137 should be populated with a zero ohm resistor, and R136 should be open. The internal buffer can be bypassed by attaching an external reference to the REF turret on the board. To reduce the ADC power consumption, | + | |
- | === === | + | |
- | {{: | + | |
- | **//Figure 3. EVAL-AD4X30-XXFMCZ Reference circuit (AD4630-24 shown. Configuration applies to all parts)// | + | |
- | + | ||
- | ==== Clock Circuit ==== | + | |
- | The ZedBoard uses a 100MHz reference clock to generate its internal clocks as well as the sample clock for the AD4630-24, AD4030-24 or AD4630-16. To simplify system operation an on-board | + | |
- | + | ||
- | {{: | + | |
- | **//Figure 4. EVAL-AD4X30-XXFMCZ clock circuit (AD4630-24 shown. Configuration applies to all parts)// | + | |
- | ==== Analog Front End ==== | + | |
- | The EVAL-AD4X30-XXFMCZ has a flexible driver network that can be configured for a variety topologies. The default network is shown in Figure 5, in which the ADA4945-1 fully differential amplifier is driving the ADC. It can accommodate both single-ended and differential signal sources, and drives the ADC differentially. As populated, it has a unity gain. When using a single-ended source, the unused input should be terminated with the equivalent source impedance. **Note:** As implemented, | + | |
- | + | ||
- | {{ : | + | |
- | **//Figure 5. Differential Driver AFE (default) (AD4630-24 shown. Configuration applies to all parts)// | + | |
- | + | ||
- | + | ||
- | ^ Function: | + | |
- | ^ Comments: | + | |
- | ^ Required changes from default configuration: | + | |
- | **//Table 2. EVAL-AD4630-xxFMCZ Default AFE Configuration// | + | |
- | + | ||
- | A second topology can be seen in Figure 6. This topology consists of a pair of unity gain buffers, the ADA4896-2. It also can be driven by either a singled-ended or differential source. This network is ideal for observing the best noise performance of the AD4630-16, due to the low voltage and current noise of the ADA4896-2 (1 nV/rtHz and 2.8 pA/rtHz, respectively). It also offers a common mode input impedance of 10 MΩ and a wide input common mode voltage range of -4.9V to +4.1V (when using +/- 5V supplies). **Note:** This driver circuit also inverts the polarity of the input signal. To preserve polarity when measuring DC voltages, connect a positive voltage to IN_A/B-. Likewise, a negative DC voltage should be connected to IN_A/B+. \\ | + | |
- | + | ||
- | {{ : | + | |
- | **// Figure 6. Dual Buffer AFE (AD4630-24 shown. Configuration applies to all parts) //** \\ | + | |
- | + | ||
- | ^ Function: | + | |
- | ^ Comments: | + | |
- | ^ Required changes from default configuration: | + | |
- | ** //Table 3. Unity Gain Dual Buffer Configuration// | + | |
- | + | ||
- | + | ||
- | Figure 7 shows a driver network which combines the ADA4896-2 with the ADA4945-1. This circuit is ideal for applications that require a high input impedance along with gain to maximize the input range of the ADC. The gain of the ADA4945-1 can modified by changing either the feedback resistors or input resistors. \\ | + | |
- | + | ||
- | {{ : | + | |
- | **//Figure 7. High Impedance Buffer with Gain AFE (AD4630-24 shown. Configuration applies to all parts)// | + | |
- | + | ||
- | ^ Function: | + | |
- | ^ Comments: | + | |
- | ^ Required changes from default configuration: | + | |
- | **// Table 4. High Impedance with Gain Configuration //** \\ | + | |
- | + | ||
- | Figure 8 shows an input configuration that allows the AD4630-16 to be directly driven from the SMA connectors. This enables testing with alternative driver configurations mounted on an external PCB. \\ | + | |
- | + | ||
- | {{ : | + | |
- | **//Figure 8. Direct Driven Inputs (AD4630-24 shown. Configuration applies to all parts)//** \\ | + | |
- | + | ||
- | ^ Function: | + | |
- | ^ Comments: | + | |
- | ^ Required changes from default configuration: | + | |
- | ** //Table 5. Direct Drive Configuration// | + | |
- | + | ||
- | ===== Controller Board ===== | + | |
- | The ZedBoard, which is the system controller board, enables the configuration of the ADC and capture of data from the evaluation board by the PC via USB (or Ethernet). The AD4X30-XX family of parts support a multi-lane serial port interface (SPI) for each data converter channel. The SPI interface for each channel is connected to the ZedBoard via the FMC connector (P1). The ZedBoard™ functions as the communication link between the PC and connected evaluation board. It buffers samples captured from the evaluation board in its DDR3 memory. The ZedBoard board requires power from a 12 volt wall adapter (included with the ZedBoard). It hosts a Xilinx® ZYNQ® 7020 SoC, which contains two ARM® Cortex-A9 Processors and a Series-7 FPGA with 85k Programmable Logic cells. A Linux OS runs on the host processor system. It communicates with the PC through either a USB 2.0 high speed port or a 10/100/1000 Ethernet port. The default software configuration uses USB. | + | |
- | ===== Evaluation Software ===== | + | |
- | ==== GETTING STARTED ==== | + | |
- | + | ||
- | The ACE evaluation software controls and configures the evaluation board through the ZedBoard. | + | |
- | ==== SOFTWARE INSTALLATION PROCEDURES ==== | + | |
- | + | ||
- | Before connecting the evaluation board to the ZedBoard, take the following steps to set up the AD4630-24, AD4030-24 or AD4630-16 for initial use in the ACE evaluation software: | + | |
- | + | ||
- | 1. Download the ACE evaluation software package from the [[adi> | + | |
- | + | ||
- | 2. Click on **Download ACE Installer** to download the file.\\ | + | |
- | + | ||
- | 3. Run the installer and follow the instructions to complete the software installation process.\\ | + | |
- | \\ | + | |
- | During the installation process, be sure to select **// | + | |
- | < | + | |
- | \\ | + | |
- | {{: | + | |
- | **//Figure 9. Select Precision Converter Components during the ACE installation// | + | |
- | \\ | + | |
- | When the following prompt appears, be sure to select **// | + | |
- | \\ | + | |
- | {{: | + | |
- | **//Figure 10. Select LibIIO components during ACE installation// | + | |
- | + | ||
- | + | ||
- | ==== EVALUATION HARDWARE SETUP ==== | + | |
- | When the ACE evaluation software installation is complete, take the following steps to set up the ZedBoard and the evaluation board together: | + | |
- | + | ||
- | 1. Insert the SD card provided with the evaluation board into J12 on the ZedBoard | + | |
- | + | ||
- | 2. Connect the Evaluation board to the FMC connector of the ZedBoard. | + | |
- | + | ||
- | 3. Connect the provided power supplies to J20 on the ZedBoard. | + | |
- | + | ||
- | 4. Connect the USB cable to the USB OTG (J13) on the ZedBoard and to the computer | + | |
- | + | ||
- | 5. Connect the desired input signal to the appropriate input on the evaluation board (J2-J5) | + | |
- | + | ||
- | 6. Move SW8 to the ON position to start the ZedBoard | + | |
- | + | ||
- | 7. Start the ACE evaluation software (see the Software Operation section). | + | |
- | + | ||
- | ==== SOFTWARE OPERATION ==== | + | |
- | To start the ACE evaluation software, from the Windows Start menu, click Analog Devices > ACE. The software window opens (see Figure 11) until the software recognizes the AD4630-24, AD4030-24 or AD4630-16 evaluation board. When the software recognizes the board, double-click on the icon in the **// | + | |
- | + | ||
- | {{: | + | |
- | + | ||
- | **//Figure 11. Select Interface Window// | + | |
- | + | ||
- | + | ||
- | + | ||
- | ==== MAIN WINDOW ==== | + | |
- | + | ||
- | {{: | + | |
- | + | ||
- | **//Figure 12. ACE Evaluation Software Main Window// | + | |
- | + | ||
- | In the main ACE evaluation software window (see Figure 12), the AD4630-16 can be configured. | + | |
- | === Lane Mode === | + | |
- | Select the number of SPI lanes to use to transmit the data. The options are 1, 2, or 4 lanes per channel. | + | |
- | === Clock Mode === | + | |
- | Selects between the echo clock mode and the SPI clock mode. | + | |
- | === Date Rate === | + | |
- | Selects between single data rate (SDR: 1-bit per clock cycle) or dual data rate (DDR: 2-bits per clock cycle). DDR is only available when using Echo clock mode or Master clock mode. **Note:** The current Linux driver and HDL do not support Master clock mode. | + | |
- | === Data Mode === | + | |
- | Selects the data output format of the AD4630-24, AD4030-24 or AD4630-16. | + | |
- | + | ||
- | === Apply Operating mode and reboot === | + | |
- | Changes to the operating parameters listed above requires a reboot of the ZedBoard. | + | |
- | + | ||
- | 1. After changing any of the operating parameters, click “Apply Operating mode and reboot”. | + | |
- | + | ||
- | 2. Close any of the following ACE windows that may be open: | + | |
- | + | ||
- | * Analysis | + | |
- | + | ||
- | * AD4630IIO | + | |
- | + | ||
- | * AD4630IIO Board | + | |
- | + | ||
- | * Start | + | |
- | + | ||
- | * System - In this tab, close the subsystem box that contains the components shown in the following figure.\\ | + | |
- | {{: | + | |
- | **//Figure 13. Subsystem view//** \\ | + | |
- | + | ||
- | 3. Click on the “Home” icon in the upper portion of the left pane. The AD4630 plug-in should appear. If not, it may be necessary to click **//Refresh Attached Hardware// | + | |
- | 4. Double-click on the part plug-in to open the board view and start using the available evaluation functions. | + | |
- | + | ||
- | + | ||
- | ==== Chip View ==== | + | |
- | + | ||
- | {{: | + | |
- | + | ||
- | **//Figure 14. Chip View//** \\ | + | |
- | + | ||
- | By clicking on the part in the main ACE evaluation software window (see Figure 12), the chip view will be opened (Figure 14). Settings for the part available in this window include enabling and configuring averaging mode, changing the sample frequency, and changing the gain and offset for each channel. Refer to the data sheet for a detailed explanation of these features. | + | |
- | + | ||
- | === Operating mode === | + | |
- | Selects between normal operating mode and low power mode. | + | |
- | === Sample Averaging === | + | |
- | Sets the number of samples to be used by the internal block averaging filter of the part. Select OFF to disable averaging, or select the desired number of samples to be averaged by the part. Ensure that the Data Mode is set to 30-bit averaged data when using this feature. | + | |
- | === Sampling Frequency === | + | |
- | Selects the desired sample frequency from a drop down menu. Note that this is the frequency of the pulse that is applied to the CNV pin. The sampling frequency can be scaled by changing the frequency of the reference clock (see the Clock Circuit section). The sampling rate selected from the menu can be scaled by applying a lower frequency external clock. The effective sampling rate is: **selected sampling frequency x f< | + | |
- | If the block averaging filter is enabled, the effective output sample rate is the sampling frequency divided by the selected block average size. | + | |
- | === Hardware Gain === | + | |
- | This sets the internal digital gain applied to the differential data. The gain can be adjusted independently for each channel. | + | |
- | === Offset === | + | |
- | This sets the internal digital offset that is applied to the differential data. The offset can be independently set for each channel. \\ | + | |
- | \\ | + | |
- | + | ||
- | + | ||
- | + | ||
- | ==== REGISTER MAP ==== | + | |
- | + | ||
- | {{: | + | |
- | + | ||
- | **//Figure 15. Register Map//** | + | |
- | + | ||
- | By clicking on **//Proceed to Memory Map//** in the lower right corner of the Chip view (see Figure 12), the AD4630 register map view will be opened (figure 15). In this view all registers can be read and selected registers can be modified. | + | |
- | + | ||
- | + | ||
- | ==== ANALYSIS VIEW ==== | + | |
- | + | ||
- | {{: | + | |
- | + | ||
- | **//Figure 16. Analysis View//** | + | |
- | + | ||
- | By clicking on **//Proceed to Analysis// | + | |
- | + | ||
- | {{: | + | |
- | + | ||
- | **//Figure 17. Time domain waveform// | + | |
- | + | ||
- | {{: | + | |
- | + | ||
- | **//Figure 18. FFT view//** | + | |
- | + | ||
- | {{: | + | |
- | + | ||
- | **//Figure 19. Histogram view//** | + | |
- | + | ||
- | ===== System Operational Constraints===== | + | |
- | ==== Sampling Frequency==== | + | |
- | The following table illustrates the maximum sampling rates that can be achieved based on the device configuration. Note that the FPGA SPI engine only supports Zone 2 data transfers from the AD4630/ | + | |
- | + | ||
- | **Table 6. Maximum sampling rate by device configuration ** | + | |
- | ^ Clocking Mode ^ Lane Mode (per channel) ^ Data Rate ^ Data format ^ Max sampling rate ^ | + | |
- | | SPI | + | |
- | | ::: | + | |
- | | ::: | + | |
- | | ::: | + | |
- | | ::: | | + | |
- | | Echo Clock | | + | |
- | | ::: | ::: | + | |
- | | ::: | ::: | + | |
- | | ::: | | + | |
- | | ::: | | + | |
- | **Note 1**: The sampling rates in Single lane, 32-bit output formats in SDR mode are limited by the FPGA SPI engine. This is not a limitation of the AD4630/ | + | |
- | + | ||
- | ===== Software Developers Guide===== | + | |
- | Analog Devices supports the development of custom applications using the EVAL-AD4X30-XX system and are described in the [[resources: | + | |
- | <note tip> | + | |
- | + | ||
- | ===== Evaluation Board Support ===== | + | |
- | Technical support for the evaluation board hardware and software can be obtained by posting a question to ADI's [[ez> | + | |
- | \\ | + | |
- | The evaluation board schematic and other board files can be found on the [[adi> | + | |
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | + |