This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:demo:reference-designs:demo-ad5758-ao8z:software [11 Sep 2019 14:41] – Removed test edita Donal O''Sullivan | resources:demo:reference-designs:demo-ad5758-ao8z:software [11 Sep 2019 17:16] – Updated GUI S/W link Donal O''Sullivan | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Software ===== | ===== Software ===== | ||
==== Firmware Installation ==== | ==== Firmware Installation ==== | ||
- | The demo board comes with the latest version of the firmware pre-installed. If you would like to re-install the firmware or update to the latest version, please follow | + | The demo board comes with the latest version of the firmware pre-installed. If you would like to re-install the firmware or update to the latest version, please follow |
- | - Download the latest version of the [[adi>> | + | - Download the latest version of the Demo board firmware. This file is called "{{ : |
- Unzip this file. | - Unzip this file. | ||
- Install the latest version of the [[adi> | - Install the latest version of the [[adi> | ||
- | - Start CrossCore Serial Flash Programmer. | + | - Start the CrossCore Serial Flash Programmer. |
-Set Target to " | -Set Target to " | ||
- Select firmware file “adi5758_20180910.hex” in the <File to download> | - Select firmware file “adi5758_20180910.hex” in the <File to download> | ||
Line 15: | Line 15: | ||
- Hold down S2 (Boot) button while briefly pressing the S1 (Reset) button. Then release S2. (See Figure 1) //This sequence is important// | - Hold down S2 (Boot) button while briefly pressing the S1 (Reset) button. Then release S2. (See Figure 1) //This sequence is important// | ||
- On the CrossCore SFP, select the correct COM port. (//Be sure to select the correct COM port here. It is usually the highest COMnn.//) | - On the CrossCore SFP, select the correct COM port. (//Be sure to select the correct COM port here. It is usually the highest COMnn.//) | ||
- | - Press [Start] to program device. (If you get the message “Failed to open serial device”, then repeat step d above, taking care to follow the exact button press sequence.) | + | - Press [Start] to program device. (If you get the message “Failed to open serial device”, then repeat step 5 above, taking care to follow the exact button press sequence.) |
- | | + | |
{{: | {{: | ||
</ | </ | ||
Line 24: | Line 24: | ||
==== GUI Installation ==== | ==== GUI Installation ==== | ||
- | This section outline how to download and install the latest version of AD5758 Eight Channel Demo Board GUI software. You can skip this step if you already have the latest version installed which is version | + | This section outline how to download and install the latest version of AD5758 Eight Channel Demo Board GUI software. You can skip this step if you already have the latest version installed which is version |
These instructions are for installation on Windows-10 but should also work for Windows-7 with minor differences. | These instructions are for installation on Windows-10 but should also work for Windows-7 with minor differences. | ||
Line 30: | Line 30: | ||
=== Step-by-step guide === | === Step-by-step guide === | ||
- | - Download the latest version of the {{ : | + | - Download the latest version of the {{ : |
- | - Unzip the file "//ad575_8_channel_evaluation_software.zip//" | + | - Unzip the file "//ad5758_0911.zip//" |
- | - Double click the "//ad575_8_channel_evaluation_software.exe//" | + | - Double click the "//ad5758_0911/ |
- Click Next in the pop-up that appears. (See Figure 3) \\ < | - Click Next in the pop-up that appears. (See Figure 3) \\ < | ||
- Read carefully the License Agreement and click "I Agree" if you agree to its content. < | - Read carefully the License Agreement and click "I Agree" if you agree to its content. < |