Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:demo:reference-designs:demo-ad5758-ao8z:introduction [06 Aug 2019 16:54] – [Introduction] Donal O''Sullivan | resources:demo:reference-designs:demo-ad5758-ao8z:introduction [07 Aug 2019 15:31] – corrected spelling. valerie hamilton |
---|
====== AD5758 + ADP1031 Eight Channel Analog Output Module ====== | ====== AD5758 + ADP1031 Eight Channel Analog Output Module ====== |
===== Introduction ===== | ===== Introduction ===== |
When designing channel-to-channel isolated analog output modules for process control applications such as programmable logic controller (PLC) or distributed control system (DCS) modules, the main trade-off usually considered is //power dissipation// vs. //channel density//. As module sizes shrink, and channel density increases, the power dissipation budget per channel must decrease to accommodate the max power dissipation budget for the module. Higher channel density also means that there is less PCB real estate available for each channel. | When designing channel-to-channel isolated analog output modules for process control applications such as programmable logic controller (PLC) or distributed control system (DCS) modules, the main trade-off usually considered is //power dissipation// vs. //channel density//. As module sizes shrink, and channel density increases, the power dissipation budget per channel must decrease to accommodate the maximum power dissipation budget for the module. Higher channel density also means that there is less PCB real estate available for each channel. |
| |
{{:resources:demo:reference-designs:demo-ad5758-ao8z:01-08-2019_14-52-59.png|}} | {{:resources:demo:reference-designs:demo-ad5758-ao8z:01-08-2019_14-52-59.png|}} |
This Board is a demonstration a system level solution where the [[adi>http://www.analog.com/ad5758|AD5758]] and the [[adi>http://www.analog.com/adp1031|ADP1031]] can be used together to implement a compact, eight channel, channel-to-channel isolated, precision analog output (AO) module, while achieving less than 2 W worst case power dissipation over a wide range of operating condition. | This Board is a demonstration a system level solution where the [[adi>http://www.analog.com/ad5758|AD5758]] and the [[adi>http://www.analog.com/adp1031|ADP1031]] can be used together to implement a compact, eight channel, channel-to-channel isolated, precision analog output (AO) module, while achieving less than 2 W worst case power dissipation over a wide range of operating conditions. |
| |
The [[adi>http://www.analog.com/adp1031|ADP1031]] solves the isolation and size challenges and the [[adi>http://www.analog.com/ad5758|AD5758]] provides a low power dissipation, precision, configurable current or voltage output channel. | The [[adi>http://www.analog.com/adp1031|ADP1031]] solves the isolation and size challenges and the [[adi>http://www.analog.com/ad5758|AD5758]] provides a low power dissipation, precision, configurable current or voltage output channel. |