This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:alliances:digilent [09 Jan 2021 00:21] Robin Getz user interwiki links |
resources:alliances:digilent [08 Feb 2021 15:16] Iulia Moldovan Change broken link |
||
---|---|---|---|
Line 3: | Line 3: | ||
<WRAP column 45%> | <WRAP column 45%> | ||
[[http://www.digilentinc.com|{{:resources:digilent.png?100 }}]] Digilent Inc. is a leader in the design, manufacture, and world wide distribution of FPGA and microcontroller technologies. Since its founding in 2000, Digilent has grown to the point where our products can now be found in over 1000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs. | [[http://www.digilentinc.com|{{:resources:digilent.png?100 }}]] Digilent Inc. is a leader in the design, manufacture, and world wide distribution of FPGA and microcontroller technologies. Since its founding in 2000, Digilent has grown to the point where our products can now be found in over 1000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs. | ||
- | * [[http://www.digilentinc.com/Products/Catalog.cfm?Cat=10&FPGA|FPGA Boards]] | + | * [[https://store.digilentinc.com/digilent-system-boards-and-components/|FPGA Boards]] |
- | * [[http://www.digilentinc.com/Products/Catalog.cfm?Cat=9|Pmods]] | + | * [[https://store.digilentinc.com/boards-and-components/expansion-modules/pmods/|Pmods]] |
</WRAP> | </WRAP> | ||
Line 81: | Line 81: | ||
| [[adi>EVAL-AD9467|AD9467-FMC-250EBZ]] | [[http://www.digilentinc.com/Products/Detail.cfm?Prod=AD9467-FMC|{{http://www.digilentinc.com/Data/Products/AD9467-FMC/TILE_AD9467_150.jpg }}]] **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9467|View Reference Design]]\\ \\ The AD9467-FMC-250EBZ board is based on the AD9467, which is a 16-Bit, 250 MSPS analog-to-digital converter that. The AD9467 provides a new level of signal processing performance for test and measurement instrumentation, defense electronics, and communications applications where high resolution over a wide bandwidth is needed. | [[adi>AD9467]] [[adi>AD9517-4]] | | | [[adi>EVAL-AD9467|AD9467-FMC-250EBZ]] | [[http://www.digilentinc.com/Products/Detail.cfm?Prod=AD9467-FMC|{{http://www.digilentinc.com/Data/Products/AD9467-FMC/TILE_AD9467_150.jpg }}]] **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9467|View Reference Design]]\\ \\ The AD9467-FMC-250EBZ board is based on the AD9467, which is a 16-Bit, 250 MSPS analog-to-digital converter that. The AD9467 provides a new level of signal processing performance for test and measurement instrumentation, defense electronics, and communications applications where high resolution over a wide bandwidth is needed. | [[adi>AD9467]] [[adi>AD9517-4]] | | ||
| [[adi>EVAL-AD9265|AD9265-FMC-125EBZ]] |{{:resources:alliances:cf_ad9265_board.jpg?150 }} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9265|View Reference Design]]\\ \\ The AD9265-FMC-125EBZ board is based on the AD9265, which is a 16-Bit, 125 MSPS analog-to-digital converter (ADC) featuring a wide bandwidth differential sample-and-hold analog input amplifier supporting a variety of user-selectable input ranges. | [[adi>AD9265]] [[adi>AD9517-4]] | | | [[adi>EVAL-AD9265|AD9265-FMC-125EBZ]] |{{:resources:alliances:cf_ad9265_board.jpg?150 }} **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9265|View Reference Design]]\\ \\ The AD9265-FMC-125EBZ board is based on the AD9265, which is a 16-Bit, 125 MSPS analog-to-digital converter (ADC) featuring a wide bandwidth differential sample-and-hold analog input amplifier supporting a variety of user-selectable input ranges. | [[adi>AD9265]] [[adi>AD9517-4]] | | ||
- | | [[adi>EVAL-AD9739A|AD9739A-FMC-EBZ]] | [[http://www.digilentinc.com/Products/Detail.cfm?Prod=AD9739A-FMC|{{http://www.digilentinc.com/Data/Products/AD9739A-FMC/TILE_AD9739A_150.jpg }}]] **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9739a|View Reference Design]]\\ \\ The new AD9739A-FMC-EBZ board is based on the AD9739A is a 14-bit, 2.5 GSPS high performance RF DAC capable of synthesizing wideband signals from dc up to 3 GHz. | [[adi>AD9739A]] [[adi>ADF4350]] | | + | | [[adi>EVAL-AD9739A|AD9739A-FMC-EBZ]] | [[https://reference.digilentinc.com/ad9739a_fmc/ad9739a_fmc|{{http://www.digilentinc.com/Data/Products/AD9739A-FMC/TILE_AD9739A_150.jpg }}]] **Reference Design:** [[/resources/fpga/xilinx/fmc/ad9739a|View Reference Design]]\\ \\ The new AD9739A-FMC-EBZ board is based on the AD9739A is a 14-bit, 2.5 GSPS high performance RF DAC capable of synthesizing wideband signals from dc up to 3 GHz. | [[adi>AD9739A]] [[adi>ADF4350]] | |
| [[adi>ad-fmcomms1-ebz|AD-FMCOMMS1-EBZ]] |{{:resources:alliances:cf_xcomm_board.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms1-ebz|View Reference Design]]\\ \\ The AD-FMCOMMS1-EBZ is an analog front end hardware platform that addresses a broad range of research, academic, industrial and defense applications. The AD-FMCOMMS1-EBZ enables RF applications from 400MHz to 4 GHz. The module is customizable to a wide range of frequencies by software without any hardware changes, providing options for GPS or IEEE 1588 Synchronization, and MIMO configurations. | [[adi>AD9122]] [[adi>ADL5375]] [[adi>ADF4351]] [[adi>ADL5602]] [[adi>ADL5380]] [[adi>AD8366]] [[adi>AD9643]] [[adi>ADF4351]] [[adi>AD9548]] [[adi>AD9523-1]] | | | [[adi>ad-fmcomms1-ebz|AD-FMCOMMS1-EBZ]] |{{:resources:alliances:cf_xcomm_board.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms1-ebz|View Reference Design]]\\ \\ The AD-FMCOMMS1-EBZ is an analog front end hardware platform that addresses a broad range of research, academic, industrial and defense applications. The AD-FMCOMMS1-EBZ enables RF applications from 400MHz to 4 GHz. The module is customizable to a wide range of frequencies by software without any hardware changes, providing options for GPS or IEEE 1588 Synchronization, and MIMO configurations. | [[adi>AD9122]] [[adi>ADL5375]] [[adi>ADF4351]] [[adi>ADL5602]] [[adi>ADL5380]] [[adi>AD8366]] [[adi>AD9643]] [[adi>ADF4351]] [[adi>AD9548]] [[adi>AD9523-1]] | | ||
| [[adi>eval-ad-fmcomms2|AD-FMCOMMS2-EBZ]] |{{:resources:alliances:ad_fmcomms2_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms2-ebz|View Reference Design]]\\ \\ The AD-FMCOMMS2-EBZ is a high-speed analog module designed to showcase the AD9361, a high performance, highly integrated RF agile transceiver intended for use in RF applications, such as 3G and 4G base station applications and software defined radios. The AD-FMCOMMS2-EBZ provides RF engineers the ability to connect the AD9361 to a RF testbench (Vector Signal Analyzer, Signal generator, etc) and measure performance. The external components (which can easily be swapped) on the AD-FMCOMMS2-EBZ have a narrower RF tuning range 2400 – 2500 MHz. It is expected that most engineers will change these external components (pin for pin replacements from various vendors are available) for their specific application/ frequency of interest. Anyone interested in a wider tuning range board should look at the AD-FMCOMMS3-EBZ. | [[adi>AD9361]] | | | [[adi>eval-ad-fmcomms2|AD-FMCOMMS2-EBZ]] |{{:resources:alliances:ad_fmcomms2_ebz.jpg?150 }} **Reference Design:** [[/resources/eval/user-guides/ad-fmcomms2-ebz|View Reference Design]]\\ \\ The AD-FMCOMMS2-EBZ is a high-speed analog module designed to showcase the AD9361, a high performance, highly integrated RF agile transceiver intended for use in RF applications, such as 3G and 4G base station applications and software defined radios. The AD-FMCOMMS2-EBZ provides RF engineers the ability to connect the AD9361 to a RF testbench (Vector Signal Analyzer, Signal generator, etc) and measure performance. The external components (which can easily be swapped) on the AD-FMCOMMS2-EBZ have a narrower RF tuning range 2400 – 2500 MHz. It is expected that most engineers will change these external components (pin for pin replacements from various vendors are available) for their specific application/ frequency of interest. Anyone interested in a wider tuning range board should look at the AD-FMCOMMS3-EBZ. | [[adi>AD9361]] | |