This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
products:audio-video:analoghdmidvi-interfaces:adv8005:app-notes:combining-multiple-adv8005 [14 Mar 2016 23:42] – Dominic Bernique | products:audio-video:analoghdmidvi-interfaces:adv8005:app-notes:combining-multiple-adv8005 [15 Mar 2016 20:05] (current) – Dominic Bernique | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
- | Some applications can combine multiple | + | Some applications can combine multiple |
Example application: | Example application: | ||
Line 13: | Line 13: | ||
This is a mode where the output timing can be fractionally locked (to an accuracy of a few clock cycles) to the VS timing of the input video, even if the output resolution differs from the input resolution. Additionally, | This is a mode where the output timing can be fractionally locked (to an accuracy of a few clock cycles) to the VS timing of the input video, even if the output resolution differs from the input resolution. Additionally, | ||
- | **Advantages: | + | **Advantages: |
**Disadvantages: | **Disadvantages: | ||
Line 31: | Line 31: | ||
====== USE CASES ====== | ====== USE CASES ====== | ||
- | ===== Star Connected | + | ===== Star Connected ADV8005 Devices ===== |
This is typical of some video wall or signage applications. One source signal is sent through a splitter to multiple ADV8005 devices in multiple sinks. Each ADV8005 crops a portion of the image and upscales it to full-screen. For example, using 4 ADV8005 devices, each one processes top-left, top-right, bottom-left or bottom-right of the image and upscales it to full-screen. Outputs are not combined; they each drive their own display. | This is typical of some video wall or signage applications. One source signal is sent through a splitter to multiple ADV8005 devices in multiple sinks. Each ADV8005 crops a portion of the image and upscales it to full-screen. For example, using 4 ADV8005 devices, each one processes top-left, top-right, bottom-left or bottom-right of the image and upscales it to full-screen. Outputs are not combined; they each drive their own display. | ||
The requirement is that a scene change happening on the input will appear to the human eye to happen at the same time on all of the ADV8005 outputs. | The requirement is that a scene change happening on the input will appear to the human eye to happen at the same time on all of the ADV8005 outputs. | ||
+ | |||
{{ : | {{ : | ||
Line 41: | Line 42: | ||
- | Best solution: Use ADV8003 or ADV8005 in frame locked mode. | + | Best solution: Use ADV8005 in frame locked mode. |
- | ===== Daisy-Chained | + | ===== Daisy-Chained ADV8005 Devices ===== |
This is typical of some video wall or signage applications. One source signal is sent to ADV8005 devices in multiple sinks. They are connected in daisy-chain fashion. Each ADV8005 crops a portion of the image and upscales it to full-screen and outputs that on its output port. On its other output port, it passes through the input to the next ADV8005 device in the chain. For example using 4 ADV8005 devices, each one processes top-left, top-right, bottom-left or bottom-right of the image and upscales it to full-screen. Outputs are not combined; they each drive their own display. | This is typical of some video wall or signage applications. One source signal is sent to ADV8005 devices in multiple sinks. They are connected in daisy-chain fashion. Each ADV8005 crops a portion of the image and upscales it to full-screen and outputs that on its output port. On its other output port, it passes through the input to the next ADV8005 device in the chain. For example using 4 ADV8005 devices, each one processes top-left, top-right, bottom-left or bottom-right of the image and upscales it to full-screen. Outputs are not combined; they each drive their own display. |