This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
playground:playground [30 Oct 2012 22:16] – test Doug Ito | playground:playground [30 May 2013 21:15] – [Page Title Change] Andy Akers | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Page Title Change ====== | ====== Page Title Change ====== | ||
+ | < | ||
{{: | {{: | ||
Line 61: | Line 61: | ||
== Level 5 Headline == | == Level 5 Headline == | ||
+ | == Signal Picture == | ||
+ | {{: | ||
- | + | This is the CN-0196 Lab board. You can change the capacitors by resolder ones up to 50V specification instead of the used 25V electrolytic ones. | |