Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
first:adis16448_imu_frc [26 Dec 2018 03:30] – remove pardon our dust warning Kristen Chong | first:adis16448_imu_frc [11 Jan 2020 05:12] (current) – fix warning Kristen Chong |
---|
| <note important>After 2020, we will begin to phase out the ADIS16448 IMU in favor of the newer ADIS16470 with updated features. We strongly encourage teams that have not obtained one of the newer IMUs to consider getting one from FIRST Choice this year. The ADIS16448 IMU is still supported, but stock will be limited and library updates/releases for this device will be slower.</note> |
====== ADIS16448 IMU Board for FIRST Robotics ====== | ====== ADIS16448 IMU Board for FIRST Robotics ====== |
The [[adi>ADIS16448]] IMU board is ADI's rugged, tactical IMU designed for use in a wide variety of applications, including industrial robots, smart agriculture, and autonomous vehicles. The [[adi>ADIS16448]] is a 10 degree-of-freedom IMU, with 3-axis gyro, 3-axis accelerometer, 3-axis magnetometer, and a barometer. | The [[adi>ADIS16448]] IMU board is ADI's rugged, tactical IMU designed for use in a wide variety of applications, including industrial robots, smart agriculture, and autonomous vehicles. The [[adi>ADIS16448]] is a 10 degree-of-freedom IMU, with 3-axis gyro, 3-axis accelerometer, 3-axis magnetometer, and a barometer. |