This shows you the differences between two versions of the page.
Next revision | Previous revisionNext revisionBoth sides next revision | ||
eval:hmc8362_user_guide [10 Aug 2020 15:05] – created Kieran Barrett | eval:hmc8362_user_guide [10 Aug 2020 15:24] – [GETTING STARTED] Kieran Barrett | ||
---|---|---|---|
Line 19: | Line 19: | ||
====ONLINE RESOURCES==== | ====ONLINE RESOURCES==== | ||
- | HMC8362 data sheet | + | * HMC8362 data sheet |
- | HMC8364 data sheet | + | |
- | Linduino DC2026C Demo Manual | + | |
====GENERAL DESCRIPTION==== | ====GENERAL DESCRIPTION==== | ||
Line 28: | Line 28: | ||
====EV1HMC8362LP6G/ | ====EV1HMC8362LP6G/ | ||
- | + | {{ : | |
- | **Insert Photo*** | + | Figure 1. Evaluation Board |
====GETTING STARTED==== | ====GETTING STARTED==== | ||
===EVALUATION BOARD SETUP PROCEDURE=== | ===EVALUATION BOARD SETUP PROCEDURE=== | ||
To configure the EV1HMC8362LP6G or EV1HMC8364LP6G for the first time, perform the following steps. | To configure the EV1HMC8362LP6G or EV1HMC8364LP6G for the first time, perform the following steps. | ||
- | 1. Verify that the analog power supply that is used to power the evaluation board configured to allow an output of 6.0 V and 200 mA of compliance current. | + | - Verify that the analog power supply that is used to power the evaluation board configured to allow an output of 6.0 V and 200 mA of compliance current. |
- | 2. Disable the power supply output. | + | |
- | 3. Using a double shielded BNC cable and a BNC to SMA adapter, connect the analog power supply to J1. | + | |
- | 4. Use the supplied shorting jumpers to configure the logic, as shown in Figure 2. In the configuration shown in Figure 2, the ADG1604 multiplexer, | + | |
- | 5. Connect the low noise, variable power supply to the SMA connector on the tuning port (J2) using a double shielded BNC cable and a BNC to SMA adapter. Torque this connection to 8 in/lb using an SMA torque wrench. | + | |
- | 6. Connect a 50 Ω RF cable capable of mating to the 2.92 mm K connector at J3 and torque this connection to 8 in/lb. Connect the other end of the cable to a signal source analyzer. | + | |
- | 7. Enable the 6 V power supply. Approximately 103 mA is drawn if the part is configured correctly. | + | |
- | 8. Enable the variable power supply and adjust the tuning voltage to within the range of the VCO band being used. | + | |
- | 9. Verify that the correct output frequency is observed on the signal source analyzer. An example using the HMC8362 is outlined in the Evaluation and Test section. | + | |
- | + | {{ : | |
- | ***Insert | + | Figure |
====EVALUATION BOARD HARDWARE==== | ====EVALUATION BOARD HARDWARE==== |