This is an old revision of the document!
Quick Start Guide for Testing the AD9213 Customer Evaluation Board AD9213-10GEBZ-B Using the ADS8-V1EBZ FPGA-Based Capture Board
Typical Setup
Figure 1. AD9213-10GEBZ-B Evaluation Board and ADS8-V1EBZ Data Capture Board, default configuration with external clocks.
Configuration for External Clocks
New photos and information here
Equipment Needed
Helpful Documents
Software Needed
Board Design and Integration Files
<These will all need to change.>
Testing
-
-
Close ACE.
Install jumper on P3 as shown below.
Figure 2. AD9213-10GEBZ-B standoff and jumper locations.
You can install standoffs at the locations (marked with an *) if needed. Alternatively, you can use foam sheets to support the board.
Connect the AD9213/9217 evaluation board to the ADS8-V1EBZ board together as shown in the following figure.
Figure 3. Connecting the AD9213-10GEBZ-B to ADS8-V1-EBZ.
Align the FMC+ connectors and apply even pressure across the connector and press the FMC connector on to its counterpart on the FPGA board.
Connect signal, clocks (optional), power and
USB cables to the boards as shown in Figure 1.
Signal (J1A): The frequency and amplitude of the test signal depend on the type of test you are performing. Full scale is typically achieved at 9dBm – 12dBm signal power at the signal generator (depending on the frequency, and insertion loss of the filter used). If in doubt about which amplitude to use, start with a lower amplitude (for example, 4dBm at the signal generator) and work up or down from there.
Optional Sample clock (J6): The sample clock works well across a wide range of amplitudes (1dBm – 10dBm at the signal generator). Because jitter performance is likely to improve as the slew rate increases, choose an amplitude towards the upper end of the stated range.
Optional FPGA Reference Clock (ADS8-V1EBZ J1): Similar to the sample clock, the reference clock works well across a wide range of amplitudes (1dBm – 10dBm at the signal generator). Unlike the sample clock, the reference clock is not sensitive to jitter/phase noise. Any signal generator that meets the frequency and power requirements works. For AD9213, the frequency of the reference clock is the (output digital data rate)/20. For AD9217, the frequency of the reference clock is the (output digital data rate)/16. The FPGA reference clock must be synchronized with the ADC sample clock.
Example: For the default JESD204B output configuration of AD9213-10GEBZ (L = 16, N’ = 16,
M = 1) at 10Gsps, the output data rate is 12.5Gbps. Reference clock frequency =12.5G/20 = 625MHz.
Example: For AD9213-6GEBZ, ACE brings the part up in 8-Lane mode. In this case (L = 8, N’ = 16,
M = 1) at 6Gsps, the output data rate is 15Gbps. Reference clock frequency = 15G/20 = 750MHz.
Connect the
USB cable from the ADS8-V1EBZ FPGA board to the Windows PC that has ACE installed.
Power on the ADS8-V1EBZ FPGA board using the switch S4. Wait several seconds after powering on the ADS8-V1EBZ, until DS17 flashes and the FPGA fan has stopped spinning.
Start ACE from Start→Programs→Analog Devices→ACE.
ACE will auto-detect the AD9213 or AD9217 board and bring up the correct ACE plugin, which will appear in the upper left portion of the
GUI. If the plugin does not appear in the upper left, select Plug-in Marketplace and select AD9213-10GEBZ-B, AD9213-6GEBZ-B, AD9217-10GEBZ-B or AD9217-6GEBZ-B, and add the selected plugin.
Double click on the AD9213 or AD9217 part number in the plugin icon in the upper left of the
GUI.
“Unknown” initially appears in the lower left corner. Wait until “Unknown” changes to “Good.”
After “State=Good” appears in the lower left, turn on the signal generators for the clock, reference clock, and signal.
Open the menu “Initial Configuration”.
Open the Initial Configuration menu to apply the default configuration settings.
Click the Apply button to configure AD9213 in its default configuration. Then double-click on the chip to proceed.
Apply default settings in the Initial Configuration menu before double-clicking on the chip.
“Output Interface
PLL Locked” will appear green. Confirm that “Common mode” is set to “Startup: Internal VCM Control” and then click “Proceed to Analysis
The Analysis page appears. Click “Run Once” to get a time domain view at the converted data.
The time domain analysis of converted data appears.
Click on the FFT icon to display the frequency domain view (FFT).
Analysis Page with Time Domain Data
Click “Run Continuously” to view repetitive FFTs.
Notes