This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
ad9213_ce [13 Mar 2021 02:21] – changed photo of jumper connections Eileen Staskunas | ad9213_ce [24 Mar 2021 00:30] – added open the initial configuration menu and photo Eileen Staskunas | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Quick Start Guide for Testing the AD9213/9217 ADC Evaluation Board Using the ADS8-V1EBZ FPGA-Based Capture Board ====== | + | ====== |
===== Typical Setup ===== | ===== Typical Setup ===== | ||
Line 51: | Line 51: | ||
- Power on the ADS8-V1EBZ FPGA board using the switch S4. Wait several seconds after powering on the ADS8-V1EBZ, until DS17 flashes and the FPGA fan has stopped spinning. | - Power on the ADS8-V1EBZ FPGA board using the switch S4. Wait several seconds after powering on the ADS8-V1EBZ, until DS17 flashes and the FPGA fan has stopped spinning. | ||
- Start ACE from Start-> | - Start ACE from Start-> | ||
- | - ACE will auto-detect the AD9213 or AD9217 board and bring up the correct ACE plugin, which will appear in the upper left portion of the GUI. If the plugin does not appear in the upper left, select Plug-in Marketplace and select AD9213-10GEBZ, | + | - ACE will auto-detect the AD9213 or AD9217 board and bring up the correct ACE plugin, which will appear in the upper left portion of the GUI. If the plugin does not appear in the upper left, select Plug-in Marketplace and select AD9213-10GEBZ, |
- Double click on the AD9213 or AD9217 part number in the plugin icon in the upper left of the GUI. | - Double click on the AD9213 or AD9217 part number in the plugin icon in the upper left of the GUI. | ||
- | - " | + | - " |
- After “State=Good” appears in the lower left, turn on the signal generators for the clock, reference clock, and signal. | - After “State=Good” appears in the lower left, turn on the signal generators for the clock, reference clock, and signal. | ||
- | - Double-click the AD9213/ | + | - |
- | - Click the Apply button to configure AD9213 in its default configuration.{{ :resources: | + | - Click the Apply button to configure AD9213 in its default configuration.{{ :ad9213_ce_apply_default_config.png}}< |
* AD9213 DDC and NCO controls are added to the configuration wizard. The following image shows a summary of the settings.{{ : | * AD9213 DDC and NCO controls are added to the configuration wizard. The following image shows a summary of the settings.{{ : | ||
- Click the " | - Click the " |