This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:interposer:adf4106 [31 Oct 2013 10:59] – Fix some typos. Istvan Csomortani | resources:fpga:xilinx:interposer:adf4106 [09 Jan 2021 00:49] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 27: | Line 27: | ||
* [[adi> | * [[adi> | ||
* [[adi>/ | * [[adi>/ | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 35: | Line 35: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
* **EVAL-ADF4106SD1Z** evaluation board | * **EVAL-ADF4106SD1Z** evaluation board | ||
Line 48: | Line 48: | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
\\ | \\ | ||
- | * **ADF4106 Driver:** https:// | + | * **ADF4106 Driver:** https:// |
* **ADF4106 Commands:** https:// | * **ADF4106 Commands:** https:// | ||
* **Xilinx Boards Common Drivers:** https:// | * **Xilinx Boards Common Drivers:** https:// | ||
Line 69: | Line 69: | ||
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| **help?** | Displays all available commands. | | | **help?** | Displays all available commands. | | ||
- | | **setregister=** | Update the selected latch with the current set ups. Accepted value:\\ latch:\\ 0 - Reference latch\\ 1 - N Counter Latch\\ 2 - Function Latch\\ 3 - Initialization Latch\\ value:\\ 24 bit values, you can find more information about the registers in the data sheet | | + | | **register=** | Update the selected latch with the current set ups. Accepted value:\\ latch:\\ 0 - Reference latch\\ 1 - N Counter Latch\\ 2 - Function Latch\\ 3 - Initialization Latch\\ value:\\ 24 bit values, you can find more information about the registers in the data sheet | |
- | | **getregister?** | Print the specified latch values in a human readable format. Accepted value:\\ latch:\\ 0 - Reference latch\\ 1 - N Counter Latch\\ 2 - Function Latch\\ 3 - Initialization Latch | | + | | **register?** | Print the specified latch values in a human readable format. Accepted value:\\ latch:\\ 0 - Reference latch\\ 1 - N Counter Latch\\ 2 - Function Latch\\ 3 - Initialization Latch | |
- | | **setfrequency=** | Set the VCO frequency. Accepted value:\\ 5 .. 6000 - betwwen 5Mhz and 6Ghz | | + | | **frequency=** | Set the VCO frequency. Accepted value:\\ 5 .. 6000 - betwwen 5Mhz and 6Ghz | |
- | | **getfrequency?** | Print the actual VCO frequency. | | + | | **frequency?** | Print the actual VCO frequency. | |
Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA. | Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA. |