world leader in high performance signal processing
This version (07 Mar 2013 03:03) was approved by mfowler.The Previously approved version (25 May 2012 21:12) is available.Diff

Debugging the DPG 2/3

DPGDownloader Only Shows Generic Eval

Verify Driver Installation

Ensure that the DPG2 and the eval board are detected in the Device Manager: If the two devices do not appear as shown, reinstall the latest version of DPGDownloader.

Verify DLL File is Present

Verify that the appropriate DLL for your evaluation board is present in: C:\Program Files (x86)\Analog Devices\DPG\ the file is named: AnalogDevices.DPG.EvalBoard.ADXXXX.dll where XXXX is the part number of your evaluation board. If the file is not present install the DAC update file for your evaluation board.