This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:dpg:debugging [25 May 2012 21:12] – [Restart Evaluation Board service] Michael Fowler | resources:eval:dpg:debugging [07 Mar 2013 03:03] (current) – [Restart Evaluation Board Service] Michael Fowler | ||
---|---|---|---|
Line 4: | Line 4: | ||
Ensure that the DPG2 and the eval board are detected in the Device Manager:{{ : | Ensure that the DPG2 and the eval board are detected in the Device Manager:{{ : | ||
If the two devices do not appear as shown, reinstall the latest version of DPGDownloader. | If the two devices do not appear as shown, reinstall the latest version of DPGDownloader. | ||
- | ==== Restart Evaluation Board Service ==== | + | |
- | Open the Start Menu, click Run, then type services.msc, | + | |
- | Select the Analog Devices Evaluation Board Service and click Restart the Service. | + | |
==== Verify DLL File is Present ==== | ==== Verify DLL File is Present ==== | ||
Verify that the appropriate DLL for your evaluation board is present in: C:\Program Files (x86)\Analog Devices\DPG\ | Verify that the appropriate DLL for your evaluation board is present in: C:\Program Files (x86)\Analog Devices\DPG\ | ||
the file is named: AnalogDevices.DPG.EvalBoard.ADXXXX.dll where XXXX is the part number of your evaluation board. If the file is not present install the DAC update file for your evaluation board. | the file is named: AnalogDevices.DPG.EvalBoard.ADXXXX.dll where XXXX is the part number of your evaluation board. If the file is not present install the DAC update file for your evaluation board. |