The AD9837 is a low power, programmable waveform generator capable of producing sine, triangular, and square wave outputs. Waveform generation is required in various types of sensing, actuation, and time domain reflectometry (TDR) applications. The output frequency and phase are software programmable, allowing easy tuning. The frequency registers are 28 bits: with a 16 MHz clock rate, resolution of 0.06 Hz can be achieved; with a 5 MHz clock rate, the AD9837 can be tuned to 0.02 Hz resolution.
The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for Renesas platforms.
HW Platform(s):
The driver contains two parts:
The Communication Driver has a standard interface, so the AD9837 driver can be used exactly as it is provided.
There are three functions which are called by the AD9837 driver:
SPI driver architecture
The following functions are implemented in this version of AD9837 driver:
Function | Description |
---|---|
unsigned char AD9837_Init(void) | Initializes the SPI communication peripheral and resets the part. |
void AD9837_Reset(void) | Sets the Reset bit of the AD9837. |
void AD9837_ClearReset(void) | Clears the Reset bit of the AD9837. |
void AD9837_SetRegisterValue(unsigned short regValue) | Writes the value to a register. |
void AD9837_SetFrequency(unsigned short reg, unsigned long val) | Writes to the frequency registers. |
void AD9837_SetPhase(unsigned short reg, unsigned short val) | Writes to the phase registers. |
void AD9837_Setup(unsigned short freq, unsigned short phase, unsigned short type); | Selects the Frequency,Phase and Waveform type. |
This section contains a description of the steps required to run the AD9837 demonstration project on a Renesas RL78G13 platform.
An EVAL-AD9837SDZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RL78G13:
EVAL-AD9837SDZ test point FSYNC → YRDKRL78G13 J11 connector Pin 1 EVAL-AD9837SDZ test point SDATA → YRDKRL78G13 J11 connector Pin 2 EVAL-AD9837SDZ test point SCLK → YRDKRL78G13 J11 connector Pin 4 EVAL-AD9837SDZ J3 connector connector DGND → YRDKRL78G13 J11 connector Pin 5 EVAL-AD9837SDZ J3 connector connector DVDD → YRDKRL78G13 J11 connector Pin 6 EVAL-AD9837SDZ J4 connector connector AGND → YRDKRL78G13 J11 connector Pin 5 EVAL-AD9837SDZ J4 connector connector AVDD → YRDKRL78G13 J11 connector Pin 6
With the Applilet3 for RL78G13 tool the following peripherals have to be configured:
Choose to generate the Transmit/receive function for the CSI10 and configure the interface with the following settings:
Configure TM00 as an interval timer:
Disable the watchdog timer:
The demo program sets up the AD9837 part to output sinusoidal, triangle and square waves. The frequency and the type of wave are displayed on the LCD.
This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RL78G13 for controlling and monitoring the operation of the ADI part.
Two software applications have to be used: Applilet3 for RL78G13 (a tool that automatically generates device drivers for MCU peripheral functions) and IAR Embedded Workbench for Renesas RL78 (the integrated development environment).
This section contains a description of the steps required to run the AD9837 demonstration project on a Renesas RX62N platform.
An EVAL-AD9837SDZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N:
EVAL-AD9837SDZ test point SDATA → YRDKRX62N J8 connector Pin 19 EVAL-AD9837SDZ test point SCLK → YRDKRX62N J8 connector Pin 20 EVAL-AD9837SDZ test point FSYNC → YRDKRX62N J8 connector Pin 15 EVAL-AD9837SDZ J4 connector Pin AVDD → YRDKRX62N J8 connector Pin 3 EVAL-AD9837SDZ J3 connector Pin DVDD → YRDKRX62N J8 connector Pin 3 EVAL-AD9837SDZ J4 connector Pin AGND → YRDKRX62N J8 connector Pin 4 EVAL-AD9837SDZ J3 connector Pin DGND → YRDKRX62N J8 connector Pin 4
The demo program sets up the AD9833 part to output sinusoidal, triangle and square waves. The frequency and the type of wave are displayed on the LCD.
This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RX62N for controlling and monitoring the operation of the ADI part.