This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:pmod:adxl345 [27 Jan 2012 16:34] – Approved Robin Getz | resources:fpga:xilinx:pmod:adxl345 [09 Jan 2021 00:57] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== ADXL345 | + | ====== ADXL345 Pmod Xilinx |
===== Introduction ===== | ===== Introduction ===== | ||
- | The [[adi> | + | The [[adi> |
- | **HW Platform(s): | + | **HW Platform(s): |
- | **System:** Microblaze, AXI, UART \\ | + | * [[xilinx>products/ |
+ | | ||
+ | | ||
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
- | The bit file provided in the project *.tar.gz | + | The bit file provided in the project *.zip file combines the FPGA bit file and the SDK elf files. It may be used for a quick check on the system. All you need is the hardware and a PC running a UART terminal and the programmer (IMPACT). |
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * LX9 microboard | + | * [[xilinx> |
- | * PMOD-ACL | + | * [[http:// |
+ | * [[http:// | ||
+ | * [[http:// | ||
==== Required Software ==== | ==== Required Software ==== | ||
- | * Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). |
- | * A UART terminal (Tera Term/ | + | * A UART terminal (Tera Term/ |
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <note tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ |
- | </note> | + | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// |
+ | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// | ||
- | Extract the project from the archive file (cf_adxl345.tar.gz) to the location you desire. | + | ==== Avnet LX9 MicroBoard Setup ==== |
- | To begin, connect | + | Extract |
- | + | ||
- | {{: | + | |
- | Start IMPACT, and initialze | + | To begin, connect |
- | {{: | + | {{: |
- | If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. After programming the ADXL345 device, the program continously monitors the X, Y and Z axes values as well as single tap, double tap and free fall detection. You may quit the program any time by pressing ' | + | ==== Digilent Nexys™3 Spartan-6 FPGA Board ==== |
- | {{: | + | Extract the project from the archive file (ADXL345_< |
- | {{: | + | |
- | {{: | + | To begin, connect the PmodACL to JA connector of NEXYS3 board (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART). |
+ | |||
+ | {{: | ||
+ | |||
+ | ==== Avnet ZedBoard ==== | ||
+ | |||
+ | To begin, connect the PmodACL to JA1 connector of ZedBoard (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART). | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ==== FPGA Configuration for Nexys3 and LX-9 MicroBoard ==== | ||
+ | |||
+ | Start IMPACT, and double click " | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ==== FPGA Configuration for ZedBoard ==== | ||
+ | |||
+ | Run the **download.bat** script from the "../bin" folder downloaded from the github (see the links in the download section of the wiki page). | ||
+ | The script will automatically configure the ZYNQ SoC and download the *.elf file afterwards. | ||
+ | |||
+ | <WRAP center round tip 80%> | ||
+ | If the download script fails to run, modify the Xilinx Tools path in **download.bat** to match your Xilinx Installation path. | ||
+ | </WRAP> | ||
+ | |||
+ | If programming was successful, the **Main Menu** will apear in your UART terminal, as seen in the picture below. There are 7 options. Pressing [e], [d], [a], [s], [r], [t] or [q] key will allow you to select the desired option. | ||
+ | After the end of every option, all the possible options (the Menu) will be shown again, allowing the user to make a new choice. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Enable Measurement** sets the ADXL345 into measurement mode. Any measurement that takes place from that moment on will be valid data. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Disable Measurement** sets the ADXL345 into standby mode. Any measurement that takes place from that moment will not be valid data (usually 0). | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Display Acceleration** displays acceleration data on all 3 Axes. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Select Measurement Range** allows choosing between 4 options: ±2g, ±4g, ±8g and ±16g. Desired measurement range is selected by pressing [1] to [4]. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Change Acquisition Rate** allows choosing different Acquisition rates for the ADXL345. Desired option is selected by pressing [1] to [9]. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Select Tap Interrupts** allows enabling or disabling tap interrupts. Desired option is selected by pressing [1] to [4]. If the tap option selected is [1] or [3], after a single tap, D2 (LX9) / LD0 (Nexys3 and ZedBoard) will be ON. If the tap option selected is [2] or [3], after two consecutive taps, D3 and D2 (LX9) / LD1 and LD0 (Nexys3 and ZedBoard) will both be on at the same time. If the tap option selected is [4], no LEDs will be ON after a single or double tap. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Stop any ongoing action** will stop any display of measurements and afterwards display the Main Menu. | ||
+ | |||
+ | {{: | ||
===== Using the reference design ===== | ===== Using the reference design ===== | ||
Line 47: | Line 105: | ||
==== Functional Description ==== | ==== Functional Description ==== | ||
- | The reference design is a simple | + | The reference design is a SPI interface |
- | The hardware supports both 12 pin and 6 pin connections. | ||
- | The hardware SPI access allows read or write of any ADXL345 registers via the address, write and read data registers. A status output is connected to the 4 LED(s) on board as follows :- | ||
- | STATUS_FF_ST: | + | <WRAP round important 80%> |
- | STATUS_FF_DT: | + | \\ |
- | STATUS_XY: | + | |
- | STATUS_Z: Z axis change \\ | + | |
+ | \\ | ||
+ | </ | ||
- | In most cases, a simple SPI access is all the software need. However, | + | <WRAP round important 80%> |
+ | When using the ZedBoard reference design | ||
- | The hardware supports three modes of operation: | + | <code c> |
+ | // Select between PS7 or AXI Interface | ||
+ | #define USE_PS7 1 | ||
+ | // SPI used in the design | ||
+ | #define USE_SPI 1 | ||
+ | // I2C used in the design | ||
+ | #define USE_I2C 0 | ||
+ | // Timer (+interrupts) used in the design | ||
+ | #define USE_TIMER 1 | ||
+ | // External interrupts used in the design | ||
+ | #define USE_EXTERNAL | ||
+ | // GPIO used in the design | ||
+ | #define USE_GPIO | ||
+ | </ | ||
- | Software triggered: In this mode, software must initiate the read to update the mirrored registers. | + | </ |
- | Interrupt triggered: In this mode, ADXL345' | + | ===== Downloads ===== |
- | Free run: In this mode, hardware free runs and continously updates the mirrored registers. \\ | + | <WRAP round download 80%> |
+ | \\ | ||
+ | **Avnet LX-9 MicroBoard: **\\ | ||
+ | * {{:resources: | ||
- | ==== Registers ==== | + | **Digilent Nexys™3:**\\ |
- | ^ QW Address< | + | * {{:resources:fpga:xilinx:pmod:adxl345_nexys3.zip|Reference design |
- | | 0x00 | 7 | 0 | mode | Free run (0x1) or sw/hw controlled (0x0). | | + | |
- | | | 6 | 0 | int_inv | Invert (0x1) interrupt pins. | | + | |
- | | | 5 | 0 | access | + | |
- | | | 4 | 0 | trigger | Software trigger, requires a 0x0 to 0x1 transition. | | + | |
- | | | 3:0 | 0 | status | Software status, ignored if hardware is active. | | + | |
- | | 0x01 | 31 | 0 | rwn | SPI access, read (0x1) or write (0x0). | | + | |
- | | | 29:24 | 0 | addr | SPI access, address. | | + | |
- | | | 23:16 | 0 | wdata | SPI access, write data. | | + | |
- | | | 15 | 0 | done | SPI access, complete (0x1) or busy (0x0). | | + | |
- | | | 7:0 | 0 | rdata | SPI access, read data. | | + | |
- | | The following registers are provided for simultaneous access in free run and interrupt triggered modes ||||| | + | |
- | | 0x03 | 15:0 | 0 | x_axis | X Axis data. | | + | |
- | | 0x04 | 15:0 | 0 | y_axis | Y Axis data. | | + | |
- | | 0x05 | 15:0 | 0 | z_axis | Z Axis data. | | + | |
- | | 0x06 | 15:0 | 0 | x_axis | ACT/TAP data. | | + | |
- | | 0x07 | 15:0 | 0 | x_axis | INT source | + | |
- | | 0x08 | 15:0 | 0 | x_axis | FIFO status data. | | + | |
- | | 0x09 | 3:0 | 0 | state | Hw state (for debug purposes only). | | + | |
- | | 1. For AXI-Lite byte addresses, multiply by 4. ||||| | + | |
+ | **Avnet ZedBoard: | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | | ||
+ | </ | ||
+ | <wrap hide> | ||
+ | ====== Linux Device Driver ====== | ||
+ | Connect PmodACL to the JA1 connector of the ZedBoard (upper row of pins). | ||
- | ==== Notes ==== | + | ===== Preparing the SD Card ===== |
- | PMOD-ACL must be connected | + | In order to prepare the SD Card for booting Linux on the ZedBoard: |
- | UART must be set to 115200 baudrate. \\ | + | * Download the device tree: [[https:// |
+ | * Configure the kernel | ||
+ | * Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step and the kernel configuration above | ||
+ | * [[/ | ||
- | **A debug data and trigger port is provided for internal monitoring of all the signals in the design.** | + | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. |
+ | If everything | ||
- | ===== Downloads ===== | + | There are 2 ways to test the driver. |
+ | * Using the terminal window | ||
+ | * Using a serial terminal | ||
- | {{: | + | ===== Using the terminal window ===== |
- | ===== More information ===== | + | Open a new terminal window by pressing |
- | | + | |
+ | Navigate to the location of the device and identify it using the following commands: | ||
+ | < | ||
+ | cd / | ||
+ | ls | ||
+ | spi32765.0 | ||
+ | cd spi32766.0 | ||
+ | cat modalias | ||
+ | spi:adxl34x | ||
+ | </ | ||
+ | If the **cat name** command doesn' | ||
+ | < | ||
+ | cd .. | ||
+ | cd spi32765.0 | ||
+ | cat modalias | ||
+ | </ | ||
+ | To see the list of options that the ADXL345 driver provides, type: | ||
+ | < | ||
+ | ls | ||
+ | autosleep | ||
+ | calibrate | ||
+ | </ | ||
+ | |||
+ | To calibrate the device, type: | ||
+ | < | ||
+ | echo 1 > calibrate | ||
+ | cat calibrate | ||
+ | 4,3,-218 | ||
+ | </ | ||
+ | |||
+ | To read the position, type: | ||
+ | < | ||
+ | cat position | ||
+ | (1, 0, 1) | ||
+ | </ | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The commands written above can also be used if not using an HDMI monitor and a wireless keyboard, by using a serial terminal, and typing the commands after the system boot-up is complete. | ||
+ | |||
+ | {{: | ||
+ | </ | ||
+ | ===== More information ===== | ||
+ | * [[ez> | ||
+ | * Example questions: {{rss> |