This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:pmod:ad7476a [08 Jun 2012 16:54] – fpga configuration Alexandru.Tofan | resources:fpga:xilinx:pmod:ad7476a [09 Jan 2021 00:49] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | |||
====== AD7476A Pmod Xilinx FPGA Reference Design ====== | ====== AD7476A Pmod Xilinx FPGA Reference Design ====== | ||
Line 8: | Line 7: | ||
Two reference designs are available for this part: | Two reference designs are available for this part: | ||
* A design which shows how to program the **AD7476A ADC** and acquire data from it. | * A design which shows how to program the **AD7476A ADC** and acquire data from it. | ||
- | | + | * **HW Platform(s): |
- | * [[http://www.xilinx.com/products/ | + | |
- | * [[http:// | + | |
- | * [[http:// | + | |
- | * **System:** Microblaze, AXI, UART \\ | + | |
- | | + | |
- | * **HW Platform(s): | + | * **HW Platform(s): |
- | * **System:** Microblaze, AXI, UART \\ | + | |
+ | | ||
====== AD7476A Pmod Reference Design ====== | ====== AD7476A Pmod Reference Design ====== | ||
+ | |||
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
Line 23: | Line 23: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
- | * [[http:// | + | * [[http:// |
+ | * [[http:// | ||
* [[http:// | * [[http:// | ||
==== Required Software ==== | ==== Required Software ==== | ||
- | * Xilinx ISE 13.2 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). |
- | * A UART terminal (Tera Term/ | + | * A UART terminal (Tera Term/ |
+ | * Linux Distribution for compiling the kernel (only required for Linux Device Drivers) | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <note tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP center round tip 80%>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ |
- | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// | + | If you are not familiar with Nexys™3 and/or Xilix tools, please visit\\ [[http:// |
- | </note> | + | If you are not familiar with ZedBoard and/or Xilix tools, please visit\\ [[http:// |
- | Extract the project from the archive file (AD7476A_< | + | |
==== Avnet LX9 MicroBoard Setup ==== | ==== Avnet LX9 MicroBoard Setup ==== | ||
- | To begin, connect the PmodAD1 to J5 connector of LX9 board, pins 1 to 6 (see image below). You can use an extension cable for ease of use. Connect the USB cables | + | |
+ | Extract the project from the archive file (AD7476A_< | ||
+ | |||
+ | To begin, connect the PmodAD1 to J5 connector of LX9 board (see image below). You can use an extension cable for ease of use. Connect the USB cable from the PC to the USB-UART female connector of the board for the UART terminal. The board will be programmed through its USB male connector. | ||
{{: | {{: | ||
==== Digilent Nexys™3 Spartan-6 FPGA Board ==== | ==== Digilent Nexys™3 Spartan-6 FPGA Board ==== | ||
- | To begin, connect the PmodAD1 to JA connector of Nexys™3 | + | |
+ | Extract the project from the archive file (AD7476A_< | ||
+ | |||
+ | To begin, connect the PmodAD1 to JA connector of NEXYS3 | ||
{{: | {{: | ||
- | ==== FPGA Configuration | + | ==== Avnet ZedBoard |
- | Start IMPACT, and double click " | + | To begin, connect the PmodAD1 to JD connector of ZedBoard (see image below). You can use an extension cable for ease of use. Connect the USB cables from the PC to the board, one for programming (Digilent USB device) and one for the UART terminal (FT232R USB UART). |
+ | |||
+ | {{: | ||
+ | |||
+ | ==== FPGA Configuration for Nexys3 and LX-9 MicroBoard ==== | ||
+ | |||
+ | Start IMPACT, and double click " | ||
{{: | {{: | ||
- | If programming was successful, you should be seeing messages appear on the terminal window as shown in the figure below. After programming the AD7476A device, the program will automatically read the values of the analog voltage inputs, Vin1 and Vin2, and print them via UART. Pressing | + | If programming was successful, you should be seeing messages appear on the terminal window as shown in the figure below. After programming the AD7476A device, the program will automatically read the values of the analog voltage inputs, Vin1 and Vin2, and print them via UART. Pressing |
{{: | {{: | ||
{{: | {{: | ||
+ | ==== FPGA Configuration for ZedBoard ==== | ||
+ | Run the **download.bat** script from the " | ||
+ | The script will automatically configure the ZYNQ SoC and download the *.elf file afterwards. | ||
+ | <WRAP center round tip 80%> | ||
+ | If the download script fails to run, modify the Xilinx Tools path in **download.bat** to match your Xilinx Installation path. | ||
+ | </ | ||
+ | |||
+ | If programming was successful, you should be seeing messages appear on the terminal window. After programming the AD7476A device, the program will automatically read the values of the analog voltage inputs, Vin1 and Vin2, and print the raw values via UART. | ||
===== Using the reference design ===== | ===== Using the reference design ===== | ||
==== Functional Description ==== | ==== Functional Description ==== | ||
- | The reference design is a simple SPI interface with multiplexed MISO pins for the AD7476A. The software programs the device | + | === Avnet LX-9 MicroBoard |
- | The hardware | + | The reference design is a custom |
- | <note important> | + | === Avnet ZedBoard === |
+ | |||
+ | The reference design is a custom SPI interface, with 2 MISO pins for the AD7476A ICs found on the PmodAD1 (PmodAD1 contains two AD7476A Integrated Circuits, which share the same CS and SCLK pins, but have separate MISO pins). The software programs the device, and afterwards, using DMA, transfers 8192 samples (4096 for Channel 1 and 4096 for Channel 2) and prints them on the UART. | ||
+ | |||
+ | <WRAP round 80% important> | ||
* Connecting the PmodAD1 to the LX-9 Board or Nexys™3 Board using an extension cable provides ease of use. | * Connecting the PmodAD1 to the LX-9 Board or Nexys™3 Board using an extension cable provides ease of use. | ||
- | * UART must be set to 57600 baudrate. | + | * UART must be set to 115200 Baud Rate for the Avnet LX-9 Microboard and ZedBoard or 9600 Baud Rate for the Digilent Nexys™3 Board. |
* The reference voltage for the AD7476A is 3.3V. | * The reference voltage for the AD7476A is 3.3V. | ||
- | </note> | + | </WRAP> |
===== Downloads ===== | ===== Downloads ===== | ||
- | {{: | + | |
- | {{: | + | <WRAP round download 80%> |
+ | \\ | ||
+ | **Avnet LX-9 MicroBoard: **\\ | ||
+ | * {{: | ||
+ | |||
+ | **Digilent Nexys™3: | ||
+ | * {{: | ||
+ | |||
+ | **Avnet ZedBoard: | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | * [[https:// | ||
+ | |||
+ | </ | ||
+ | <wrap hide> | ||
+ | ====== Linux Device Driver - Xilinx SPI Core ====== | ||
+ | |||
+ | Connect PmodAD1 to the JA1 connector of the ZedBoard (upper row of pins). | ||
+ | |||
+ | ===== Preparing the SD Card ===== | ||
+ | |||
+ | In order to prepare the SD Card for booting Linux on the ZedBoard: | ||
+ | * Download the device tree: [[https:// | ||
+ | * Follow the instructions on the following wiki page, but use the device tree downloaded on the previous step | ||
+ | * [[/ | ||
+ | |||
+ | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | ||
+ | If everything is correct, the system should boot up. If you don't have an HDMI monitor, connect to the board via UART, Baud Rate 115200. | ||
+ | |||
+ | There are 2 ways to test the driver. | ||
+ | * Using the terminal window | ||
+ | * Using the ADI IIO Oscilloscope | ||
+ | |||
+ | ===== Using the terminal window ===== | ||
+ | |||
+ | Open a new terminal window by pressing **Ctrl+Alt+T**. | ||
+ | |||
+ | Navigate to the location of the device and identify it using the following commands: | ||
+ | < | ||
+ | cd / | ||
+ | ls | ||
+ | iio:device0 iio:device1 trigger0 | ||
+ | cd iio\: | ||
+ | cat name | ||
+ | ad7476a | ||
+ | </ | ||
+ | |||
+ | If the **cat name** command doesn' | ||
+ | < | ||
+ | cd .. | ||
+ | cd iio\: | ||
+ | cat name | ||
+ | </ | ||
+ | |||
+ | To see the list of options that the AD7476A driver provides, type: | ||
+ | < | ||
+ | ls | ||
+ | buffer | ||
+ | dev | ||
+ | </ | ||
+ | |||
+ | To read the raw input voltage, type: | ||
+ | < | ||
+ | cat in_voltage0_raw | ||
+ | 2156 | ||
+ | </ | ||
+ | |||
+ | To read the scaled input voltage, type: | ||
+ | < | ||
+ | cat in_voltage_scale | ||
+ | 0.410000 | ||
+ | </ | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The commands written above can also be used if not using an HDMI monitor and a wireless keyboard, by using a serial terminal, and typing the commands after the system boot-up is complete. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ===== Using the ADI IIO Oscilloscope ===== | ||
+ | |||
+ | Install the ADI IIO Oscilloscope using the instructions from the following wiki page: | ||
+ | * [[/ | ||
+ | |||
+ | Launch the ADI IIO Oscilloscope. | ||
+ | |||
+ | Open the **Settings** menu and select **Impulse generator** submenu. A popup window will appear and allow you to select an impulse generator (a high resolution timer) and its frequency. The conversions for both the ADC and the DAC are started by the impulses of the generator. Click the **OK** button. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Select **ad7476a** from the **Device** drop-down menu. Click on **in_voltage0 Active channels**, and press the **Green Play Button**. Data will no be dislayed in the main plot window. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ====== Linux Device Driver - Custom HDL PCore ====== | ||
+ | |||
+ | Connect PmodAD1 to the JD1 connector of the ZedBoard (upper row of pins). | ||
+ | |||
+ | ===== Preparing the SD Card ===== | ||
+ | |||
+ | In order to prepare the SD Card for booting Linux on the ZedBoard: | ||
+ | * Download the device tree: [[https:// | ||
+ | * Download the Xilinx XPS project: [[https:// | ||
+ | * Download the AD7476A IPcore: [[https:// | ||
+ | * Download the project libraries: [[https:// | ||
+ | * Follow the instructions on the following wiki page, but use the device tree and project downloaded on the previous step | ||
+ | * [[/ | ||
+ | |||
+ | Make sure you have an HDMI monitor connected to the ZedBoard, plug in the SD Card and power on the board. | ||
+ | If everything is correct, the system should boot up. If you don't have an HDMI monitor, connect to the board via UART, Baud Rate 115200. | ||
+ | |||
+ | There are 2 ways to test the driver. | ||
+ | * Using the terminal window | ||
+ | * Using the ADI IIO Oscilloscope | ||
+ | |||
+ | ===== Using the terminal window ===== | ||
+ | |||
+ | Open a new terminal window by pressing **Ctrl+Alt+T**. | ||
+ | |||
+ | Navigate to the location of the device and identify it using the following commands: | ||
+ | < | ||
+ | cd / | ||
+ | ls | ||
+ | iio:device0 trigger0 | ||
+ | cd iio\: | ||
+ | cat name | ||
+ | AD7476A | ||
+ | </ | ||
+ | |||
+ | If the **cat name** command doesn' | ||
+ | < | ||
+ | cd .. | ||
+ | cd iio\: | ||
+ | cat name | ||
+ | </ | ||
+ | |||
+ | To see the list of options that the AD7476A driver provides, type: | ||
+ | < | ||
+ | ls | ||
+ | buffer | ||
+ | </ | ||
+ | |||
+ | To read the raw input voltage, type: | ||
+ | < | ||
+ | cd buffer | ||
+ | echo 100 > length | ||
+ | echo 1 > enable | ||
+ | hexdump -x / | ||
+ | 0000000 | ||
+ | 0000010 | ||
+ | 0000020 | ||
+ | 0000030 | ||
+ | 0000040 | ||
+ | 0000050 | ||
+ | 0000060 | ||
+ | </ | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The commands written above can also be used if not using an HDMI monitor and a wireless keyboard, by using a serial terminal, and typing the commands after the system boot-up is complete. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ===== Using the ADI IIO Oscilloscope ===== | ||
+ | |||
+ | Install the ADI IIO Oscilloscope using the instructions from the following wiki page: | ||
+ | * [[/ | ||
+ | |||
+ | Launch the ADI IIO Oscilloscope. | ||
+ | |||
+ | Select **AD7476A** from the **Device** drop-down menu. Set the desired number of samples in the **Sample Count** tab. Click the **Green Play Button** in order to start capturing and displaying data. Click **Stop** to stop the process. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | </ | ||
====== AD7476A Pmod and AD7303 Pmod Reference Design ====== | ====== AD7476A Pmod and AD7303 Pmod Reference Design ====== |