This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:kc705:adv7511 [18 Nov 2019 13:26] – Stanca-Florina Pop | resources:fpga:xilinx:kc705:adv7511 [08 Feb 2021 13:21] (current) – Change broken link Iulia Moldovan | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Introduction ===== | ===== Introduction ===== | ||
- | The [[adi> | + | The [[adi> |
===== Supported Carriers ===== | ===== Supported Carriers ===== | ||
Line 13: | Line 13: | ||
* [[xilinx> | * [[xilinx> | ||
* [[xilinx> | * [[xilinx> | ||
- | * [[http://zedboard.com/ | + | * [[xilinx> |
Line 29: | Line 29: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | To begin, connect an HDMI cable between the board HDMI out and the HDMI monitor. After the hardware setup, turn the power on to the board. | + | The following steps will get your system up and running. |
- | Run the **//evaluate.bat//** script. This script uses XMD to program the FPGA with the HDL Reference Design | + | - To begin, connect an HDMI cable between |
+ | - Download the [[adi> | ||
+ | - Build the HDL project according | ||
+ | - Choose the carrier board in the software by uncommenting the appropriate define in the **src/ | ||
+ | - Build the software project according to the [[https:// | ||
- | **Note: | + | < |
If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. | If programming was successful, you should be seeing messages appear on the terminal as shown in figure below. | ||
Line 49: | Line 53: | ||
=== Xilinx block diagram === | === Xilinx block diagram === | ||
- | {{resources: | + | {{resources: |
=== ADV7511 block diagram === | === ADV7511 block diagram === | ||
Line 56: | Line 60: | ||
The reference design consists of two independent pcore modules. | The reference design consists of two independent pcore modules. | ||
- | The video part consists of a Xilinx VDMA interface and the ADV7511 video interface. The ADV7511 interface consists of a 16bit YCbCr 422 with separate | + | The video part consists of an AXI DMAC interface and the ADV7511 video interface. The ADV7511 interface consists of a 16bit YCbCr 422 with separate |
The reference design defaults to the 1080p video mode. Users may change the video settings by programming the following registers. The core requires a corresponding pixel clock to generate the video. This clock must be generated externally. | The reference design defaults to the 1080p video mode. Users may change the video settings by programming the following registers. The core requires a corresponding pixel clock to generate the video. This clock must be generated externally. | ||
Line 76: | Line 80: | ||
A color pattern register provides a quick check of any RGB values on the monitor. If enabled, the register data is used as the pixel data for the entire frame. | A color pattern register provides a quick check of any RGB values on the monitor. If enabled, the register data is used as the pixel data for the entire frame. | ||
- | The audio part consists of a Xilinx DMA interface and the ADV7511 spdif audio interface. The audio clock is derived from the bus clock. A programmable register (see below) controls the division factor. The audio data is read from the DDR as two 16bit words for the left and right channels. It is then transmitted on the SPDIF frame. The sample frequency and format may be controlled using the registers below. The reference design defaults to 48KHz. | + | The audio part consists of an AXI DMAC interface and the ADV7511 spdif audio interface. The audio clock is derived from the bus clock. A programmable register (see below) controls the division factor. The audio data is read from the DDR as two 16bit words for the left and right channels. It is then transmitted on the SPDIF frame. The sample frequency and format may be controlled using the registers below. The reference design defaults to 48KHz. |
==== Registers ==== | ==== Registers ==== | ||
Line 106: | Line 110: | ||
The project contains 2 components: the Reference Design files and the ADV7511 Transmitter Library. All the components have to be downloaded from the links provided in the **Downloads** section. | The project contains 2 components: the Reference Design files and the ADV7511 Transmitter Library. All the components have to be downloaded from the links provided in the **Downloads** section. | ||
- | ==== Software | + | ==== Serial |
- | + | ||
- | Example for a ZC702 board: | + | |
- | * After [[http:// | + | |
- | * Open the Xilinx SDK for Vivado. When the SDK starts it asks to provide a folder where to store the workspace. Any folder can be provided. | + | |
- | * Go to // | + | |
- | {{ : | + | |
- | * Use a new hardware platform, so choose //**New**// in //**Target Hardware**// | + | |
- | {{ : | + | |
- | * At the **Target Hardware Specification** section browse the location of the hardware description file. This file's extension should be **.xml** or **.hdf**, and is located in the directory of the hdl design. **Note:** If the file does not exist, probably you forgot to make an **Export hardware** (in Vivado **File** -> **Export** -> **Export Hardware...**) | + | |
- | {{ : | + | |
- | * Then give a name to the project and click // | + | |
- | {{ : | + | |
- | * In the next window choose //**Empty Application**// | + | |
- | {{ : | + | |
- | * Now the project without source code looks like this | + | |
- | {{ : | + | |
- | * Then the no-OS software for the used FPGA board must be added from Github. Also the library must be added (ZC library for a Zynq based platform(except ZED), ZED library for a ZED platform or Microblaze library for AC701, | + | |
- | {{ : | + | |
- | * Afterwards click right on project name and go to // | + | |
- | {{ : | + | |
- | * In the window that appears, go to // | + | |
- | {{ : | + | |
- | * In the same window, go to // | + | |
- | {{ : | + | |
- | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the Console window will display the result of the build. If the build is not done automatically select the // | + | |
- | {{ : | + | |
- | * At this point the software project setup is complete, the FPGA can be programmed and the software can be downloaded into the system. You can program the FPGA by going to //**Xilinx Tools**// | + | |
- | {{ : | + | |
- | * Then choose this bitstream and press // | + | |
- | {{ : | + | |
- | * This window will appear next. | + | |
- | {{ : | + | |
- | * Afterwards a //Run Configuration// | + | |
- | {{ : | + | |
* The no-OS drivers source code does the following actions: | * The no-OS drivers source code does the following actions: | ||
Line 149: | Line 119: | ||
* This is what is transmitted through UART: | * This is what is transmitted through UART: | ||
{{ : | {{ : | ||
- | * The output of the example program can be viewed in the SDK console by enabling the //Connect STDIO Console// option and setting the baud rate of the UART port to 115200. | ||
- | {{ : | ||
As an alternative an UART terminal can be used to capture the output of the example program. The number of used UART port depends on the computer' | As an alternative an UART terminal can be used to capture the output of the example program. The number of used UART port depends on the computer' | ||
Line 164: | Line 132: | ||
The HDL Reference Designs and the no-OS Software can be downloaded from the Analog Devices Github.\\ | The HDL Reference Designs and the no-OS Software can be downloaded from the Analog Devices Github.\\ | ||
\\ | \\ | ||
- | |||
- | **Evaluation Scripts:** | ||
- | <WRAP round download 80%> | ||
- | * **AC701 Evaluation Script: ** [[https:// | ||
- | * **KC705 Evaluation Script: ** [[https:// | ||
- | * **VC707 Evaluation Script: ** [[https:// | ||
- | * **ZC702 Evaluation Script: ** [[https:// | ||
- | * **ZC706 Evaluation Script: ** [[https:// | ||
- | * **Zed Evaluation Script: ** [[https:// | ||
- | </ | ||
**HDL Reference Designs:** | **HDL Reference Designs:** | ||
Line 187: | Line 145: | ||
**no-OS Software:** | **no-OS Software:** | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
- | * **ADV7511 | + | * **ADV7511 |
- | * **ADV7511 AC701 Reference Design: ** https:// | + | |
- | * **ADV7511 KC705 Reference Design: ** https:// | + | |
- | * **ADV7511 VC707 Reference Design: ** https:// | + | |
- | * **ADV7511 ZC Library: ** https:// | + | |
- | * **ADV7511 ZC702 Reference Design: ** https:// | + | |
- | * **ADV7511 ZC706 Reference Design: ** https:// | + | |
- | * **ADV7511 ZedBoard Library: ** https:// | + | |
- | * **ADV7511 ZedBoard Reference Design: ** https:// | + | |
</ | </ | ||
<WRAP round help 80%> | <WRAP round help 80%> | ||
- | * Questions? [[https://ez.analog.com/ | + | * Questions? [[ez>community/ |
</ | </ | ||