This is an old revision of the document!
This document presents the steps to setup an environment for using the EVAL-CN0271-SDPZ evaluation board together with the Xilinx KC705 FPGA board, the Xilinx Embedded Development Kit (EDK) and the Micrium µC-Probe run-time monitoring tool. Below is presented a picture of the EVAL-CN0271-SDPZ Evaluation Board with the Xilinx KC705 board.
For component evaluation and performance purposes, as opposed to quick prototyping, the user is directed to Analog Devices System Demonstration Platform (SDP). The SDP consists of a:
The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. Each SDP evaluation daughter board includes the necessary installation files needed for this performance testing. It's expected that the analog performance on the two platforms may differ.
Below is presented a picture of SDP-B Controller Board with the EVAL-CN0271A-SDPZ Evaluation Board.
The circuit from the EVAL-CN0271-SDPZ board is a complete thermocouple signal conditioning circuit with cold junction compensation followed by a 16-bit sigma-delta (Σ-Δ) analog-to-digital converter (ADC). The AD8495 thermocouple amplifier provides a simple, low cost solution for measuring K type thermocouple temperatures, including cold junction compensation. A fixed gain instrumentation amplifier in the AD8495 amplifies the small thermocouple voltage to provide a 5 mV/°C output. The high common-mode rejection of the amplifier blocks commonmode noise that the long thermocouple leads can pick up. For additional protection, the high impedance inputs of the amplifier make it easy to add extra filtering. The AD8476 differential amplifier provides the correct signal levels and common-mode voltage to drive the AD7790 16-bit, Σ-Δ ADC. The circuit provides a compact low cost solution for thermocouple signal conditioning and high resolution analog-to-digital conversion.
The AD7790 is a low power, complete analog front end for low frequency measurement applications. It contains a low noise 16-bit Σ-Δ ADC with one differential input that can be buffered or unbuffered along with a digital PGA, which allows gains of 1, 2, 4, and 8.
The first objective is to ensure that you have all of the items needed and to install the software tools so that you are ready to create and run the evaluation project.
The following table presents a short description the reference design archive contents.
Folder | Description |
---|---|
Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. |
Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. |
Software | Contains the source files of the software project that will be run by the Microblaze processor. |
uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. |
Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.
At this point everything is set up and it is possible to start the evaluation of the ADI hardware through the controls in the uC-Probe application provided in the reference design.
Launch uC-Probe from the Start → All Programs → Micrium → uC-Probe.
Select uC-Probe options.
Set target board communication protocol as RS-232
Setup RS-232 communication setting
The following figure presents the uC-Probe interface that can be used for monitoring and controlling the operation of the EVAL-CN0271A-SDPZ evaluation board.
The communication with the board is activated / deactivated by toggling the ON/OFF switch. If the ON/OFF switch is set to ON and there is no Activity, it means that there is a communication problem with the board. See the Troubleshooting section for indications on how to fix the communication problems.
Data acquired from the AD7790 is plotted in the Graph Window, and the current temperature that is being read is displayed in the Numeric Display located in the bottom left of the graph.
In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: