Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:fpga:xilinx:interposer:ad9116 [20 Feb 2012 09:49] – fixed link Alexandru Tofanresources:fpga:xilinx:interposer:ad9116 [31 Jan 2024 09:53] (current) – Mark as obsolete iulia Moldovan
Line 1: Line 1:
-====== AD971x/AD911x-DPG2 FMC Interposer & Evaluation Board / Xilinx ML-605 Reference Design ======+====== (OBSOLETE) AD971x/AD911x-DPG2 FMC Interposer & Evaluation Board / Xilinx ML-605 Reference Design ====== 
 + 
 +<WRAP round important 65%> 
 +Support for AD971x/AD911x-DPG2 project on this website only for legacy purposes. The support for this project has been discontinued, latest tested files can be found in the Downloads section. 
 +</WRAP>
  
 ===== Supported Devices ===== ===== Supported Devices =====
Line 10: Line 14:
 ===== Evaluation Boards ===== ===== Evaluation Boards =====
  
-  * [[adi>en/digital-to-analog-converters/da-converters/ad9114/products/EVAL-AD9114/eb.html|AD9114-DPG2-EBZ]] +  * [[adi>AD9114-DPG2-EBZ]] 
-  * [[adi>en/digital-to-analog-converters/da-converters/ad9115/products/EVAL-AD9115/eb.html|AD9115-DPG2-EBZ]] +  * [[adi>AD9115-DPG2-EBZ]] 
-  * [[adi>en/digital-to-analog-converters/da-converters/ad9116/products/EVAL-AD9116/eb.html|AD9116-DPG2-EBZ]] +  * [[adi>AD9116-DPG2-EBZ]] 
-  * [[adi>en/digital-to-analog-converters/da-converters/ad9117/products/EVAL-AD9117/eb.html|AD9117-DPG2-EBZ]]+  * [[adi>AD9117-DPG2-EBZ]]
    
 ===== Introduction ===== ===== Introduction =====
Line 21: Line 25:
 The flexible power supply operating range of 1.8 V to 3.3 V and low power dissipation of the AD9114/AD9115/AD9116/AD9117 make them well suited for portable and low power applications. The flexible power supply operating range of 1.8 V to 3.3 V and low power dissipation of the AD9114/AD9115/AD9116/AD9117 make them well suited for portable and low power applications.
  
-**HW Platform(s):** [[http://www.xilinx.com/products/boards-and-kits/EK-V6-ML605-G.htm|Virtex-6 ML605 (Xilinx)]], [[http://www.analog.com/en/digital-to-analog-converters/da-converters/ad9114/products/EVAL-AD9114/eb.html|AD9114 Evaluation Board (ADI)]] / [[http://www.analog.com/en/digital-to-analog-converters/da-converters/ad9115/products/EVAL-AD9115/eb.html|AD9115 Evaluation Board (ADI)]] / [[http://www.analog.com/en/digital-to-analog-converters/da-converters/ad9116/products/EVAL-AD9116/eb.html|AD9116 Evaluation Board (ADI)]] / [[http://www.analog.com/en/digital-to-analog-converters/da-converters/ad9117/products/EVAL-AD9117/eb.html|AD9117 Evaluation Board (ADI)]], [[http://www.analog.com/en/digital-to-analog-converters/da-converters/ad-dac-fmc/products/product.html|DAC FMC Interposer Board (ADI)]] \\+**HW Platform(s):** [[xilinx>products/boards-and-kits/EK-V6-ML605-G.htm|Virtex-6 ML605 (Xilinx)]], [[adi>EVAL-AD9114|AD9114 Evaluation Board (ADI)]] / [[adi>EVAL-AD9115|AD9115 Evaluation Board (ADI)]] / [[adi>EVAL-AD9116|AD9116 Evaluation Board (ADI)]] / [[adi>EVAL-AD9117|AD9117 Evaluation Board (ADI)]], [[adi>ad-dac-fmc|DAC FMC Interposer Board (ADI)]] \\
 **System:** Microblaze, AXI, UART **System:** Microblaze, AXI, UART
  
Line 47: Line 51:
 ==== Running Demo (SDK) Program ==== ==== Running Demo (SDK) Program ====
  
-<note tip>If you are not familiar with ML605 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/boards/ml605/reference_designs.htm]] for details. +<WRAP tip>If you are not familiar with ML605 and/or Xilix tools, please visit\\ [[xilinx>products/boards/ml605/reference_designs.htm]] for details. 
-</note>+</WRAP>
  
 Extract the project from the archive file (AD911x.zip) to the location you desire.  Extract the project from the archive file (AD911x.zip) to the location you desire. 
Line 133: Line 137:
   - **Section 13** User must press the button in order for the AD9512 related modifications to take place   - **Section 13** User must press the button in order for the AD9512 related modifications to take place
  
-<note important>+<WRAP important>
   * If you drag a slider and it doesn't change the value in the numeric indicator next to it, please press Stop and then Play again. At the bottom of the screen, the bytes/sec should be increasing with 200 per second. If they increase only with 50 per second, please press Stop and Play again.   * If you drag a slider and it doesn't change the value in the numeric indicator next to it, please press Stop and then Play again. At the bottom of the screen, the bytes/sec should be increasing with 200 per second. If they increase only with 50 per second, please press Stop and Play again.
   * If you receive (Pc Port Open) at the bottom of the screen, please press Stop, close your COM port, reprogram the FPGA, launch the software and try again.   * If you receive (Pc Port Open) at the bottom of the screen, please press Stop, close your COM port, reprogram the FPGA, launch the software and try again.
   * In **Section 10** please select DIVSEL so that (DCLKIO / 2^n) is between 0.5 MHz and 4 MHz for optimal Calibration results   * In **Section 10** please select DIVSEL so that (DCLKIO / 2^n) is between 0.5 MHz and 4 MHz for optimal Calibration results
-</note>+</WRAP>
  
 ===== Downloads ===== ===== Downloads =====
-{{:resources:fpga:xilinx:pmod:ad9116.zip|Reference design source code}}+ 
 +<WRAP round download 80%> 
 +{{:resources:fpga:xilinx:interposer:ad9116.zip|Reference design source code}} 
 +</WRAP> 
 + 
 +===== Support ===== 
 + 
 +==== HDL / Hardware Questions ==== 
 + 
 +For questions regarding the AD9116 chip, or the AD911x eval board, please ask them in the [[ez>community/data_converters/high-speed_dacs|High Speed DAC]] sub-community. 
 + 
 +==== No-OS Questions ==== 
 +For questions regarding the no-OS drivers for any of the components on the AD-FMCOMMS2-EBZ please use the [[ez>community/linux-device-drivers/microcontroller-no-os-drivers|Microcontroller and No-OS Driver]] sub-community. 
resources/fpga/xilinx/interposer/ad9116.1329727756.txt.gz · Last modified: 20 Feb 2012 09:49 by Alexandru Tofan