Condition-based monitoring (CbM) enables early detection and diagnosis of machine and system abnormalities. Identifying and isolating these issues creates opportunities for optimizing replacement part inventories, scheduling downtime for planned maintenance, and making run-time process adjustments that can extend the life of equipment.
The EVAL-CN0579-ARDZ is a 4-channel, high resolution, wide bandwidth, high dynamic range, IEPE-compatible interface data acquisition (DAQ) system that interfaces with IC piezoelectric (ICP®)/IEPE sensors. While most solutions that interface with piezoelectric sensors in the market are AC-coupled and lack DC and subhertz measurement capabilities, this solution is DC-coupled. By looking at the complete data set from an IEPE vibration sensor in the frequency domain (DC to 50 kHz), the type and source of a machine fault can be better predicted using the position, amplitude, and number of harmonics found in the fast Fourier transform (FFT) spectrum.
The main input on the EVAL-CN0579-ARDZ are right-angle SMA connectors on the primary side of the board, as such it is highly recommended to connect the sensor using an SMA cable. If this is not possible, due to the type of sensor or otherwise, use the headers to connect the board with other standard wires.
LED | Location | Function |
---|---|---|
PWR LEDs (DS1 to DS2) | bottom-left corner | indicates board power |
FAULT LEDs (DS3 to DS6) | near each SMA connector | indicates the status of switch's fault flag |
SHUTDOWN LED (DS7) | left side of U19 | indicates status of shutdown logic/buffer, FDA, SW disable |
The EVAL-CN0579-ARDZ includes solder jumpers (P17 to P20) to control current source. The jumpers connect the current source to the circuit and may be removed for testing without a current source.
All connector pinouts for the EVAL-CN0579-ARDZ are described in the table below.
Connector | Pin No. | Pin Name | CN0579 Pin Function |
---|---|---|---|
Arduino DIO 1 (P12) | 1 | SCL | SCL |
2 | SDA | SDA | |
3 | AREF | NC (Not connected) | |
4 | GND | GND | |
5 | 13 / SCLK | SCLK | |
6 | 12 / MISO | MISO | |
7 | 11 / PWM / MOSI | MOSI | |
8 | 10 / PWM / CS | CS_ADC | |
9 | 9 / PWM | DRDY_N | |
10 | 8 | DCLK | |
Arduino DIO 0 (P14) | 1 | 7 | DOUT0 |
2 | 6 / PWM | DOUT1 | |
3 | 5 / PWM | DOUT2 | |
4 | 4 | DOUT3 | |
5 | 3 / PWM | SHUTDOWN_N | |
6 | 2 | RESET_N | |
7 | TX | NC | |
8 | RX | NC | |
Arduino Analog (P13) | 1 | AIN0 | NC |
2 | AIN1 | NC | |
3 | AIN2 | NC | |
4 | AIN3 | NC | |
5 | AIN4 | NC | |
6 | AIN5 | NC | |
Arduino Power (P11) | 1 | NC | NC |
2 | IOREF | IOREF | |
3 | RESET | NC | |
4 | 3.3 V | 3V3 | |
5 | 5V | 5V | |
6 | GND | GND | |
7 | GND | GND | |
8 | Vin | NC |
To achieve reasonable noise measurements, the piezo vibration sensor must be stabilized using either an active shaker table, which cancels environmental vibrations; or anchored to a massive object, which makes sensor still. For noise measurements done on EVAL-CN0579-ARDZ, the piezo vibration sensor was anchored to a massive object, where it is also connected directly to the input of the signal chain.
The board also has many test points, most of which are labeled and are fairly self-explanatory. The table below describes some of the most significant test points and their connections.
Test Point | Description |
---|---|
26V8 | Connects to the 26.8 V rail before it's reduced to 26 V. |
26V0 | Connects to the 26 V rail. |
5V5 | Connects to the 5.5 V rail before it's reduced to 5 V. |
5V0 | Connects to the 5 V rail. |
TP1 | Connects to the voltage reference of the DAC for IEPE sensor. |
TP6 / TP11 / TP16 / TP21 | Connects to signal chain after passing through the fault protection switch |
TP7 / TP12 / TP17 / TP22 | Connects to VOCM. |
TP8 / TP13 / TP18 / TP23 | Connects to signal chain that is level shifted. |
TP9 / TP14 / TP19 / TP24 | Connects to FDA_OUT_N0 of the ADC driver. |
TP10 / TP15 / TP20 / TP25 | Connects to FDA_OUT_P0 of the ADC driver. |
TP27 / TP29 / TP31 / TP33 | Connects to output from the bias voltage correction. |
TP34 | Connects to ADC reference buffer. |
TP35 | Connects to differential conversion reference buffer output / VOCM. |
TP36 | Connects to 32.768 MEGHz clock output. |
TP37 | Connects to VCM of ADC. |
The following is the list of items needed in order to replicate this demo.
To prepare the SD card for the DE10-Nano board:
The following is the list of items needed in order to replicate this demo.
To prepare the SD card for the DE10-Nano board:
The EVAL-CN0579-ARDZ is supported by the Libiio library. This library is cross-platform (Windows, Linux, Mac) with language bindings for C, C#, Python, MATLAB, and others. Two easy examples that can be used with the EVAL-CN0579-ARDZ are:
To be able to connect your device, the software must be able to create a context. The context creation in the software depends on the backend used to connect to the device, as well as the platform where the EVAL-CN0579-ARDZ is attached. The platforms currently supported for the EVAL-CN0579-ARDZ are Cora Z7 and DE10-Nano using the ADI Kuiper Linux. The user needs to supply a URI, which will be used in the context creation. The Libiio is a library for interfacing with IIO devices.
Install the Libiio package on your machine.
The iio_info command is a part of the libIIO package that reports all IIO attributes.
Upon installation, simply enter the command on the terminal command line to access it.
Open SSH Terminal Software (PuTTY, TeraTerm, or similar). The user should now start the PuTTY application and enter certain values in the configuration window. In the terminal, run:
analog@analog:~$ iio_info -u ip:<ip_address>
iio_info -s
Prompting this on the command terminal in your Windows PC will give you the IP address to access the EVAL-CN0579-ARDZ.
ssh analog@<ip_address>
analog@analog:~$ iio_info -u ip:<ip_address>
There are different commands that can be used to manage the device being used. The iio_attr command reads and writes IIO attributes.
analog@analog:~$ iio_attr [OPTION]...
Example:
analog@analog:~$ iio_attr -a -C
Make sure to download/update to the latest version of IIO Oscilloscope.
https://github.com/analogdevicesinc/iio-oscilloscope/releases
PyADI-IIO is a Python abstraction module for ADI hardware with IIO drivers to make them easier to use. This module provides device-specific APIs built on top of the current libIIO Python bindings. These interfaces try to match the driver naming as much as possible without the need to understand the complexities of libIIO and IIO.
After installing and configuring PYADI-IIO on your machine, you are now ready to run Python script examples. In our case, run the cn0579_example.py.
.../pyadi-iio/examples $ python3 cn0579_example.py
The expected output should look like this:
Without input signal:
With input from ADALM2000 (1 Vp-p, 1 kHz) on Channel 0:
GitHub link for the Python sample script: CN0579 Python Example
EVAL-CN0579-ARDZ Design & Integration Files
Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. Register to receive all these great benefits and more!
End of Document