This is an old revision of the document!
This document describes the No-OS software used to control the AD4003 part and includes an example of how to initialize a AD4003 part.
The AD4003/AD4007/AD4011/AD4020 are low noise, low power, high speed, 18-bit, precision successive approximation register (SAR) analog-to-digital converters (ADCs). The AD4003, AD4007, and AD4011 offer 2 MSPS, 1 MSPS, and 500 kSPS throughputs, respectively. They incorporate ease of use features that reduce signal chain power consumption, reduce signal chain complexity, and enable higher channel density. The high-Z mode, coupled with a long acquisition phase, eliminates the need for a dedicated high power, high speed ADC driver, thus broadening the range of low power precision amplifiers that can drive these ADCs directly while still achieving optimum performance. The input span compression feature enables the ADC driver amplifier and the ADC to operate off common supply rails without the need for a negative supply while preserving the full ADC code range. The low serial peripheral interface (SPI) clock rate requirement reduces the digital input/output power consumption, broadens processor options, and simplifies the task of sending data across digital isolation.
The ADAQ4003 is an 18-bit precision data acquisition sub-system SiP design on a laminate that includes the AD4003 ADC with a fully differential driver the ADA4945, a reference buffer (the ADA4807), a precision resistor iPassive network on a separate die along with discrete capacitors and resistors. The device solves many design challenges for a wide range of applications similar to AD400x, yet it still provides the flexibility. It offers over 75% area savings compared to discrete design (i.e. Increased channel density and reduced signal chain BOM) and reduces TTM.
In the ADI Reference Designs HDL User Guide can be found an in-depth presentation and instructions about the HDL design in general.
The reference design uses the standard SPI Engine Framework with an integrated pulse generator, which will provide the required conversion rate for the ADC.
In order to build the HDL design the user has to go through the following steps:
The reference design uses an integrated pulse generator to synchronise the capture events during continuous conversion. The required sampling rate can be set in system_bd.tcl file to the required values:
1) Reference clock frequency for SPI interface clock
set spi_clk_ref_frequency 100
2) Device resolution
set adc_resolution 20
3) The targeted sampling rate:
set adc_sampling_rate 1800000
In order to perform the software setup the user has to go through the following steps:
The driver has two modes of operation:
In single conversion mode a single sample is read from the ADC, while in offload mode a buffer is loaded with a user specified number.
To switch between these two modes this define must be modified:
#define SPI_ENGINE_OFFLOAD_EXAMPLE 1
Function | Description |
---|---|
int32_t ad400x_init(struct ad400x_dev **device, struct ad400x_init_param init_param) | Initialize the device. |
int32_t ad400x_remove(struct ad400x_dev *dev) | Free the resources allocated by ad400x_init(). |
int32_t ad400x_spi_reg_read(struct ad400x_dev *dev, uint8_t *reg_data) | Read register. |
int32_t ad400x_spi_reg_write(struct ad400x_dev *dev, uint8_t reg_data) | Write register. |
int32_t ad400x_spi_single_conversion(struct ad400x_dev *dev, uint32_t *adc_data) | Read a single sample. |
enum ad400x_supported_dev_ids{ ID_AD4003, ID_AD4007, ID_AD4011, ID_AD4020, }; struct ad400x_dev { /* SPI */ spi_desc *spi_desc; /* Device Settings */ enum ad400x_supported_dev_ids dev_id; }; struct ad400x_init_param { /* SPI */ spi_init_param spi_init; /* Device Settings */ enum ad400x_supported_dev_ids dev_id; uint8_t num_bits; bool turbo_mode; bool high_z_mode; bool span_compression; bool en_status_bits; }; |
HW Platform(s):