Development kits
Supported image sensors & cameras
Cables
GMSL Deserializer Evaluation Kit
AD-GMSLCAMRPI-ADP# Adapter
Once Linux boots you'll see on the HDMI monitor the Linux desktop and on the top left corner a shortcut to the script named video_cfg.sh. Double clicking on the icon will start the media-ctl configuration script. The script is running in background without any pop ups.
After the script was executed once, one should double click on Qt V4L2 test Utility icon to start the video capture application. A window like bellow should open. First the user must select video0 device by clicking the open icon.
A new instance of Qt V4L2 test Utility should be started and selected video1 this time. After this step the play button should be pressed on both Qt V4L2 test Utility instances. Video should be visible on the 2 windows.
OpenGL rendering is recommended to be disabled by accessing Qt V4L2 test Utility capture menu. Capture will start only if both Qt V4L2 test Utility instances are on play state. This is a current HDL limitation.
The GMSL Linux kernel drivers, the complete Linux distributions for the supported processing platforms, and software user guides can be found on the Analog Devices GMSL github repository.
The project and the project's overview can be found at the following links: project's link overview's link.