No renderer 'pdf' found for mode 'pdf'
EVALUATING THE AD9114/AD9115/AD9116/AD9117 AND THE AD9714/AD9715/AD9716/AD9717 DIGITAL-TO-ANALOG CONVERTERS
Preface
Typical Setup
Figure 1. EVAL-AD911x / EVAL-AD971x Evaluation Setup
Tip: Click on any picture in this guide to open an enlarged version.
Helpful Files:
UG-073 for DPG2/DPG3 users and for reference on evaluation board jumper selection
-
-
-
-
-
-
-
Software Needed:
Known Issue: ACE may fail to detect HS-DAC boards, details
here.
Hardware Needed:
-
-
12Vdc 1A Wall Wart for SDP-H1
AD-DAC-FMC-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board
PC with ACE and DPG Lite Software Applications
High-Frequency Continuous Wave Generator
Signal/Spectrum Analyzer
(2)
USB A to
USB Mini Cables
(2) SMA Cables
Quick Start Guide
-
Connect SDP-H1 to PC via
USB and to a 12Vdc 1A power supply.
Set clock input to 125MHz and 3dBm.
Press SW1 Button to reset the AD9114/AD9115/AD9116/AD9117/AD9714/AD9715/AD9716/AD9717.
Open ACE. The board will be automatically recognized by the software. Otherwise, install the plugin for Board.AD911x or Board.AD971x in ACE Plugin Manager Available packages.
Start DPG Lite or DPG Downloader. At the SDP-H1 part of the software, the device part number and clock frequency should be displayed.
In ACE, apply the values in the Initial Configuration wizard as shown in Figure 2.
Figure 2. ACE Initial Configuration Wizard for EVAL-AD9717
In DPG Lite or DPG Downloader, from the Add Generator Waveforms pulldown menu select Single Tone and apply the settings as shown in Figure 3. Set the desired frequency to 15
MHz. Set DAC resolution to the DAC’s number of bits (14 for AD9717/9117, 12 for AD9716/9116, and so on). Check the Unsigned Data box.
Figure 3. DPG Lite session for EVAL-AD9717
Select the tone from the Data Vector pulldown menu.
Press the download arrow and then the play button. The spectrum similar to Figure 4 should appear in the signal/spectrum analyzer.
Figure 4. EVAL-AD9717 FFT for Fdac=125MHz, Fout=15MHz
Troubleshooting
This section lists items to check and practices to use when debugging any unexpected performance of a board. It also provides information on how to check for proper operation when using the modulator in the signal chain.
If unexpected results occur
Reset the part (SW1) and rerun the
SPI software.
Sync/reset the clock (SW2) when using the clock chip.
Check the voltage at TP30 (COREVDD), which should be 1.75
V.
Check the voltage at TP3 (VREF), which should be 1.0
V.
Probe S11 (DATACLK) to be sure that the DAC is properly receiving data and that a clock signal is present. This signal can also be probed at R64 near the part on-board (should be unsoldered from initial setup instructions).
When using the modulator, check to make sure the common-mode voltage is 0.5
V at the input of the modulator by probing at R24 or R61 for the I or Q channels, respectively.
If the common-mode voltage is not as expected, unplug the board and check the resistances at R13, R14, R52, and R53 for the correct values of the particular board. If a proper reading is not present, unsolder J13, J14, J19, and J23, which removes the resistors from the parallel connection with 1 kΩ/100 Ω at the input of the modulator to measure the individual resistances of those components. Check if the resistance values are still incorrect and if so, change out for the appropriate values listed above. If not, try resoldering the jumpers and test again to make sure there was not a problem with the previous connection.