This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:ad8232-evaluation-guide [29 Jan 2014 22:24] – Updated to latest board revision 035378a RevA Gustavo Castro | resources:eval:ad8232-evaluation-guide [08 Sep 2014 15:58] (current) – Eliminated contents that are already under UG-514 Gustavo Castro | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== AD8232 EVALUATION BOARD DOCUMENTATION ===== | ====== AD8232 EVALUATION BOARD DOCUMENTATION ===== | ||
- | <WRAP tip>This page contains the documentation | + | <WRAP tip>The user guide (UG-514) |
- | http://wiki.analog.com/ | + | http://www.analog.com/ |
- | </ | + | or by following this link: |
- | + | ||
- | + | ||
- | ===== FEATURES ===== | + | |
- | * **Ready to use Heart Rate Monitor (HRM) Front end** | + | |
- | * **Operates in 2 or 3 electrode configurations** | + | |
- | * **Directly interface to data acquisition and ADCs** | + | |
- | * **Easy feature selection with switches** | + | |
- | * **Allows various circuit configurations** | + | |
- | + | ||
- | + | ||
- | {{: | + | |
- | //Figure 1. AD8232-EVALZ Evaluation Board (08-035378 REV A)// | + | |
- | ===== GENERAL DESCRIPTION ===== | + | |
- | The AD8232-EVALZ contains an AD8232 Heart Rate Monitor Front End conveniently mounted with the necessary components for initial evaluation in fitness applications. Inputs, outputs, supplies and leads-off detection terminals have been routed to test pins to simplify connectivity. Switches and jumpers are available for setting the input bias voltage, shutdown (SDN), fast-restore (FR), and AC/DC leads-off detection mode | + | |
- | + | ||
- | ===== QUICK START ===== | + | |
- | The board ships with a default configuration for three-electrode systems connected to the hands. For this operation, verify that the switches and jumpers are set to the default values shown in Table 1. For two-electrode configurations, | + | |
- | + | ||
- | + | ||
- | **TABLE 1. Quick Start Switch Settings** | + | |
- | + | ||
- | ^SETTING | + | |
- | |Fast Restore Enabled | + | |
- | |DC Leads Off Detection|S2 | + | |
- | |Operation Enabled | + | |
- | |Input bias set by RLD and +Vs|INPUT BIAS SEL|P3 | | + | |
- | + | ||
- | + | ||
- | - Connect the power supply common to the GND terminal on the board. Connect a +3.3V supply voltage between at the +3.3V terminal. | + | |
- | - Connect the terminals LA and RA to the signal source. | + | |
- | - The right-leg drive is available via the RL terminal. Connect this terminal to the source reference. | + | |
- | - The output signal is available on the OUT terminal and it may be connected to a properly isolated system. | + | |
- | + | ||
- | <WRAP important> | + | |
- | + | ||
- | ===== DEFAULT CIRCUIT CONFIGURATION ===== | + | |
- | + | ||
- | A simplified schematic is shown in Figure 2. The full schematic can be found at the end of this document \\ \\ | + | |
- | {{: | + | |
- | //Figure 2. AD8232-CHARZ Board Simplified Schematic (Refer to Figure 12 for complete version)// | + | |
- | + | ||
- | The evaluation board ships with a default configuration for applications that involve three-electrodes connected at the hands. The terminals LA (left arm), RA (right arm), and RL (right leg) serve as the signal inputs and right-leg drive electrode connections respectively. | + | |
- | + | ||
- | ==== Signal Path: Inamp and Filters ==== | + | |
- | The instrumentation amplifier has a fixed gain of 100 and the op-amp is set for a gain of 11. The overall gain is 1100V/V, which limits the maximum differential input signal to about 2.7mVp-p. Exceeding this amplitude will not damage the AD8232, but the signal at the output will appear distorted. Due to the filter’s high-Q, there is additional peaking that sets the maximum observed gain above 1100V/V around 15Hz. The total gain may be changed by adjusting the resistors R16 and R17, but this will have a direct impact on the Q of the low-pass filter. Note that the instrumentation amplifier has a fixed gain of 100.\\ \\ | + | |
- | The entire signal chain operates from a single-supply voltage. For this purpose, the reference buffer is set to a ratiometric level at mid-supply using two 10MΩ resistors (R14 and R15). The integrated reference buffer output provides a mid-supply dc level for the system. The signal at the output will ride on top of this mid-supply level. This voltage is available at the REFOUT pin (TP19) to serve as reference level for subsequent signal-acquisition stages.\\ \\ | + | |
- | The circuit implements a two-pole high pass filter for eliminating motion artifacts and the electrode half-cell potential. Additionally, | + | |
- | A complete version of the schematic and a section summarizing the explanation of the components can be found at the bottom of this page.\\ | + | |
- | \\ | + | |
- | + | ||
- | + | ||
- | ==== Right-Leg Drive Amplifier ==== | + | |
- | + | ||
- | The integrated right-leg drive (RLD) amplifier senses the common mode voltage present at the signal inputs and can drive an opposing signal into the patient. This driven electrode functionality maintains the voltage between the patient and the AD8232 constant, greatly improving the common mode rejection ratio.\\ | + | |
- | \\ | + | |
- | The board configures the RLD amplifier as an integrator, formed by an internal 150kΩ resistor and an external capacitor of 1nF (C6). This results in a loop gain of about 20 at line frequencies, | + | |
- | \\ | + | |
- | In two-lead configurations, | + | |
- | \\ | + | |
- | ===== FILTER CONFIGURATION===== | + | |
- | + | ||
- | The resistor and capacitor values for the filters were selected to provide effective noise rejection in applications that involve pulse detection while the subject is in motion. The filter parameters can be adjusted to fit other applications.\\ | + | |
- | \\ | + | |
- | ==== High-Pass Filters ==== | + | |
- | + | ||
- | The instrumentation amplifier in the AD8232 applies gain and high pass filtering simultaneously. | + | |
- | \\ | + | |
- | f< | + | |
- | \\ | + | |
- | | + | |
- | \\ | + | |
- | {{: | + | |
- | //Figure 3. Frequency response In-Amp filter (dc blocking feature)// | + | |
- | \\ | + | |
- | \\ | + | |
- | An ac-coupling network (C4 and R9) at the output of the instrumentation amplifier introduces a second pole. The cutoff frequency is that of a regular passive first-order high-pass filter\\ | + | |
- | \\ | + | |
- | f< | + | |
- | \\ | + | |
- | This results in a 7Hz cutoff frequency for 0.22μF and 100kΩ. Both high-pass filters together yield a total roll-off of 40dB per decade. Be aware that setting the same pole location for both high-pass filters will result in 6dB attenuation at the corner frequency. In addition, because the output of this filter is unbuffered, the instrumentation amplifier exhibits higher output impedance at the input of the subsequent low pass filter. | + | |
- | \\ | + | |
- | ==== Low-Pass Filter ==== | + | |
- | The internal uncommitted op amp is used to build a two-pole low pass filter with gain, using a Sallen-Key configuration. The following design equations set the low-pass cut-off frequency, gain and Q.\\ | + | |
- | \\ | + | |
- | f< | + | |
- | \\ | + | |
- | Gain = 1 + R16/R17\\ | + | |
- | \\ | + | |
- | Q = √{ (R10 C8 R13 C9) / [R10 C9 + R13 C9 + R13 C8 (1 - Gain) ] }\\ | + | |
- | \\ | + | |
- | Notice that changing the gain or the cutoff frequency will have an effect on Q and vice versa. | + | |
- | \\ | + | |
- | The evaluation board components place the cutoff frequency for the low-pass filter at approximately 25Hz and the gain to 11. Keep the sum of R16 and R17 above 50kΩ to save power and to avoid excessive loading of the output.\\ | + | |
- | \\ | + | |
- | Figure 4 shows the transfer function of the signal from the differential input of the instrumentation amplifier to VOUT with the default filter configuration.\\ | + | |
- | \\ | + | |
- | {{: | + | |
- | //Figure 4. Gain vs. Frequency// | + | |
- | \\ | + | |
- | \\ | + | |
- | ==== Additional Low-Pass Filters ==== | + | |
- | The components R18, C14, R19 and C15 offer additional filtering options. The terminal labeled OUTF is located after the first filter (R18 and C14). The terminal OUTFF is located after both filters. | + | |
- | ===== LEADS-OFF DETECTION ===== | + | |
- | The AD8232 includes leads off detection features. It provides modes optimized for either two or three-electrode configurations. | + | |
- | ==== DC Leads-Off Detection ==== | + | |
- | To use this mode, the position of the switch S2 must be the same as the “DC” label on the board. | + | |
- | \\ | + | |
- | In DC leads-off mode, the AD8232 checks each input individually, | + | |
- | + | ||
- | ==== AC Leads-Off Detection ==== | + | |
- | To use this mode, the position of the switch S2 must be the same as the “AC” label of the board. To maintain the inputs inside the common-mode range of the amplifier, the bias level for the inputs may be set to REFOUT or RLD by placing the jumper on P2 or P4 respectively.\\ | + | |
- | \\ | + | |
- | This mode is useful when using only two electrodes (no separate driven electrode). The AD8232 detects when an electrode is disconnected by sourcing a small 100 kHz current into the electrodes. | + | |
- | + | ||
- | ===== FAST RESTORE ===== | + | |
- | The fast restore function (FR) reduces the duration of otherwise long settling tails of the high-pass filters. After an abrupt change that rails the amplifier (such as a leads-off condition), the AD8232 automatically adjusts to a higher filter cutoff frequency. This functionality allows the AD8232 to recover quickly, and therefore take valid measurements soon after reconnecting the electrodes to the subject. To enable this function, set the switch S1 to the position labeled FR_EN.\\ | + | |
- | \\ | + | |
- | ===== BOARD SETTINGS FOR TWO ELECTRODE CONFIGURATION ===== | + | |
- | The AD8232-EVALZ can be configured to suit two-electrode applications, | + | |
- | \\ | + | |
- | + | ||
- | TABLE 2. Two-electrode configuration | + | |
- | + | ||
- | ^SETTING^LABEL | + | |
- | |AC Leads-off detection|S2 | + | |
- | |Input bias set by RLD|INPUT BIAS SEL|P4 | | + | |
- | + | ||
- | Alternatively, | + | |
- | + | ||
- | Keep in mind that the gain and filtering may need to be adjusted depending on the location of the electrodes. Note that narrow bandwidths offer the highest rejection to motion artifacts and other external interferences, | + | |
- | \\ | + | |
- | ===== LAYOUT DIAGRAMS ===== | + | |
- | The AD8232-EVALZ is a two-layer board with components mounted on the primary side only. Rubber feet are available on the secondary side for mechanical stability. The layout diagrams are provided as a visual aid and reference design. The PCB has been designed following standard practices to ensure signal integrity and reduce manufacturing costs.\\ | + | |
- | \\ | + | |
- | {{: | + | |
- | //Figure 5. Top Assembly// | + | |
- | \\ | + | |
- | {{: | + | |
- | //Figure 6. Primary side// | + | |
- | \\ | + | |
- | {{: | + | |
- | //Figure 7. Secondary side// | + | |
- | \\ | + | |
- | ===== EVALUATION BOARD COMPONENT EXPLANATION ===== | + | |
- | + | ||
- | <WRAP tip>The board should be thoroughly cleaned after any rework. Leaving contaminants such as residual flux from the soldering will have a negative impact on the input impedance and operation of the board.</ | + | |
- | + | ||
- | **Input Bias Selection: P1, P2, P3, P4, | + | |
- | R1, R2**\\ \\ | + | |
- | In three-electrode configurations, | + | |
- | \\ | + | |
- | Two-electrode configuration: | + | |
- | P4: Connects pull up resistors to the RLD (right-leg drive) amplifier output. This is the recommended configuration for two electrode configurations.\\ | + | |
- | P2: Connects pull up resistors to REFOUT, which is typically at mid-supply.\\ | + | |
- | \\ | + | |
- | Three-electrode configuration: | + | |
- | P3: Connects pull up resistors to +VS. This is the standard configuration for three-electrode configurations. \\ | + | |
- | P1: This jumper position allows connecting the pull-up resistors to a voltage provided by the user. This is useful in systems that expect high power-line noise (50Hz or 60Hz). A higher voltage than the supply, such as 5V, can help in maintaining the inputs within the common-mode range of the amplifier. Apply this voltage between TP4 and ground.\\ | + | |
- | \\ | + | |
- | **In-Amp High Pass Filter: C7, R11**\\ \\ | + | |
- | The cutoff frequency is set to 7.2Hz. Refer to the High-Pass Filters section for more information\\ | + | |
- | \\ | + | |
- | **AC-Coupling: | + | |
- | The cutoff frequency of this high-pass filter is set to 7.2Hz. Because this is a DC-blocking circuit, connecting R11 to the REFOUT voltage is necessary to allow negative signal swings. Refer to the High-Pass Filters section for more information\\ | + | |
- | \\ | + | |
- | **Low Pass Filter (Sallen-Key): | + | |
- | This circuit provides two functions: a dual pole low pass filter and gain. On the evaluation board, the cutoff of this filter is set at 25 Hz, and the gain to 11. This brings the total gain of the AD8232 to 11×100 = 1100. Refer to the Low-Pass Filter section for more information\\ | + | |
- | \\ | + | |
- | **Additional low pass filters: R18, R19, R20, C14, C15, C16**\\ \\ | + | |
- | Not populated. These provide pads for the user to add additional filtering on the output and the reference voltage. Refer to the Additional Low-Pass Filters section for more information\\ | + | |
- | \\ | + | |
- | **Mid-supply level: R14, R15, C11**\\ \\ | + | |
- | R14 and R15 form a supply-ratiometric reference voltage for the system. The AD8232 buffers this voltage and makes it available at the REFOUT terminal. Select high resistor values for R14 and R15 to reduce power consumption. The evaluation board uses 10MΩ for both. C11 is required for filtering and stability. Power line noise may be considerably worse without C11. Due to large resistor and capacitor values used on the evaluation board, the time constant for this voltage is 5 seconds and will take about half a minute to observe a stable voltage at the output of REFOUT after power up. Shutting down the part through S3 will not discharge C11 and there will be no settling time related to this voltage.\\ | + | |
- | \\ | + | |
- | + | ||
- | **Right leg drive: C6, R5, R7**\\ \\ | + | |
- | C6 is 1nF, which together with an internal 150kΩ resistor, results in a loop gain of 20 around the typical line frequencies and a crossover frequency of 1kHz. The value of R5 is set to 499kΩ to avoid stability problems. For more information, | + | |
- | + | ||
- | R7 is not populated. It can be used to limit the loop gain at low frequencies and to shift the amplifier’s dominant pole. | + | |
- | \\ | + | |
- | \\ | + | |
- | **Optional RFI Filter: R3, R4, C1,C2, C3**\\ \\ | + | |
- | Pads are provided for capacitors to implement additional RFI filtering. C2 and C3 should be the same value and well matched. C1 should be a larger value than C2 and C3. This minimizes degradation of CMRR at higher frequencies due to tolerance mismatch of C2 and C3.\\ | + | |
- | \\ | + | |
- | If C2 = C3 = C and R3 = R4 = R then\\ | + | |
- | Common mode signal cutoff frequency: 1/ (2πRC)\\ | + | |
- | Differential signal cutoff frequency: 1/ | + | |
- | \\ | + | |
- | A lower common mode signal cutoff frequency will improve RFI rejection, but may increase the risk of instability with a right leg drive feedback loop.\\ | + | |
- | \\ | + | |
- | The board should be thoroughly cleaned after any rework. Leaving contaminants such as residual flux from the soldering will have a negative impact on the input impedance and operation of the board.\\ | + | |
- | \\ | + | |
- | \\ | + | |
- | ===== EVALUATION BOARD SCHEMATIC ===== | + | |
- | CLICK ON THE PICTURE TO SEE A LARGER VERSION | + | |
- | {{: | + | |
+ | http:// | ||
+ | To access the documentation for revision **A03321A**, | ||
+ | http:// | ||
+ | </ | ||