Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
university:tools:uartjtag [07 Oct 2022 07:10] Joyce Velascouniversity:tools:uartjtag [14 Mar 2023 06:32] (current) – updated the design files download link Joyce Velasco
Line 10: Line 10:
 Analog Devices provides a small adapter board [[adi>ADALM-UARTJTAG]] to be used for JTAG and UART, in order to make that easier for programming and debugging. You are encouraged to use this on your designs for the same reason we do - the standard JTAG connector is huge, and there are times where good old fashion console UART is valuable for doing debug. The 1.8V supply on the connector above is the I/O voltage, and can be used anywhere between 1.8V and 3.3V. Analog Devices provides a small adapter board [[adi>ADALM-UARTJTAG]] to be used for JTAG and UART, in order to make that easier for programming and debugging. You are encouraged to use this on your designs for the same reason we do - the standard JTAG connector is huge, and there are times where good old fashion console UART is valuable for doing debug. The 1.8V supply on the connector above is the I/O voltage, and can be used anywhere between 1.8V and 3.3V.
  
-In the box, you should have received the UARTJTAG board, ribbon cable, jumper, and [[https://www.samtec.com/products/ftsh|Samtec FTSH-105-01-L-D 10]] position dual row 0.05" through hole pin connector.+In the box, you should have received the UARTJTAG board, ribbon cable, and jumper.
  
 {{ :university:tools:jtaguart:adalm-uartjtag.png?400 |}} {{ :university:tools:jtaguart:adalm-uartjtag.png?400 |}}
Line 32: Line 32:
 ===== Schematic, PCB Layout, Bill of Materials ===== ===== Schematic, PCB Layout, Bill of Materials =====
 <WRAP round download 80%> <WRAP round download 80%>
-  * {{:university:tools:jtaguart:adalm-jtaguart.pdf|Rev A Schematics}} +[[adi>media/en/evaluation-documentation/evaluation-design-files/adalm-uartjtag-designsupport.zip|ADALM-UARTJTAG Design & Integration Files]] 
-  * {{:university:tools:jtaguart:adalm-jtaguart_fab.zip|Rev A Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) +  * Schematic 
-  * {{:university:tools:jtaguart:adalm-jtaguart.xlsx|Rev A Bill of materials}} +  * PCB Layout 
-  * {{:university:tools:jtaguart:adalm-jtaguart_brd.zip|Rev A Allegro Board File}} (This file is [[http://www.7-zip.org/7z.html|compressed]]). Get the [[https://www.cadence.com/en_US/home/tools/pcb-design-and-analysis/allegro-downloads-start.html|Allegro FREE Physical Viewer]] to view. +  * Bill of Materials 
-</WRAP> +  * Allegro Project (get the [[https://www.cadence.com/en_US/home/tools/pcb-design-and-analysis/allegro-downloads-start.html|Allegro FREE Physical Viewer]] to view)
- +
-<WRAP round download 80%> +
-  * {{|Rev B Schematics}} +
-  * {{|Rev B Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) +
-  * {{|Rev B Bill of materials}} +
-  * {{|Rev B Allegro Board File}} (This file is [[http://www.7-zip.org/7z.html|compressed]]). Get the [[https://www.cadence.com/en_US/home/tools/pcb-design-and-analysis/allegro-downloads-start.html|Allegro FREE Physical Viewer]] to view.+
 </WRAP> </WRAP>
  
university/tools/uartjtag.txt · Last modified: 14 Mar 2023 06:32 by Joyce Velasco