Wiki

This version is outdated by a newer approved version.DiffThis version (28 Jan 2021 22:37) was approved by Robin Getz.The Previously approved version (05 Feb 2019 16:09) is available.Diff

This is an old revision of the document!


ADALM-UARTJTAG hardware

Analog Devices provides a small adapter board (ADALM-UARTJTAG) to be used for JTAG and UART, in order to make that easier for programming and debugging. You are encouraged to use this on your designs for the same reason we do - the standard JTAG connector is huge, and there are times where good old fashion console UART is valuable for doing debug. The 1.8V supply on the connector above is the I/O voltage, and can be used anywhere between 1.8V and 3.3V.

In the box, you should have received the UARTJTAG board, ribbon cable, jumper, and Samtec FTSH-105-01-L-D 10 position dual row 0.05“ through hole pin connector.

The PCB includes a jumper, which forces the Zynq to HALT on JTAG. This is great for halting, and not allowing anything to run, but does does pull down a chip select for SPI flash, and will not allow the SPI flash to be found by the on chip bootloader, or by U-Boot. (If you are loading a U-Boot over JTAG).

The pin connector is likely inserted into the ribbon cable:

3  4

but can be removed, and either soldered to the PCB, or left in the ribbon cable, so you don't loose it.

2

If you do want more, they can be obtained from Samtec, Digikey or Arrow.

Downloads

university/tools/uartjtag/hardware.1611869736.txt.gz · Last modified: 28 Jan 2021 22:35 by Robin Getz