Wiki

This version is outdated by a newer approved version.DiffThis version (17 Apr 2019 17:54) was approved by Travis Collins.The Previously approved version (15 Mar 2019 19:05) is available.Diff

This is an old revision of the document!


ADALM-PLUTO for End Users

Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNU Radio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org, etc.) platform over USB. As you can see, we have lots of examples with MATLAB and Simulink, as we find that a very powerful environment, and a path to a releasable radio (you can take your algorithms, and easily embed them into a custom product).

Contents

Make sure all things are in ./users

  1. Intro to the Software. Installing Device Drivers on:
  2. Upgrading the the ADALM-PLUTO Firmware .
  3. Calibrating the ADALM-PLUTO.
  4. Customizing the ADALM-PLUTO.
  5. Once the driver are configured and set up, you can interact with the ADALM-PLUTO Active Learning Module from:
    1. gqrx, an open source software defined radio receiver (SDR) powered by the GNU Radio
    2. SDRangel, an Open Source Qt5 / OpenGL 3.0+ SDR and signal analyzer frontend to various hardware.
    3. SDR#. The PlutoSDR frontend for SDRsharp can be found here: sdrsharp-plutosdr
    4. SoapySDR. The Soapy SDR plugin for PlutoSDR can be found here: SoapyPlutoSDR
university/tools/pluto/users.1555516443.txt.gz · Last modified: 17 Apr 2019 17:54 by Travis Collins