university:tools:pluto:users [10 Apr 2017 18:29]
Robin Getz add a how far/fast section
university:tools:pluto:users [04 Jun 2021 16:54] (current)
Robin Getz add accessories
Line 3: Line 3:
 {{  :​university:​tools:​pluto:​pluto_in_hand.png?​200|}} {{  :​university:​tools:​pluto:​pluto_in_hand.png?​200|}}
  
-Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNU Radio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org,​ etc) platform over USB. As you can see, we have lots of examples with MATLAB and Simulink, as we find that a very powerful environment,​ and a path to a releasable radio (you can take your algorithms, and easily embed them into a custom product).+Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNU Radio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org,​ etc.) platform over USB. As you can see, we have lots of examples with MATLAB and Simulink, as we find that a very powerful environment,​ and a path to a releasable radio (you can take your algorithms, and easily embed them into a custom product).
  
 ===== Contents ===== ===== Contents =====
Line 10: Line 10:
     - [[./​users/​name|What'​s with the name?]] //​PlutoSDR?//​     - [[./​users/​name|What'​s with the name?]] //​PlutoSDR?//​
     - [[./​users/​understanding|Understanding the Internals]]     - [[./​users/​understanding|Understanding the Internals]]
 +    - [[./​users/​temp|How hot?]]
     - [[./​users/​far_fast|How Far, How fast?]]     - [[./​users/​far_fast|How Far, How fast?]]
       - [[./​users/​transmit|RF Output]]       - [[./​users/​transmit|RF Output]]
 +        - [[./​users/​phase_noise|Phase Noise & Accuracy]]
       - [[./​users/​receive|RF Input]]       - [[./​users/​receive|RF Input]]
         - [[./​users/​receiver_sensitivity|Receiver Sensitivity]]         - [[./​users/​receiver_sensitivity|Receiver Sensitivity]]
 +        - [[./​users/​non_quad|Dealing with Non-Quadrature signals]]
     - [[./​users/​antennas|Antennas]]     - [[./​users/​antennas|Antennas]]
   - [[./​users/​quick_start|Quick Start]]   - [[./​users/​quick_start|Quick Start]]
Line 23: Line 26:
   - [[./​users/​calibration|Calibrating]] the ADALM-PLUTO.   - [[./​users/​calibration|Calibrating]] the ADALM-PLUTO.
   - [[./​users/​customizing|Customizing]] the ADALM-PLUTO.   - [[./​users/​customizing|Customizing]] the ADALM-PLUTO.
-    - using more than one the ADALM-PLUTO on the same PC. 
   - Once the driver are configured and set up, you can interact with the [[adi>​ADALM-PLUTO]] Active Learning Module from:   - Once the driver are configured and set up, you can interact with the [[adi>​ADALM-PLUTO]] Active Learning Module from:
-    - Using Pluto with the [[/​resources/​tools-software/​linux-software/​iio_oscilloscope|IIO oscilloscope]] +    - [[/​resources/​tools-software/​linux-software/​iio_oscilloscope|IIO oscilloscope]] 
-      - example 1 +    - [[http://​gqrx.dk/​|gqrx]],​ an open source software defined radio receiver (SDR) powered by the GNU Radio 
-    - Using Pluto with the [[http://​gqrx.dk/​|gqrx]],​ an open source software defined radio receiver (SDR) powered by the GNU Radio and the Qt graphical toolkit+    - [[mw>​hardware-support/​adalm-pluto-radio.html|Official support for MATLAB and Simulink]] ​ 
-    - Using Pluto with [[/​resources/​tools-software/​linux-software/​libiio/​clients/​matlab_simulink|MATLAB]] ​ +    - [[/​resources/​tools-software/​linux-software/​libiio/​clients/​matlab_simulink|MATLAB ​IIO Bindings]] 
-      - example 1 +    - [[/​resources/​tools-software/​linux-software/​gnuradio|GNU Radio]] 
-    - Using Pluto with [[/​resources/​tools-software/​linux-software/​libiio/clients/matlab_simulink|Simulink]] +    - [[https://github.com/​f4exb/​sdrangel|SDRangel]], an Open Source Qt5 / OpenGL 3.0+ SDR and signal analyzer frontend to various hardware. 
-      example 2 +    [[https://​airspy.com/​download/​|SDR#​]]. The PlutoSDR frontend for SDRsharp can be found here: [[https://​github.com/​Manawyrm/​sdrsharp-plutosdr|sdrsharp-plutosdr]] 
-    - Using Pluto with [[/​resources/​tools-software/​linux-software/​gnuradio|GNU Radio]] +    - [[https://​github.com/​pothosware/​SoapySDR|SoapySDR]]. The Soapy SDR plugin for PlutoSDR can be found here: [[https://​github.com/​jocover/​SoapyPlutoSDR|SoapyPlutoSDR]] 
-      example 1+    - [[https://​github.com/​radiosd/​PlutoSdr|Access and control of PlutoSDR hardware using python bindings to libiio]] ​   
 +    - [[:resources/​tools-software/​linux-software/​pyadi-iio|Python Interfaces]] 
 +    [[:​university/​tools/​pluto/​controlling_the_transceiver_and_transferring_data|C Examples]] 
 +  - [[Accessories]] ​
  
  
  
university/tools/pluto/users.1491841741.txt.gz · Last modified: 10 Apr 2017 18:29 by Robin Getz