Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Next revisionBoth sides next revision
university:tools:pluto:users [10 Mar 2017 14:57] – add a page for Antennas Robin Getzuniversity:tools:pluto:users [14 Jan 2021 05:38] – use mw> interwiki links Robin Getz
Line 3: Line 3:
 {{  :university:tools:pluto:pluto_in_hand.png?200|}} {{  :university:tools:pluto:pluto_in_hand.png?200|}}
  
-Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNU Radio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org, etc) platform over USB. As you can see, we have lots of examples with MATLAB and Simulink, as we find that a very powerful environment, and a path to a releasable radio (you can take your algorithms, and easily embed them into a custom product).+Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNU Radio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org, etc.) platform over USB. As you can see, we have lots of examples with MATLAB and Simulink, as we find that a very powerful environment, and a path to a releasable radio (you can take your algorithms, and easily embed them into a custom product).
  
 ===== Contents ===== ===== Contents =====
Line 10: Line 10:
     - [[./users/name|What's with the name?]] //PlutoSDR?//     - [[./users/name|What's with the name?]] //PlutoSDR?//
     - [[./users/understanding|Understanding the Internals]]     - [[./users/understanding|Understanding the Internals]]
-    - [[./users/transmit|RF Output]] +    - [[./users/temp|How hot?]] 
-    - [[./users/receive|RF Input]]+    - [[./users/far_fast|How Far, How fast?]] 
 +      - [[./users/transmit|RF Output]] 
 +        - [[./users/phase_noise|Phase Noise & Accuracy]] 
 +      - [[./users/receive|RF Input]] 
 +        - [[./users/receiver_sensitivity|Receiver Sensitivity]] 
 +        - [[./users/non_quad|Dealing with Non-Quadrature signals]]
     - [[./users/antennas|Antennas]]     - [[./users/antennas|Antennas]]
   - [[./users/quick_start|Quick Start]]   - [[./users/quick_start|Quick Start]]
Line 21: Line 26:
   - [[./users/calibration|Calibrating]] the ADALM-PLUTO.   - [[./users/calibration|Calibrating]] the ADALM-PLUTO.
   - [[./users/customizing|Customizing]] the ADALM-PLUTO.   - [[./users/customizing|Customizing]] the ADALM-PLUTO.
-    - using more than one the ADALM-PLUTO on the same PC. 
   - Once the driver are configured and set up, you can interact with the [[adi>ADALM-PLUTO]] Active Learning Module from:   - Once the driver are configured and set up, you can interact with the [[adi>ADALM-PLUTO]] Active Learning Module from:
-    - Using Pluto with the [[/resources/tools-software/linux-software/iio_oscilloscope|IIO oscilloscope]] +    - [[/resources/tools-software/linux-software/iio_oscilloscope|IIO oscilloscope]] 
-      - example 1 +    - [[http://gqrx.dk/|gqrx]], an open source software defined radio receiver (SDR) powered by the GNU Radio 
-    - Using Pluto with the [[http://gqrx.dk/|gqrx]], an open source software defined radio receiver (SDR) powered by the GNU Radio and the Qt graphical toolkit+    - [[mw>hardware-support/adalm-pluto-radio.html|Official support for MATLAB and Simulink]]  
-    - Using Pluto with [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|MATLAB]]  +    - [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|MATLAB IIO Bindings]] 
-      - example 1 +    - [[/resources/tools-software/linux-software/gnuradio|GNU Radio]] 
-    - Using Pluto with [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|Simulink]] +    - [[https://github.com/f4exb/sdrangel|SDRangel]], an Open Source Qt5 / OpenGL 3.0+ SDR and signal analyzer frontend to various hardware. 
-      example 2 +    [[https://airspy.com/download/|SDR#]]. The PlutoSDR frontend for SDRsharp can be found here: [[https://github.com/Manawyrm/sdrsharp-plutosdr|sdrsharp-plutosdr]] 
-    - Using Pluto with [[/resources/tools-software/linux-software/gnuradio|GNU Radio]] +    - [[https://github.com/pothosware/SoapySDR|SoapySDR]]. The Soapy SDR plugin for PlutoSDR can be found here: [[https://github.com/jocover/SoapyPlutoSDR|SoapyPlutoSDR]] 
-      example 1+    - [[https://github.com/radiosd/PlutoSdr|Access and control of PlutoSDR hardware using python bindings to libiio]]    
 +    - [[:resources/tools-software/linux-software/pyadi-iio|Python Interfaces]] 
 +    [[:university/tools/pluto/controlling_the_transceiver_and_transferring_data|C Examples]]
  
  
  
university/tools/pluto/users.txt · Last modified: 20 Feb 2023 17:37 by Brian OLoughlin