university:tools:pluto:users:receive [15 Jun 2017 00:12]
Robin Getz add graph
university:tools:pluto:users:receive [01 Feb 2021 13:33]
Iulia Moldovan
Line 3: Line 3:
 ===== Receive Architecture ===== ===== Receive Architecture =====
  
-The AD9363 receive chain is based on [[wp>​Direct-conversion_receiver|Direct Conversion]] technique.+The AD9363 receive chain is based on [[wp>​Direct-conversion_receiver|Direct Conversion]] technique. Although this block diagram is for the [[adi>​AD9361]],​ it is also appropriate for the [[adi>​AD9363]] found inside the ADALM-PLUTO. The difference between the two units is the tuning range, a minor missing features (DCXO, external LO are missing and the RF channel bandwidth is reduced).
  
 {{:​resources:​eval:​user-guides:​ad-fmcomms2-ebz:​ad9361.svg?​950x650|}} {{:​resources:​eval:​user-guides:​ad-fmcomms2-ebz:​ad9361.svg?​950x650|}}
Line 21: Line 21:
   * Input fidelity (how accurate is the reception)   * Input fidelity (how accurate is the reception)
  
-For the ADALM-PLUTO, ​the both the receiver sensitivity and input accuracy are both frequency dependent. For plots vs frequency, check out the detailed [[../​devs/​performance|performance section]].+For the ADALM-PLUTO,​ both the receiver sensitivity and input accuracy are frequency dependent. For plots vs frequency, check out the detailed [[../​devs/​performance|performance section]].
  
-This is the output of the [[http://​www.keysight.com/​find/​89600B|Keysight 89600 VSA software]], which is used to measure signal demodulation and complete vector signal analysis. In this case, we generate an LTE 10 (10MHz wide channel), and transmit it out the Tx port of the [[http://​www.keysight.com/​find/E4438C|E4438C ESG Vector Signal Generator]] and capture it on the ADALM-PLUTO'​s Rx port, and the save the data, and load it into the VSA software for analysis. We can measure the RF offset (frequency error = 67Hz), and how accurate the 64-QAM constellation is created (an EVM of -43 dB, or less than 0.6% RMS error) - which is pretty good (better than the AD9363 datasheet).+This is the output of the [[http://​www.keysight.com/​find/​89600B|Keysight 89600 VSA software]], which is used to measure signal demodulation and complete vector signal analysis. In this case, we generate an LTE 10 (10MHz wide channel), and transmit it out the Tx port of the [[https://​www.keysight.com/​en/pd-1000004297%3Aepsg%3Apro/​esg-vector-signal-generator|E4438C ESG Vector Signal Generator]] and capture it on the ADALM-PLUTO'​s Rx port, and then save the data, and load it into the VSA software for analysis. We can measure the RF offset (frequency error = 67Hz), and how accurate the 64-QAM constellation is created (an EVM of -43 dB, or less than 0.6% RMS error) - which is pretty good (better than the AD9363 datasheet).
  
 {{:​university:​tools:​pluto:​users:​rev_b_rx_lte10.png?​800|}} {{:​university:​tools:​pluto:​users:​rev_b_rx_lte10.png?​800|}}
university/tools/pluto/users/receive.txt · Last modified: 01 Feb 2021 13:33 by Iulia Moldovan