Both sides previous revisionPrevious revisionNext revision | Previous revision |
university:tools:pluto:users:antennas [10 Mar 2017 18:44] – add more info Robin Getz | university:tools:pluto:users:antennas [01 Feb 2021 14:55] (current) – Change broken link Iulia Moldovan |
---|
The antennas connectors on the ADALM-PLUTO are standard polarity [[wp>SMA_connector|SubMiniature version A]] (SMA) connectors. There are many ways to [[wp>Antenna_measurement|characterize]] an antenna, from gain (or loss), radiation pattern, beamwidth, polarization, and impedance. | The antennas connectors on the ADALM-PLUTO are standard polarity [[wp>SMA_connector|SubMiniature version A]] (SMA) connectors. There are many ways to [[wp>Antenna_measurement|characterize]] an antenna, from gain (or loss), radiation pattern, beamwidth, polarization, and impedance. |
| |
The actual antennas included with the ADALM-PLUTO are [[http://www.jinchanggps.com/jinchang_en/product_detail.asp?id=68|Jinchang Electron]] {{./jcg401.pdf|JCG401}}. While the JCG401 is specified for 824-894 and 1710-2170MHz, they do operate over a much wider range, but it should be understood that all antennas are filters. They will have some frequency selectivity (however, they are not brick wall filters). Just because something is specified for 824 MHz, does not mean that it will not pick up something at 600MHz, or even 87MHz, or it might not. | The actual antennas included with the ADALM-PLUTO are [[https://www.jinchanggps.com/JCG401-GSM-Antenna-pd45551675.html|Jinchang Electron]] {{./jcg401.pdf|JCG401}}. While the JCG401 is specified for 824-894 and 1710-2170MHz, they do operate over a much wider range, but it should be understood that all antennas are filters. They will have some frequency selectivity (however, they are not brick wall filters). Just because something is specified for 824 MHz, does not mean that it will not pick up something at 600MHz, or even 87MHz, or it might not. |
| |
The {{./jcg401.pdf|JCG401 datasheet}} does spec radiation pattern, beamwidth, polarization, and impedance, but leaves out performance (gain or loss) over frequency - since it is spec'ed for 824-894 and 1710-2170MHz. We can quickly do that ourselves with the help of a [[http://www.keysight.com/find/E5071C|E5071C ENA Series Network Analyzer]]. We connect the two antennas to the two ports, calibrate with a wire, and then run a S<sub>21</sub> test. | The {{./jcg401.pdf|JCG401 datasheet}} does spec radiation pattern, beamwidth, polarization, and impedance, but leaves out performance (gain or loss) over frequency - since it is spec'ed for 824-894 and 1710-2170MHz. We can quickly do that ourselves with the help of a [[http://www.keysight.com/find/E5071C|E5071C ENA Series Network Analyzer]]. We connect the two antennas to the two ports, calibrate with a wire, and then run a S<sub>21</sub> test. |
| |
[[wp>Scattering_parameters|S-parameters]] describe the input-output relationship between ports (or terminals) in an electrical system. For instance, if we have 2 ports (intelligently called Port 1 and Port 2), then S<sub>12</sub> represents the power transferred from Port 2 to Port 1. S<sub>21</sub> represents the power transferred from Port 1 to Port 2. In general, S<sub>NM</sub> represents the power transferred from Port M to Port N in a multi-port network. For an excellent side view into antenna's check out Peter Joseph Bevelacqua 's excellent reference : [[http://www.antenna-theory.com/http://antenna-theory.com]] | [[wp>Scattering_parameters|S-parameters]] describe the input-output relationship between ports (or terminals) in an electrical system. For instance, if we have 2 ports (intelligently called Port 1 and Port 2), then S<sub>12</sub> represents the power transferred from Port 2 to Port 1. S<sub>21</sub> represents the power transferred from Port 1 to Port 2. In general, S<sub>NM</sub> represents the power transferred from Port M to Port N in a multi-port network. For an excellent side view into antennas check out Peter Joseph Bevelacqua's excellent reference: [[http://antenna-theory.com]] |
| |
Running an S<sub>21</sub> test on the E5071C will broadcast a tone from one antenna (on port 2), and receive it on the other (port 1), and plot the results (in dB) compared to a wire that was used during the calibration on the instrument. It's interesting note that we are measuring both Rx and Tx capabilities. It is possible that the Rx at sub 600MHz could be fine, and it is just a Tx problem (unlikely, but I just wanted to point it out). | Running an S<sub>21</sub> test on the E5071C will broadcast a tone from one antenna (on port 2), and receive it on the other (port 1), and plot the results (in dB) compared to a wire that was used during the calibration on the instrument. It's interesting note that we are measuring both Rx and Tx capabilities. It is possible that the Rx at sub 600MHz could be fine, and it is just a Tx problem (unlikely, but I just wanted to point it out). |